Search Results for gross moter meaning
The Brain of Modern Vehicles: Understanding Car Computing
At the core of car computing lies the Central Computing Unit, often referred to as the vehicle's brain. This pivotal component is responsible for aggregating and integrating a myriad of electronic systems, ensuring that every aspect of the vehicle operates in harmony.
The Next Generation Auto Standard - Amphenol CS
Amphenol ICC’s Minitek MicroSpace ™ Crimp-to-Wire connector platform's unique design enables LV214 Severity-2 and performs at 1.8, 1.5 and 1.27mm pitch. It has many advantages over its USCAR certified counterparts. The Minitek MicroSpace ™ has an operating temperature of 130̊ C which makes it suitable to be even used inside an engine.
Driving Safe with LV214 and USCAR Standards - Amphenol CS
LV214 is an essential industry specification that regulates the automobile industry. Along with USCAR, LV214 plays a significant role in determining the quality of automotive components. This blog will focus on USCAR and LV214 and explore the products from Amphenol that are qualified to meet standards and specifications.
Magnetostrictive Liquid Level Transmitters with ... - Temposonics
‘Gross Observed Volume of the Product’ – The total volume of the tank occupied by the product liquid. When measuring only one liquid, it is also the total volume of liquid in the tank (GOVT). When measuring two liquids it is the total volume of liquid in the tank minus the volume of the interface liquid (GOVT – GOVI). GOVT
Understanding Different Cable Gland Thread Types: NPT, Metric, & PG
Cable glands are an essential component of any electrical installation, and understanding the different types of thread used in cable glands is important. The three most common types of threads used in cable glands are NPT, Metric, and PG.
P72 Traditional/CW Trolling Motor/In-hull - Airmar
The P72 is a small, economical, trolling-motor transducer and can also be used as an in-hull or portable-mounted sensor. The P72’s small size also makes it well suited for ice fishing. Find an Airmar Certified Installer/Dealer Near You!
Accelerometers: Hermetic sealing and helium leak testing
Units with leak rates above about 1 x10-3 cc/sec will saturate the detector and are usually considered "gross leakers." A "gross leaker" is not considered hermetic, even though it is welded and may look sealed! All accelerometers rated as "hermetic" on the data sheet are qualified using HLT.
Low frequency machinery monitoring: measurement considerations
Low frequency monitoring of industrial machinery requires specialized sensors, instrumentation and measurement techniques. The primary goal when measuring low frequency vibrations is to minimize electronic noise from the sensor and monitoring instrument.
General Motors | Amphenol Global Search | Amphenol
In the dynamic realm of robotics, the seamless integration of motors and drives is the cornerstone of efficient and precise movement. Amphenol is a leading supplier of advanced interconnect systems, sensors and antennas for a growing array of automotive applications.
What is a shock? - Temposonics
What is a shock? A shock is a single short-time high impact load. Such a load occurs, for example, when an object falling from a table hits the floor. The more rigid the object and the floor are, the higher the shock applied to the object.
12 things to consider when selecting an accelerometer
Selecting an industrial accelerometer – what to consider • Acceleration and velocity sensors monitor for different faults – Velocity sensors are used for the majority of applications because velocity is the best overall
Understanding MIL-C-24368/1 Shore Power Assemblies - TPC Wire
MIL-C-24368/1 is a military specification that defines the requirements for shore power assemblies used in naval and maritime applications. These assemblies are designed to provide a safe and reliable electrical connection between a docked vessel and the shore power supply.
HYDRO POWER TURBINE GENERATOR ROTOR MONITORING - PCB
The AT-7000/ Motor Monitor can also be configured to additionally measure rotor voltages and currents, detect ground faults, and monitor shaft torque and torsional vibration. The Motor Monitor is a variation of the AT-7000 product line. R4
Moisture Meters - Amphenol Sensors
Protimeter offers a leading line of handheld moisture meters and thermo-hygrometers for building survey, building restoration, construction and agriculture. With nearly 60 years of experience in the design and manufacture of moisture measurement products, Protimeter leads the way in design, innovation, performance and integrity.
MMS 2 Moisture Measurement System - Protimeter
Now, with wireless capability, the Protimeter MMS3 represents the latest in moisture measurement technology. Its ergonomic 4-in-1 design allows for fast accurate full building moisture diagnostics both on and below the surface, from new building construction to refurbishing projects in existing buildings.
Human Machine Interface (HMI)- The Intelligent Interface between ...
HMI can be any medium that helps you communicate with the connected machineries or devices from a simple mobile device like a tablet, to multi-touch-enabled control panels installed in high-end CNC machines (Computerized Numerical Control). Why are HMIs Used?
Poland Secures $745 Million Deal for 200 US-made AARGM-ER Missiles
The AGM-88G AARGM-ER is an advanced iteration of the AGM-88 missile series, featuring a dual-pulse solid rocket motor and an advanced warhead, effectively doubling its range over previous versions.
Sensors for Aerospace Ground Testing | PCB Piezotronics
GVT (Ground Vibration Testing) - Includes sensors for modal analysis and random vibration testing, and shakers to create the excitations. Reliability and Functional Testing - A great deal of aerospace ground testing involves exposing systems to realistic loading and environmental testing conditions.
Empowering Autonomous Robots: The Role of Battery ... - Amphenol CS
Much like in electric vehicles, the Battery Management System (BMS) emerges as a critical player, ensuring the efficient utilization of energy and the safeguarding of batteries against potential hazards. In this blog post, we delve into the pivotal role of BMS in robotics, exploring its benefits and applications.
Why Do You Need A Temporary Power Source? - TPC Wire
When it comes to an unexpected loss of power, finding yourself in reactive mode is not where you want to be. Being prepared is the only way to keep your plant fully operational in an unexpected power outage and the ability to deploy your own supplementary temporary power is now a possibility.