Search Results for “absorption spectroscopy diagram
Infrared Sensor Application Note 1 A Background to Gas Sensing by Non ...
IR gas absorption spectra cover a wide range from 2.0 to 20 microns and show a multiplicity of broad peaks and fine line structures. These features are characteristics of the gases, rather like individual fingerprints.
Single and multi-sensor SDD detectors for beam-line applications
detector systems for x-ray spectroscopy applications using synchrotron radiation, conventional x-ray tube or charged particle beam excitation. Previously known as e2v scientific instruments and Gresham Scientific Instruments, SGX produces detectors from standard designs through customised assemblies to complex multi-element detectors. All
Engineering Assets - All Sensors
Looking for specific information when deciphering low-pressure sensor data? Utilize our definition of terms from A to Z. Absolute Pressure: Pressure measured relative to a vacuum. Usually expressed in pounds per square inch absolute (psia).
Introduction to Electrochemical (EC) Gas Sensors - SGX Sensortech
SGX electrochemical sensors detect gases by producing a chemical reaction between the gas and oxygen contained in the sensor. This reaction produces a small current, which is proportional to the concentration of the gas present. The sensor is, in effect, a type of fuel cell.
IMPACT AND DROP TESTING - PCB
on various components. Design engineers request data in energy units such as Joules, yet the data must be recorded using force, velocity, acceleration, d. tance, and time units. The purpose of this paper is to present the test engineer with a guide for using force measurements obtained during impact testing to compute the a.
'Total Quality with Rapid Through-put of Powdered Metal and Cast ... - PCB
To ensure necessary quality, 100% end-of-line part inspection must be implemented; traditional NDT techniques such as magnetic particle, liquid penetrant, eddy current and X-ray, or purely visual inspection, are painstaking, subjective manual processes.
Cooling Tower Application Study - Wilcoxon Sensing Technologies
An Amphenol Company info@wilcoxon.com www.wilcoxon.com buy.wilcoxon.com Cooling Tower Application Study The machine shop was able to perform repairs on the motor for a total cost of just under $5,000, well be-
NovaSensor Medium and High Pressure MEMS Pressure Sensor Die
When excited by either constant voltage or constant current, the P883 die produces a differential millivolt output signal directly proportional to the applied pressure.
General Signal Conditioning Guide - PCB
quartz and ceramic ICP® sensors. These sensors are comprised of a basic piezoelectric transduction mechanism (which has an output proportional to force, pressure, accel-eration, or strain, depending on the sensor type) coupled to a h.
Pellistor Application Note 1 Pellistor Sensor Technology & Applications
Pellistors are gas sensors that detect combustible gases and vapours in air (or atmospheres containing oxygen), in concentrations approaching the explosive range. In this case, they are operating in a catalytic mode where the target gas is burnt and the heat liberated is measured by the sensor.
amphe-lite-subminiature-connectors-catalog-amphenol-industrial
AMPHENOL CORPORATION Amphenol Industrial Operations 191 Delaware Avenue Sidney, NY 13838-1395 Telephone: 888-364-9011 Fax: 520-397-7169
NovaSensor PT2710 Pressure and Temperature Sensor Die
When excited by either constant voltage or constant current, a PT2710 pressure sensor produces a differential millivolt output signal directly proportional to the applied pressure. With NovaSensor’s SenStable® process, PT2710 die features excellent long-term stability and repeatability (< 0.1% / year typical).
TECHNICAL NOTE TN-17 - PCB
Comparing advantages and limitations of the two systems may be helpful in selecting an accelerometer and measurement system best suited for a specific laboratory, field, factory, underwater, shipboard or airborne application. This paper will review sensor selection considerations involving two general types of piezoelectric sensors.
The following presentation slides are for reference purposes only ...
Amphenol PCD’s Electrocon Line comprises a family of rugged, high-reliability screw-terminal/edgecard connectors. They combine the discrete wire termination capability of a screw-terminal bl11ock with the mass termination convenience of an edgecard connector.
SGX Infrared Gas Sensor Evaluation Kit IR-EK2 User Guide
Set four alarm levels (2 per channel) which drive on-board LEDs and open collector outputs. Log readings of peak-to-peak output signal, gas concentration and temperature using the supplied PC Data Logging Program. Read the Manual! The supplied CD should auto-run on your PC when inserted into a CD drive. Select ‘User Guide’ from the CD menu.
FAKRA CONNECTOR SERIES - Amphenol RF
12 different mechanical and color codes, plastic housing with locking feature and audible clicking noise, minimum of 100 mating cycles and a frequency range of DC to 6 GHz. These connectors are available in numerous configurations with straight, and right angle solutions for cable applications, as well as edge-launch and PCB designs.
QUICK REFERENCE TECHNICAL GUIDES - PCB
PCB has compiled their most common technical sensor information into four comprehensive quick reference guides; Accelerometers, Acoustics, Pressure, and Force.
800Gb/s OSFP Transceivers | Optical Interconnect | Amphenol
Amphenol's 800G OSFP optical modules include 2xDR4 (plus), 2xFR4 (plus), 2xLR4, AOC, and AOC breakout series, which adopt LC or MPO optical ports and are compatible with IEEE802.3, OIF-CMIS and other standards. It is mainly used in 800G Ethernet applications and other environments. Have any questions? Talk with us directly using LiveChat.
FORCE & STRAIN FUNDAMENTALS - PCB
PCB offers multiple ICP® signal conditioners from 1 to 16 channels with current adjustment within 2 - 20 mA at +18 to +30 volts DC. Refer to PCB Tech Note TN-32 for more information on signal conditioners and impedance.
General Signal Conditioning Guide - PCB
Core competencies include ICP® and charge output piezoelectric, piezoresistive, strain gage, MEMS and capacitive sensors and instrumentation.