Search Results for 30-271
CDS30DE-380/2700 - 30dB Directi - RFS Technologies an Amphenol Company
RFS Technologies designs and manufactures premium-quality cable and antenna solutions for wireless, public safety, distributed antenna system (DAS) and other telecom markets in North America. As an Amphenol company, we’re part of a global powerhouse in high-technology, interconnect, sensor and antenna solutions that’s enabling the electronics revolution across almost every industry. Our ...
Amphenol Ardent Concepts
30 Insertion Loss US Patent Numbers 6,787,709, 7,556,503, 8,926,342. CR Molded GHz Sockets and Connectors for I-GA, BGA, Board to Board High Repeatability, High Durability, Low Cost ARDENT CONCEPTS Innovativo tntorconnoet Sotut;ons BGA Configuration I-GA Configuration
Charles Universal Broadband Enclosure CUBE-RL21221xxx General ...
LT-RL21221xxx Page 4 of 8 14 th Printing 3.5. Lifting the CUBE See the supplemental documentation for CUBE weight. Charles recommends the following
NovaSensor NPP-301 Pressure Sensor FAQ's - amphenol-sensors.com
If a car tire measures 30 psig at sea level, then the NPP-301 will measure 44.7 psia, which is the tire pressure plus the ambient pressure of 14.7 psia. If the same car tire travelled to 10,000 feet, the NPP-301 would still measure 44.7 psia, but a tire gauge will read 34.6 psig (44.7-10.1), because the ambient pressure is only 10.1 psia.
SMP Female to SMP Female 3" Cable Assembly for .047 Cable
EU RoHS Directive 2011/65/EU Yes, w/ Exemption 6C . These products comply with the substance restrictions of the Restriction on Hazardous Substances Directive 2011/65/EU (RoHS2).
Thermometrics ZTP-115 Thermopile IR Sensor
Noise Voltage 30 nV rms R.M.S., 25°C NEP 0.50 nW/Hz1/2 500K, 1 Hz Detectivity 1.00 E08 cmHz1/2/W 500K, 1 Hz Time Constant 20 ms Parameter Limits Units Condition Min Typ Max Resistance 9.7 10 10.3 kW Tol. :3%, @25°C Beta - Value 3930 3970 4010 K Tol. :1%, Defined at 25°C/85°C Absolute Maximum Ratings
amphe-power-radsok-technology-catalog-amphenol-industrial
30 Impala Road 2196 Sandton - Chislehurston South Africa Tel: (27-11) 783-9517 Fax: (27-11) 783-9519 E-mail: amphenol_africa@csi.com TURKEY Amphenol Turkiye Ayazaga Mah. Meydan Sk. No. 28 Beybi Giz Plaza, Kat. 26 Maslak 34396 Istanbul Phone:90 (212) 335 25 01 Fax:90 (212) 335 25 00
NovaSensor NPP-301 Series Pressure Sensor - amphenol-sensors.com
200 kPa ≈30 psi 700 kPa ≈100 psi Maximum Pressure 3x rated pressure Electrical @ 77°F (25°C) unless otherwise stated Excitation 3.0 V 10 VDC maximum Input Impedance 5,000 ±20% Ω Output Impedance 5,000 ±20% Ω Environmental Electrostatic Damage (ESD) Class 1 Operating Temperature Range –40°F to 257°F (–40°C to 125°C) Mechanical (1)
NTC Thermistors Type RL30 - amphenol-sensors.com
Uncoated Disc With Radial Leads Description Point-matched disc thermistor with bare lead-wires. Features • Low cost solid state sensor • Resistance tolerances down to ±2%
CDS30DE-694/3800 - 30dB Directi - RFS Technologies an Amphenol Company
RFS Technologies designs and manufactures premium-quality cable and antenna solutions for wireless, public safety, distributed antenna system (DAS) and other telecom markets in North America. As an Amphenol company, we’re part of a global powerhouse in high-technology, interconnect, sensor and antenna solutions that’s enabling the electronics revolution across almost every industry. Our ...
5 4 3 2 1 ECO # B ADDED 30dB AMPLITUDE 13-1417/15/13 T
2782-6051-db yyww marking area.86 21.84 c new format/added marking 14-40212/9/14 t.kuhn b added 30db amplitude 13-1417/15/13 t.kuhn electrical frequency range dc - 26.5 ghz
Amphenol Broadband Solutions (ABS) Dual Winner in 2020 Diamond ...
Wallingford, CT September 30, 2020 – Amphenol Broadband Solutions (ABS) announced today that it won two 2020 Broadband Technology Report (BTR) Diamond Technology Review Awards: one for its OSP-AOM and one for its SIKs. The awards are based on a variety of criteria, including unique technological innovation, ease-of-use, efficiency, reliability
NovaSensor NPP-301 Series Pressure Sensor - amphenol-sensors.com
200 kPa ≈30 psi 700 kPa ≈100 psi Maximum Pressure 3x rated pressure Electrical @ 77°F (25°C) unless otherwise stated Excitation 3.0 V 10 VDC maximum Input Impedance 5,000 ±20% Ω Output Impedance 5,000 ±20% Ω Environmental Electrostatic Damage (ESD) Class 1 Operating Temperature Range –40°F to 257°F (–40°C to 125°C) Mechanical (1)
NovaSensor NPP-301 Pressure Sensor FAQ's - amphenol-sensors.com
If a car tire measures 30 psig at sea level, then the NPP-301 will measure 44.7 psia, which is the tire pressure plus the ambient pressure of 14.7 psia. If the same car tire travelled to 10,000 feet, the NPP-301 would still measure 44.7 psia, but a tire gauge will read 34.6 psig (44.7-10.1), because the ambient pressure is only 10.1 psia.
3282-7001-dB B Model (1) - xmacorp.com
0-10, 12, 15, 20, 30 db attenuation accu racy 0 - 6 db ± 0.3 db 7 - 12 db ± 0.5 db 21 - 30 db ± 0.75 db vswr 1.25:1 max. power (avg) 2 watts @ 25°c derates linearly to 0.5 watts @ 125° c power (peak) 250 watts 5us pw, .05%dc impedance 50 ohms temperature ran ge (°c)-65 to +125 materials center contact nd coupling nut gold pla ted becu ...
NTC Thermistors Type RL30 - amphenol-sensors.com
Uncoated Disc With Radial Leads Description Point-matched disc thermistor with bare lead-wires. Features • Low cost solid state sensor • Resistance tolerances down to ±2%
Application Overview – Ethernet over T1 (Router) - Charles Industries
2/3/2003 Application Overview – Ethernet over T1 (Router) Application: Ethernet LAN Extension over T1 (Charles 360-80 Intelligent Channel Bank with RAD TinyRouter) Customer Solutions: Enterprise, Campus, ITCOs, CLECs. Description: This solution allows customers to cost effectively provide Ethernet connectivity to PCs and other devices served by a T1 network.
NovaSensor NPP-301 Pressure Sensor FAQ's - amphenol-sensors.com
If a car tire measures 30 psig at sea level, then the NPP-301 will measure 44.7 psia, which is the tire pressure plus the ambient pressure of 14.7 psia. If the same car tire travelled to 10,000 feet, the NPP-301 would still measure 44.7 psia, but a tire gauge will read 34.6 psig (44.7-10.1), because the ambient pressure is only 10.1 psia.
NovaSensor NPP-301 Pressure Sensor FAQ's - amphenol-sensors.com
If a car tire measures 30 psig at sea level, then the NPP-301 will measure 44.7 psia, which is the tire pressure plus the ambient pressure of 14.7 psia. If the same car tire travelled to 10,000 feet, the NPP-301 would still measure 44.7 psia, but a tire gauge will read 34.6 psig (44.7-10.1), because the ambient pressure is only 10.1 psia.
Charles Universal Broadband Enclosures - Charles Industries
CUBE Applications Macro Cell Equipment With the strong push to roll out LTE, large numbers of new macro cells are being built. Cell site equipment has gotten smaller and more efficient over the years, and movement towards CRAN