Search Results for access api
Software Development Kit - PCB
The SDK provides the documentation needed to use the http API that is built into the HVM200 and the libraries to access data stored in HVM200 data files. This is accomplished by communicating to the sound level meter over a network using a tcp/ip socket.
Please log in - Sachsenkabel pulse
We provide various Application Programming Interfaces (APIs) for easy documentation of our products in your software and for the automated transfer of order, product and quality data. An API key is required to get access to the API functions. The key is available in your pulse account.
HUMAN VIBRATION METER - PCB
we offer a software development kit, SDK, to facilitate the development. The HVM200 API is based upon http, html and JSON so command and responses are plain text and highly portable; which makes software development much easier. A DLL with a C-sharp API is also provided with the SDK in order to access data in files.
Operation Manual Level Plus DDA Interface - temposonics.com
a petroleum liquid is compared to water. Allowable values are 0 to 100 degrees API . e of an object at a specific temperature. The densit. plant or factory automation environment. Developed and .
Magnetostrictive Liquid Level Transmitters with Temposonics
API Gravity The measure of how heavy or light a petroleum liquid is compared to water. Allowable values are 0 to 100 degrees API for (6A) and 0 to 85 degrees API for (6B). D DDA ‘Direct Digital Access’ – The proprietary digital protocol developed by MTS for use in intrinsically safe areas. Density
PCTEL - SeeHawk ® Central
This site reports data for the United States, compiled from testing information entered into SeeHawk Central. Data will continue to be updated as more users upload test results, but as of July 2023 it represents a small fraction of tests conducted using PCTEL’s testing solution or other methods.
FAQ - Amphenol Socapex
What is the primary function of Amphenol Socapex USB3 Type A - Type C adapter? The adapter allows integration of new equipment with a USB Type C port without disassembling an existing USB2 or USB3 Type A connection. What is the maximum data transmission speed of the reinforced adapter? The adapter supports USB 3.2 Gen 1 with data rates up to 5Gb/s.
Gflex® Scanning Receiver | Test & Measurement - PCTEL
The G flex ® scanning receiver is the next generation of mobile network testing from PCTEL®. Designed to support drive testing, walk testing, and government applications for 2G-5G and beyond, the G flex sets a new standard for power, portability, and flexibility in a 5G and mmWave capable scanner.
Software Downloads | Support - PCTEL
Download the latest utilities, software, drivers & more for your PCTEL products, devices, and software.
Support - PCTEL
Download software, firmware, drivers, and documentation for PCTEL products. Firmware updates are available here for scanning receivers under warranty. Product return instructions and Return Materials Authorization (RMA) forms. Explore calibration, upgrade, and repair options for scanning receivers and related test and measurement products.
SHORT-FORM PRODUCT CATALOG - Wilcoxon Sensing Technologies
improve safety, and simplify access to critical machine information. HOW IT WORKS 1 2 4 3 INSTRUMENTATION including handheld data collectors and reference sources are useful tools for all analysts, in both permanent and portable installations. CABLE ASSEMBLIES carry the signal from the sensor. Choose a suitable cable for the environment,
Model 2775C PE/IEPE Signal Conditioner IM2775C - PCB
ground isolation for cleaner data collection. With capability to install up to six units in an optional 19-inch rack accessory (model 4948A), the flexible setup of the model 2775C is accomplished either manually via the unit’s front panel, or via the unit’s .
Operation Manual Level Plus CHAMBERED - Temposonics
A Bidirectional communication protocol that provides data access between intelligent field instruments and host systems. I Interface Noun; The measurement of the level of one liquid when that liquid is below another liquid. Interface Adj.; The Software Graphical User Interface (GUI) that allows the user to access software protocols (HART®, DDA ...
IBflex® Scanning Receiver | Test & Measurement - PCTEL
Low power consumption and a hot-swap battery system make the IB flex scanner a convenient tool for a long day of walk testing or interference hunting. The IBflex® is portable & accurate, built for testing of indoor & outdoor 5G NR, LTE, 2G/3G cellular, WiFi & public safety/LMR networks. Learn more.
t3-4 | Amphenol Global Search | Amphenol
Amphenol Network Solution s’ patented 6-port DSX-3 design provides acces s to both sides of the T3 signal to greatly simplify maintenance. Rear cross- connect and total front access options are available. ELF-3206-1200 2-Termination Rear Cross-Connect DSX-3 Module BNC I/O field Mini-WECO Module jacks . ELF-3206-1900.
Gflex Scanning Receiver Brochure - PCTEL
Test up to 120 5G channels simultaneously. Measure the full channel on every 5G band. Benchmark multi-operator 2G-5G with one unit. Support government applications with I/Q testing. Download this brochure for G flex® product features and specifications.
Level Plus - Temposonics
「一般的な原油」、api比重に対して60℉に体積を補正します。 6b軽油 「一般的な製品」、api比重に対して60℉に体積を補正します。 6c化学品 個別かつ特別な用途に適した「体積補正係数(vcf)」、熱膨張係数に 対して60℉に容量を補正します。 6c mod
Privacy & Policy - Amphenol CS
Amphenol respects individuals' rights under the GDPR, and we may ask you for additional information to confirm your identity and for security purposes, before providing individuals with access to their personal data. There may also be circumstances where Amphenol is permitted by law to deny access.
IBflex® Scanning Receiver Brochure - PCTEL
IB flex ® scanning receiver combines portability and accuracy with the power to test multiple technologies and bands simultaneously. It can be used to deploy 5G New Radio networks in sub-6 GHz spectrum, verify public safety coverage, optimize dense small cell deployments, and improve the reliability of IoT systems.
取扱説明書 - Temposonics
HART® インテリジェントなフィールド機器とホストシステムとの間のデータアクセスを提供する双方向通信プロトコル。 名詞:別の液体の下に位置するある液体の水面の高さ。 インターフェース形容詞:ユーザーによるソフトウェアプロトコル(へのアクセスを可能にするソフトウェアHART、DDA、MODBUS)フェース(GUI)。 グラフィカルユーザーインター. ‘Intrinsically safe’された相互接続配線を有する装置内の電気エネルギーを火花や加(本質的安全)- 爆発の可能性がある空気に曝露熱の影響が発火の原因となり得ないレベルにまで制限することを基礎とする保護タイプ。