Search Results for airmar
ST850 Smart™ Sensor SST Thru-hull NMEA 2000® - Airmar
Speed and Temperature. The ST850 is a low-profile, retractable, thru-hull sensor that computes accurate speed and temperature data and sends it to any NMEA 2000 ® network. These low-profile units are nearly flush, minimizing drag with only 5 mm (3/16") extending outside of the hull.
CM270W Traditional Cavity Mount - Airmar
Airmar no longer manufactures this transducer. 1kW. The CM270W is designed for tank mounting in commercial fishing vessels. It's versatile design also allows it to be flush mounted in the keel of larger sportfishing vessels.
220WXH WeatherStation® Instrument - Airmar
Certs And Standards: CE, IPX6, RoHS, IEC61000-4-2, IEC60945, IEC60950_1C, IEC60950_22A, EN55022, EN55024, EN14982
T80 Temperature Sensor - Airmar
Transom or Bulkhead Mount. The T80 stainless steel model can be mounted on a vessel's transom to measure water temperature. It can also be used in a live well or engine room.
DST800L 235kHz, 100W, Smart™ Sensor, Bronze Long-Stem, NMEA ... - Airmar
The DST800L is a Smart ™ Triducer ® Multisensor that offers depth, speed, and temperature functions in one thru-hull fitting. The long-stemmed transducer is designed for use in thick-hulled, wooden boats or vessels with a steep deadrise. The optional high-performance fairing vertically orients the beam for strong return echoes, resulting in optimal performance even at higher speeds.
B17-HP Smart™ Sensor Thru-hull - Airmar
The B17-HP, high-precision temperature sensor responds quickly and accurately to temperature changes. The 25 mm (1") bronze button on the sensor’s face along with the specialized fast-response thermistor provide a five-second time constant and ±0.3ºC (±0.17ºF) accuracy.
AT225 Airducer® Ultrasonic Transducer - Airmar
Non-contact level, flow, distance, proximity and object detection measurement is reliably delivered by the ultrasonic AT225. It includes rugged sealed construction and operates at 228 kHz.
Machinist - Airmar
Join Airmar as a Machinist and be part of a skilled team manufacturing precision components for marine electronics. Learn about the responsibilities and qualifications for this role, including operating CNC machines, interpreting blueprints, and performing quality checks. Explore competitive compensation, benefits, and a supportive work environment.
ST69 Transom Mount - Airmar
Speed and Temperature. The ST69 is the ultimate, high-speed, transom-mounted sensor. The paddlewheel and housing do not project below the hull which minimizes spray and drag.
SS175H Chirp-ready Tilted Element Thru-hull - Airmar
1 kW. Airmar’s low-profile, Chirp-ready, transducer models are the perfect addition to smaller boats such as center consoles. The high-frequency band, transmitting between 130 and 210 kHz, has a narrow beamwidth—excellent for pinpointing fish holding tight to wrecks, reefs, and other structures.
SS538 Survey Transducer - Airmar
Airmar’s commitment to innovative technology has produced the SS538. This broadband, 200 kHz transducer has a Q of 2 and very good sensitivity.
Production Operator II - Airmar
Explore a rewarding career as a Production Operator II at Airmar Technology Corporation. Join our team and contribute to the manufacturing excellence that powers innovation in marine and industrial sensor technology.
Process Improvement Coordinator - Airmar
Explore exciting career opportunities at Airmar, a leading company. Join us as a Process Improvement Coordinator and contribute to our innovative culture. Discover a fulfilling career where your skills make a difference. Apply now!
Dealer Details - Airmar
AIRMAR ISO Certification (PDF Download) Supplier Change Notification (PDF Download) Supplier Corrective Action Request (PDF Download) Supplier Quality Support Manual (PDF) DISCOVER. Videos. What is XID? AIRMAR Certified Installers. Installer Finder. WeatherStationWX.com
M190-33 kHz Survey Transducer - Airmar
Cable Type: C43, one shielded twisted pair (2-14 AWG) with braided shield, black neoprene jacket, 10 mm (13/32") diameter
B164 Traditional/CW Tilted Element™ Thru-hull - Airmar
1 kW. Step up to a 1 kW—without a fairing! The 1 kW, flush-mount, Tilted Element ™ transducer is perfect for fast, trailered vessels that cannot accommodate a High-performance Fairing. The flush-mounted, bronze housing extends less than 6.35 mm (1/4") below the hull, so it can sit on trailer rollers and bunks.
ARK30 Airducer® Ultrasonic Transducer - Airmar
Non-contact level, flow and distance measurement is reliably delivered by the ultrasonic ARK30. Its rugged one-piece Kynar PVDF housing makes it suitable for the most chemically aggressive environments.
CM265LH Chirp-ready Cavity Mount - Airmar
1 kW. We know that specific frequencies excel at detecting certain species of fish: Bluefin Tuna—60 kHz, squid—133 kHz, and cod—175 kHz. Airmar’s CM265LH transducer includes all these frequencies plus every other frequency in the high and low bandwidth.
B75H Chirp-ready Tilted Element Thru-hull - Airmar
600 W. Airmar’s low-profile, Chirp-ready, transducers are the perfect addition to smaller boats such as center consoles. The high-frequency band of the B75H, operating between 130 and 210 kHz, has a narrow beamwidth—excellent for pinpointing fish holding tight to wrecks, reefs, and other structures.
ATK200 Airducer® Ultrasonic Transducer - Airmar
The ultrasonic ATK200 brings proven dependability to level, flow, distance, proximity and object detection measurement applications. Its rugged one-piece Kynar PVDF housing makes it suitable for chemically aggressive environments.