Search Results for amphenol aerospace operations ms27656t25f46s
9001 | Amphenol Global Search | Amphenol
Amphenol Aerospace's Statements and Certifications. Military and Commercial Electrification Part 3 – Building the Bridge to Fully-Electric Platforms ... Amphenol Aerospace Operations Initial Certification Date Overall Scope: The design, development, and manufacture of high performance electrical and fiber optic connectors, cable assemblies ...
Ruggedized SATA Connector | Products | Amphenol Aerospace
The R-SATA (r ugged ized) S ATA connector is perfectly suited as the primary internal storage interconnect for desktop and mobile PCs, connecting the system to peripherals such as hard drives, solid state drives, optical drives, and removable magnetic media drives. The R-SATA supports SATA 3.0 protocol, delivering 6.25 Gb/s data rates and beyond. Amphenol’s R-SATA connector s utilize a m ...
EU RoHS II CoC - amphenol-aerospace.com
In response to your compliance status inquiry regarding the following product, Amphenol Aerospace Operations (AAO) and Amphenol Commercial Air Division (ACAD) offers the following information: AAO/ACAD Part Number EU RoHS II Compliant Part/Product Description Exemptions (If Applicable) M39029/56‐349 YES CONTACT, SOCKET 6(c)
Commercial Aerospace | Markets - Amphenol
Amphenol is a leading provider of high-performance interconnect systems and components to the commercial aerospace market. In addition to connector and interconnect assembly products, we also provide rigid and flexible printed circuits as well as high-technology cable management products.
FiberQuad Ruggedized Quadrax Contacts - Amphenol Aerospace
Each Quadrax contact can contain a fiber optic transmitter or receiver; Support for speeds up to 28.05 Gbps; Support for 1300nm multi-mode (for legacy protocols such as 100-Base-FX), 1310nm singlemode, and 850nm multi-mode wavelengths
M6242 SERIES | Products | Amphenol Aerospace
Amphenol Connectors Cross Reference Guide Military and Commercial Electrification Part 3 – Building the Bridge to Fully-Electric Platforms Artificial Intelligence, C5ISR, Smart Weapon Systems, and More: Exploring The Next Generation of Defense Systems
Reduced Flange Jam Nut Receptacles - Amphenol Aerospace
Provides space savings inside the box or on the panel; Provides direct and indirect weight savings; 30% lighter than standard 38999/24 (w/o stand-offs)
News - Amphenol Aerospace
Amphenol Aerospace Director of Operations Jason Youngs prepares to get dunked during Amphenol Aerospace’s annual Open House at the company’s Sidney, NY facility on Aug. 27. With attendees paying for the chance to dunk them, Youngs opted to donate his proceeds to Women in Electronics, a nonprofit that seeks to expand opportunities for women ...
Differential Twinax Contacts | Products | Amphenol Aerospace
EMI Shielding: 360-degree shielding on each pair Voltage Rating: 500 Vrms max @ sea level Dielectric Withstanding Voltage: 500 VAC RMS sea level Temperature Range:-65C to 175C Bandwidth: Up to 1.25 GHz Data Rate: Exceeding 2.5 Gbps. Voltage Rating: 500 Vrms max. @ sea level
EU RoHS II CoC - amphenol-aerospace.com
In response to your compliance status inquiry regarding the following product, Amphenol Aerospace Operations (AAO) and Amphenol Commercial Air Division (ACAD) offers the following information: AAO/ACAD Part Number EU RoHS II Compliant Part/Product Description Exemptions (If Applicable)
EU RoHS II CoC - amphenol-aerospace.com
In response to your compliance status inquiry regarding the following product, Amphenol Aerospace Operations (AAO) and Amphenol Commercial Air Division (ACAD) offers the following information: AAO/ACAD Part Number EU RoHS II Compliant Part/Product Description Exemptions (If Applicable)
rohs | Amphenol Global Search | Amphenol
Amphenol provides multiple options for alternate to cadmium platings, including Durmalon, Black Zinc Nickel, and the new AP-93 1000-hour salt spray approved plating. Amphenol uses the RoHS requirements and the latest revisions to the MIL-DTL-38999 specification to develop these platings.
Statements and Certifications - Amphenol Aerospace
Amphenol Connectors Cross Reference Guide Military and Commercial Electrification Part 3 – Building the Bridge to Fully-Electric Platforms Artificial Intelligence, C5ISR, Smart Weapon Systems, and More: Exploring The Next Generation of Defense Systems
m39029 | Amphenol Global Search | Amphenol
M39029/59-366 Supersedes MS27535 L-1107-E December 2004 FSCM77820 Amphenol Aerospace AMPHENOL CORPORATION Amphenol Aerospace 40-60 Delaware Avenue Sidney, New York 13838-1395 www.amphenol-aerospace.com * May be soldered. ... Amphenol Aerospace Operations and Commercial Air Division hereby acknowledges the referenced product is in conformity ...
Amphenol Connector Reference Guide - Volume 2 | Amphenol Aerospace
Consult Amphenol Aerospace Sidney NY for variations. * Coaxial arrangements are not available in these classes. ** For more information on Coax/Triax/Twinax Ground Plane Connectors consult Amphenol Aerospace. NOTE: Catalog 12-C3 catalog was released Jan. 2010. It covers the majority of the circular connector products offered by Amphenol Aerospace.
High Density 38999 Style Connectors - Amphenol Aerospace
The HD38999 family of connectors has over 30% more contact density than the highest density Mil-Spec 38999 connectors of similar size. This series of connectors was designed to utilize mil-specified 38999 components with the exception of the insert arrangements.
The Coming Electrification of the Military - Amphenol Aerospace
Amphenol Aerospace’s High Power 38999 connector is the optimal power connector solution for high-power applications. The High Power 38999 meets the applicable requirements of MIL-DTL-D38999 Series III and provides current carrying capacity up to 1000 amps.
ROHS Compliant Alternatives to Cadmium Plating - Amphenol Aerospace
Amphenol provides multiple options for alternate to cadmium platings, including Durmalon, Black Zinc Nickel, and the new AP-93 1000-hour salt spray approved plating. Amphenol uses the RoHS requirements and the latest revisions to the MIL-DTL-38999 specification to develop these platings.
Businesses | Amphenol
Each of our Amphenol businesses partners with its customers across different market segments and regions to connect our world through leading-edge innovation. ... Amphenol Aerospace Operations New York, U.S. Amphenol Air LB France ... Amphenol Commercial Aerospace New York, U.S. Amphenol ConneXus Stockholm, Sweden ...
Series Five FAQ's - Amphenol Aerospace
Amphenol Aerospace has consistently proven itself to be a supporter of open standards, having provided the IP necessary for the U.S. government and others to specify many connector series, including 2M. If there is sufficient demand for an open standard for Series Five, Amphenol will support its creation. How is Series Five different from 2M?