Search Results for amphenol sensor megasquirt
Thermometrics Surface Mount Devices - amphenol-sensors.com
Amphenol Advanced Sensors. 2 Type NHQ Specification Surface mount chip 1206 size Description A range of 1206 size surface mount NTC chip thermistors.The terminations are nickel barrier with tin plating. General Soldering Recommendations • Maximum storage time in closed package: One year
NPX1 NovaSensor Sensors - amphenol-sensors.com
Amphenol Advanced Sensors. General Operating Temperature-40°F to 257°F (-40°C to 125°C) Storage Temperature-67°F to 257°F (-55°C to 125°C) Battery Supply Voltage 2.1 to 3.6 V (3.0 V typical) Supply Current 600 nA typical power down current at 3.6 V Pressure Ranges
Neonatal Temperature Monitoring | Skin Surface - amphenol-sensors.com
Amphenol Advanced Sensors carries an extensive line of MA100 and MA300 type interchangeable NTC chip thermistor assemblies for neonatal vital signs monitor. The NTC chip is protected in a plastic cap or metal disk, which will be secured directly to the newborn’s skin by a reflective adhesive patch. Designed with ultimate thermal transfer in ...
www.amphenol-sensors.com
Thermometrics® Sensor Temperature Resistance Curves -Reference Guide 2 © Amphenol Thermometrics, Inc., 967 Windfall Road, St. Marys, PA 15857, USA www.amphenol ...
www.amphenol-sensors.com
Thermometrics® Sensor Temperature Resistance Curves -Reference Guide 2 © Amphenol Thermometrics, Inc., 967 Windfall Road, St. Marys, PA 15857, USA www.amphenol ...
adam amphenol | Amphenol Global Search | Amphenol
Amphenol-Tuchel Electronics China Branch 20 Tianshan Road Changzhou 213022 Phone +86 519 8511 0301 www.amphenol.info Amphenol-Tuchel Electronics GmbH | August - Haeusser Strasse 10 | 74080 Heilbronn, Germany Telephone: +49 (0)7131 929 - 0 | Fax: +49 (0)7131 929 - 486 |www.amphenol.info | info@industrial-amphenol.com
NTC Type JW, JC - amphenol-sensors.com
NTC Type JW, JC Thermometrics Waterproof Clip-On Pipe Sensor Author: GE Subject: The JW and JC pipe sensors are suitable for use in conditions of high condensation and occasional immersion in water. Created Date: 3/25/2014 7:45:03 AM
Indoor Agriculture: Smart Greenhouse Environmental Monitoring and Control
Telaire has over 35 technology patents including ABC Logic™ and warrants single wavelength sensor calibration for the life of the sensor. Amphenol Advanced Sensors is a trusted OEM partner providing temperature, humidity, pressure, CO 2 and dust sensors to solution providers in the HVAC, automotive, industrial and healthcare markets.
Motor Coil Temperature Sensor | Amphenol Advanced Sensors
The sensor can be interlaced into the stator coil or tied to the neutral bus bar on the motor circuit. The sensor provides temperature feedback to indicate motor load or stall conditions. If the motor has an excessive load or a stall condition, the current in the coil of the busbar increases.
PROTIMETER - amphenol-sensors.com
Amphenol Advanced Sensors PROTIMETER How to Measure Moisture in Buildings Dampness is hazardous before you can see it. It is important to note that materials do not become visibly damp, and do not feel damp to the touch until they are quite dangerously damp. Wood, for example, does not feel damp
Environmental, Social and Governance - Amphenol
Amphenol’s high-performance culture of entrepreneurial accountability is uniquely powerful in ensuring a sustainable future.By giving our local management around the world the authority to run their respective businesses, the entire Amphenol organization is empowered to truly “think globally, but act locally.”. View our Sustainability Report to learn about our approach and progress on ...
Thermometrics CR1 High Performance Thermistor Coating for Harsh ...
Pressure (TMAP) Sensors, the CR1 Coating offers a unique combination of properties that can be used in many applications where moisture, high temperatures or chemicals can damage other thermistor coatings. Amphenol Advanced Sensors is a leading innovator in advanced sensing technologies and innovative
Patient Monitoring | Drug Delivery - amphenol-sensors.com
Thermometrics Adhesive Mounted Surface Sensors feature a surface mount cup for use as skin temperature sensors or on flat surfaces. They consist of small bead, disc or thermistor types <0.100" OD with shielded, jacketed or coaxial cable extension leads, as well as a maximum temperature rating of 140°F to 500°F (60°C to 260°C).
Telaire T3000 Series CO2 Sensors for Harsh Environments
Sensing Method Non-Dispersive Infra-Red (NDIR), single or dual wavelength. Power Supply Requirements 15 – 15Vdc ±10% 24 - 18-30 VAC RMS, 50/60 Hz, or 18 to 42 VDC,
lvpo1-bsfa-012 | Amphenol Global Search | Amphenol
Discover the RH5 high-performance rod-type sensors for precise position measurements in hydraulic or pneumatic cylinders. Operating temperature up to +85°C, pressure resistance up to 800 bar. ... Learn about the features and benefits of Amphenol's MIL-DTL-55302 Low Mating Force rectangular connector series, which meets military standards and ...
career opportunities | Amphenol Global Search | Amphenol
Amphenol Tecvox is a global leader in the design, development, and delivery of quality automotive connectivity solutions. Amphenol Tecvox has experience with world-class project-management techniques that can take any product from the drawing board to reality in a professional and cost-effective manner.
NPA Pressure Sensors for Respiratory Care - Amphenol
Amphenol Advanced Sensors NPA Pressure Sensors for Respiratory Care Product Spotlight The NovaSensor Pressure Amplified (NPA) Sensor is a surface mount pressure sensor provided in a miniature size as a cost-effective solution for respiratory applications that require calibrated performance. Housed in a 14-pin SOIC surface