Search Results for amphenol sensors
GE Advanced Sensors | Amphenol Global Search | Amphenol
Amphenol Advanced Sensors is a world leader in advanced measurement and sensor-based technology solutions. We design and manufacture precision instruments and systems that measure temperature, pressure, humidity and gas concentration for customers around the world in the Healthcare, Transportation and Industrial Markets. ... 551121A Model GE
TST-10 Turbidity Sensor - amphenol-sensors.com
Amphenol Advanced Sensors. Specifications Part Number TST-10 Rated Voltage DC 5V (between No #1 & Ground) Voltage Differential 2.7V ± 20% Test Method After testing voltage in water (0 NTU), voltage test in water (4000 NTU) (Turbidity level Calibration -> Master NTU standard liquid )
Surface-Mount Pressure Sensor Series - amphenol-sensors.com
Amphenol Advanced Sensors Subject: The NPA product series is provided in a miniature size as a cost effective solution for applications that require calibrated performance. Packaged in a SOIC14 pin surface mount, the NPA Series is available in Gauge, Absolute \ ´·v #OúzS ^+ C¯è¹Ph ã :¢pG OXä ½ ôm [@p ÀOc§ l° ÑJU&ìu»eß!JAu·i ...
Ring Terminal Temperature Sensor - amphenol-sensors.com
Amphenol Advanced Sensors . RTS Series Ring Terminal Temperature Sensors Mechanical Dimensions D1 L1 L2 D3 T L3 D2 Image M3 3.2 See dimensions drawing 6±2 4.5 1 16 7 (1) M4 4.2 6±2 5 1 20 8 (1) M5 5.2 6±2 5 1 20 10 (1) M6 6.4 6±2 5.6 1.2 25 14 (1) & (2) Dimensions
NovaSensor Fuel Particulate Sensors - GPF/DPF - Amphenol Sensors
At Amphenol Sensors, we make Quality, Safety and Environmental Protection a top priority. We believe that making sustainable choices in the way we conduct our business creates short-term and long-term value for our stakeholders. We do not create long-term value by merely complying with regulations, but we go beyond compliance to find ways to ...
About - All Sensors
Amphenol All Sensors Corporation is an industry leader in the design and manufacturing of ultra-low pressure sensors. All Sensors’ product line is notable for its high accuracy and repeatability. The sensors are particularly suited for low and ultra-low pressure applications for flow measurement and control. Ideal markets for All Sensors ...
NovaSensor NPI-15 Series - amphenol-sensors.com
Amphenol Advanced Sensors. NPI-15 Series dimensions NPI-15 Series Specifications Description The NovaSensor NPI-15 Series incorporates state-of-the-art IsoSensor technology, which gives the OEM user the best in price and performance. They are designed to operate in hostile environments and
Amphenol Completes Acquisition of MTS Systems
Amphenol expects the MTS Sensors business to add approximately $350 million in sales in the first twelve months after closing. As previously disclosed, MTS Sensors is expected to be $0.05 accretive to Amphenol’s earnings per share in the first twelve months after closing, which excludes acquisition-related expenses and reflects the Company ...
R290 Archives - Amphenol Sensors
At Amphenol Sensors, we make Quality, Safety and Environmental Protection a top priority. We believe that making sustainable choices in the way we conduct our business creates short-term and long-term value for our stakeholders. We do not create long-term value by merely complying with regulations, but we go beyond compliance to find ways to ...
Electric Vehicle Sensor & Battery Safety Resource Hub
Electric vehicles are no longer a pipe dream. They’re already here and are ushering in a new era in modern transportation the world over. Meeting the new demands of this new market for function and safety, Amphenol Advanced Sensors has developed sensor technology designed to keep electric vehicles of all sorts running at peak performance.
Air Quality Sensors | Humidity Transmitters - amphenol-sensors.com
TELAIRE T8700 | Relative Humidity & Temperature Transmitter . Telaire T8700 | T8700 is a precision humidity and temperature transmitter for HVAC control applications that uses Amphenol Advanced Sensors own ChipCap Sensor, allowing for quick and simple field replacement, negating the need to replace or return the complete transmitter for recalibration.
Patient Monitoring | Medical Instrumentation - amphenol-sensors.com
Thermometrics ZTP-315 Infrared (IR) Sensors consist of thermo-elements, flat infrared filter and a thermistor for temperature compensation, all in a hermetically-sealed TO-46 (18) package. Thermopile IR Sensors are used for non-contact, or infrared, surface temperature measuring.
Telaire SM-UART-04L Laser Dust Sensor - amphenol-sensors.com
Title: Telaire SM-UART-04L Laser Dust Sensor Author: Amphenol Advanced Sensors Subject: SM-UART-04L is a PM2.5 laser-based Particulate Dust Sensor that detects dust particle concentration in air by using an optical sensing method.
ZTP-315 | Thermometrics Infrared (IR) Sensors - amphenol-sensors.com
Thermometrics ZTP-315 Infrared (IR) Sensors consist of thermo-elements, flat infrared filter and a thermistor for temperature compensation, all in a hermetically-sealed TO-46 (18) package. Thermopile IR Sensors are used for non-contact, or infrared, surface temperature measuring.
Telaire T6615 Series CO2 Sensor - Amphenol Sensors
At Amphenol Sensors, we make Quality, Safety and Environmental Protection a top priority. We believe that making sustainable choices in the way we conduct our business creates short-term and long-term value for our stakeholders. We do not create long-term value by merely complying with regulations, but we go beyond compliance to find ways to ...
NTC Type MA - amphenol-sensors.com
Amphenol Advanced Sensors. NTC Type MA Specifications MA100 Designed for use in catheter assemblies, these sensors are available with nominal resistance values of 2252, 3000, 5000, and 10,000 Ω at 77°F (25°C). Close monitor-ing of manufacturing processes allow Thermometrics
SSI Technologies, LLC
Level Sensors. Whatever your media, tank depth, and profile, SSI Technologies, LLC most likely has an ultrasonic liquid level sensor for you. Our ultrasonic liquid level sensors use ultrasonic technology to generate a high-frequency sound wave to measure the time for the echo to reflect off of the target and return to the ultrasonic liquid level sensor.
CCT High-Pressure / Temperature Sensor - Amphenol Sensors
At Amphenol Sensors, we make Quality, Safety and Environmental Protection a top priority. We believe that making sustainable choices in the way we conduct our business creates short-term and long-term value for our stakeholders. We do not create long-term value by merely complying with regulations, but we go beyond compliance to find ways to ...