Search Results for amphenol-sensors.com
Contact Us | Amphenol Advanced Sensors
Interested in innovative technology by Amphenol Advanced Sensors? Send us a message and we'll put you in touch with an expert that's dedicated to finding the right solution for you. Markets Menu. Transportation. Industrial. Medical. Pharmaceutical . PRODUCTS. Temperature Sensors; Pressure Sensors; Air Quality Sensors ...
TELAIRE | CO2, HUMIDITY & DUST SENSORS - amphenol-sensors.com
As the world’s first and leading manufacturer of Non-Dispersive Infrared (NDIR) Carbon Dioxide (CO 2) Sensors, Telaire has been on the forefront of CO 2 sensors technology for over 25 years. Telaire holds 30+ awarded patents in CO 2 sensors, including the original automatic calibration algorithm - ABC Logic. In more recent years, Telaire has expanded its product line to include other air ...
About – Amphenol Sensors
Where Innovation Thrives Amphenol Sensors is a leader in innovative sensor technologies and forward-thinking measurement solutions built for a large variety of industries. We create value by providing critical information for real-time decisions. We offer domain expertise, rapid customization, world-class manufacturing capabilities and lasting customer relationships. We strive to give our ...
Ultrasonic Sensors – Amphenol Sensors
Ultrasonic Sensors Airmar With a highly experienced team of scientists, designers, engineers and technicians as well as a vertically integrated business model, Airmar has the capability of bringing innovative products from concept to production. Today, Airmar employs over 300 people worldwide and is dedicated to producing a diverse and innovative line of products to satisfy […]
Product Spotlights | Amphenol Advanced Sensors
Amphenol Advanced Sensors plays an important role in this application by providing highly accurate and robust assemblies using NTC thermistor technology for temperature measurement. Pressure Sensors for Respiratory Care | By NovaSensor. The NovaSensor Pressure Amplified (NPA) Sensor is a surface mount pressure sensor provided in a miniature ...
Automotive - Amphenol Sensors
Amphenol Sensors is a leading innovator in sensor technologies and measurement solutions. Offering the most diverse sensor portfolio of standard and customized products for the world’s most demanding regulatory and industry-driven applications, Amphenol creates value by providing critical information for real-time decisions. ...
Medical – Amphenol Sensors
Amphenol is a pioneer in the development of new and increasingly robust sensor technologies for medical applications. We offer innovative solutions, fast development cycles and excellent quality control to meet the most stringent requirements. ... At Amphenol Sensors, we make Quality, Safety and Environmental Protection a top priority.
Low Pressure Sensor Solutions | All Sensors
The Amphenol All Sensors AUAV series is a dual sensor specifically designed for the demanding requirements of Unmanned Aerial Vehicles (UAVs). This sensor combines a high-accuracy differential pressure sensors with Baraometric (Altitude) pressure sensor in a single package. Features: Compact and Lightweight Dual Sensors in a Single Package
Amphenol
Amphenol Advanced Sensors The AX221058S is a fully calibrated Hydrogen detection sensor designed for applications where battery thermal runaway events are a concern. The output of the sensor is a ratio metric analog output with a detection range of 0 to 16% H2 gas concentration. 1. Pin Description Pin Name Description 1 GND Ground
Amphenol
Amphenol Advanced Sensors AX222058 Relative Humidity, Temperature, Pressure and Hydrogen Concentration A combination sensor capable of providing up to four measurements including humidity, temperature, pressure and hydrogen concentration specifically for battery system applications. These measurements are
Temperature Sensors – Amphenol Sensors
Temperature Sensors Thermometrics, Inc. With more than 70 years of experience in the development, design and manufacture of high quality sensors, Thermometrics offers one of the most comprehensive ranges of temperature measurement and sensor products in the world today – NTC Thermistors, PTC Thermistors, Infrared (IR) Sensors, Current Limiters, Temperature Standards, and Temperature Sensor ...
ZTP-135SR Thermometrics IR Sensor - amphenol-sensors.com
Amphenol Advanced Sensors. Thermopile Chip Parameter Limits Units Condition Min Typ Max Chip Size 1.8 x 1.8 mm2 Diaphragm Size 1.4 x 1.4 mm2 Active Area 0.7 x 0.7 mm2 Internal Resistance 42 60 81 kΩ 25 °C Resistance T.C. 0.12 %./ °C Responsivity 43 62 81 V/W 500K, 1Hz
Temperature Sensors | NTC Thermistors - amphenol-sensors.com
CO2, Humidity & Dust Sensors. Moisture Meters. Thermal Validation & Monitoring. Thermometrics | NTC Thermistors. Thermometrics, Inc., offers a wide range of NTC Thermistors from component-level to complete sensor assemblies. They are manufactured from the oxides of transition metals and can operate over the range of -196°C to 1000°C ...
Contact - Amphenol Sensors
Contact Us Amphenol Sensors Headquarters Phone (814) 834-9140 Email sensors@amphenol-sensors.com Address 967 Windfall Road, St. Marys, PA 15857, US
Hydrogen Technologies - Amphenol Sensors
Leading the industry in Hydrogen Technologies Go Back Amphenol Sensors is a leading innovator in sensor technologies and measurement solutions. Offering the most diverse sensor portfolio of standard and customized products for the world’s most demanding regulatory and industry driven applications, Amphenol creates value by providing critical information for real time decisions. Amphenol ...
Thermometrics Archives - Amphenol Sensors
At Amphenol Sensors, we make Quality, Safety and Environmental Protection a top priority. We believe that making sustainable choices in the way we conduct our business creates short-term and long-term value for our stakeholders. We do not create long-term value by merely complying with regulations, but we go beyond compliance to find ways to ...
Ventostat T8041/T8042 CO2 Duct Probe Transmitter | Telaire
CO 2 transmitters can be used in a broad range of applications including air quality monitoring in buildings.; CO 2 concentration levels in buildings are monitored to provide an indication of occupancy and to drive a ventilation control strategy. An effective DCV (Demand Controlled Ventilation) strategy will conserve energy and maintain indoor air quality.
Locations | Amphenol Advanced Sensors
Amphenol Advanced Sensors has locations around the globe with domain expertise, world-class manufacturing capabilities, exceptional technical support, and service to match. Americas . St. Marys, PA, USA (Corporate Headquarters) Amphenol Thermometrics, Inc. 967 Windfall Road
Thermometrics NTC Type 95 Series Thermistors - amphenol-sensors.com
Amphenol Advanced Sensors. 2 Type DC95 Specifications Description Epoxy-coated interchangeable NTC thermistor chips with bare tinned copper lead wires. Options Consult Factory for Availability of Options: • Other resistance values in the range of 1000 Ω to