Search Results for another tesat
Sensor overloading tech tip - Wilcoxon Sensing Technologies
Another test method is to use a “mechanical filter,” such as a piece of rubber or even a business card, which can be temporarily placed between the sensor and machine. This type of mechanism will filter out much of the high frequency vibration which may be overloading the sensor.
IMPACT AND DROP TESTING - PCB
A simple test method of measuring impact force versus displacement, and then integrating for the area under force-displacement curve provides an output in energy units.
Dynamic Strain Sensors and Accelerometers for Structural Testing
The main results of the test campaign will be shown, where both strain sensor and accelerometer measurements are processed simultaneously, resulting in the strain and displacement mode shapes, respectively.
How Sensor Mounting Affects Measurements - PCB
another analyst is getting different results than they are when they are seemingly making the same measurements, particularly with overall measurements. To help address this problem, the General Motors
Sensor overloading - Wilcoxon Sensing Technologies
Another test method is to use a “mechanical filter,” such as a piece of rubber or even a business card which can be temporarily placed between the sensor and machine. This type of mechanism will filter out much of the high frequency vibration which may be overloading the sensor.
Sensor overloading - Wilcoxon Sensing Technologies
Another test method is to use a “mechanical filter,” such as a piece of rubber or even a business card which can be temporarily placed between the sensor and machine. This type of mechanism will filter out much of the high frequency vibration which may be overloading the sensor.
Accelerometers: Hermetic sealing and helium leak testing
Wilcoxon industrial sensors have the highest hermetic seal rating in the industry. Wilcoxon uses the Helium Leak Test (HLT) to qualify the sealing of all sensor designs and maintains a continuous monitoring program to ensure the proper sealing of all hermetically rated accelerometers.
AE-AN-TR-014-TR Multicoax Series TR to TR - Amphenol Ardent Concepts
Further in the design and test, one may now want to connect the same board to another board to show overall system compliance. Since the footprint is the same one can simply use the TR to TR when needed to connect the test board to another for compliance test.
Design and Construction of the VPX Connector - Amphenol Aerospace
TCS to develop the VITA 46 R-VPX connector. The Amphenol Aerospace R-VPX connector meets or exceeds all of the requirements called out in VITA 46 and Tel. cordia GR-1217-CORE-i02 test specifications. Amphenol has also proven the R-VPX connector is fully intermateable and intermountable with TE Connec.
Streamlined Test Setup with TEDS Technology - PCB
Using the same simple two-wire electrical connection, these smart sensors are now able to identify themselves over a network, allowing completely self-configurable transducer setup. This paper describes how to efficiently use TEDS technology on large multi-channel structural tests, such as modal analysis.
gpib connector | Amphenol Global Search | Amphenol
Amphenol shielded GPIB cables are designed to exceed the latest IEEE-488 specifications and will connect to any GPIB/HPIB controller, test instrument, or daisy-chain to another GPIB cable. Buy 0.3m Amphenol GP-IE156327SS-000.3 Cables Direct from the Factory at Cables on Demand.
Troubleshooting accelerometer installations - Wilcoxon Sensing Technologies
Testing ensures data integrity and can identify most commonly occurring problems. The troubleshooting techniques presented are very simple and can be performed using most monitoring systems and data collectors or simple test equipment. Many installation and sensor problems can be detected by measuring the bias voltage of the sensor.
High Sensitivity Accelerometers to Monitor Traffic and Railroad ...
PCB ® manufactures sensors used by design engineers and predictive maintenance professionals to test and measure vibration, pressure, force, acoustics, load, and shock in research and development as well as industrial applications.
AE-AN-SK-008 - SK SERIES - PCB FOOTPRINT AND MOUNTING SPECIFICATIONS
Our contact sets provide the fastest, most electrically efficient connection thanks to the utilization of dual sided compression mount technology. In our SK SeriesTM sockets these contacts are housed within the interface portion of the socket. They are the electrical connection bridging the gap between the device under test and the PCB below.
4-20 mA vibration monitoring of chillers & cooling units
However, there are two methods to make a 4-20 mA vibration signal available to the PLC system. Traditional dynamic Integrated Electronic Piezoelectric (IEPE) accelerometers can be wired through a signal conditioning vibration transmitter module to create 4-20 mA output.
GPIB Cables - Shielded GPIB Cable for Sale | Cables on Demand - Amphenol
Amphenol shielded GPIB cables are designed to exceed the latest IEEE-488 specifications and will connect to any GPIB/HPIB controller, test instrument, or daisy-chain to another GPIB cable.
Vibration monitoring of pumps - Wilcoxon Sensing Technologies
Here is a quick guide to cut through some of the complexity. Accelerometers should be mounted on or near the stuffing box in the horizontal direction, coincident with the suction or discharge piping; a second measurement should be made at 90° from that.
Sensor Calibration Global Service Centers - PCB
PCB’s offers a range of factory calibration services for accelerometers, dynamic pressure sensors, microphones, and forces sensors.
Fundamentals of Torque- tension and Coefficient of Friction Testing - PCB
a torque-tension test and at times a coefficient of friction test. The torque-tension test usually consists of an acceptance input torque window at a specified tension or clamp load value, while the coefficient of friction test requires an acceptance coefficient of friction window (typically the reference coeffi.
Troubleshooting accelerometer installations - Wilcoxon Sensing Technologies
Testing ensures data integrity and can identify most commonly occurring problems. The troubleshooting techniques presented are very simple and can be performed using most monitoring systems and data collectors or simple test equipment. Many installation and sensor problems can be detected by measuring the bias voltage of the sensor.