Search Results for army points
4U6VT360X06F xys5 - Amphenol Antenna Solutions
Always attach the antenna using all mounting points. Do not install the antenna with the connectors facing upwards. BOTTOM VIEW - CONNECTOR DIAGRAM OMNI 24.0 IN FIXED TILT. REV121721NA ACROSS THE WORLD. AROUND THE CORNER. www.amphenol-antennas.com 7 of 17
R-VPX Evolution 2.0 VITA 46.30 Connectors - Amphenol Aerospace
Improving off original Vita 46 standards, Amphenol’s R-VPX Evolution 2.0 is the next generation of high-speed ruggedized backplane connectors. R-VPX Evolution 2.0 series connectors are designed and optimized to achieve data rates in excess of 25 Gb/s, meeting VITA 46.30 requirements.
Push Pull Connectors | Products | Amphenol Aerospace
Amphenol circular push/pull connectors are the industry-standard locking connector with quick disconnect features.
PCTEL Expands Industrial IoT Portfolio with Wireless Communication ...
BLOOMINGDALE, Ill.--(BUSINESS WIRE)--Aug. 12, 2020-- PCTEL, Inc. (Nasdaq: PCTI), a leading global provider of Industrial IoT (IIoT) antennas and purpose built, application specific devices, today announced the expansion of its IIoT portfolio with its new wireless communication sensor platform. The integrated wireless communication sensor platform includes a battery-powered wireless sensor ...
PCTEL and Ranplan Streamline Next-Generation Indoor Network Planning
SeeHawk ® Central Automated Workflow Management Platform; SeeHawk ® Collect Software; SeeHawk ® Reports Software; SeeHawk ® Touch Software
ENGINEERING REPORT EWOM - アンフェノールジャパン株式会社
associated contacts in figures 3.5-3, 3.5-4, & 3.5-5 from J3, column 8 shows points of wear through the gold to the nickel. There is some minor intrusion to the copper layer on the wafer, but the wear does not extend through the nickel. There is no wear thru of the nickel on the backplane contacts. Appendix B contains all the SEM EDS maps taken.
CDQ012 conflict minerals policy - amphenol-invotec.com
At this point, Amphenol Invotec can advise that to the best of our knowledge none of our products contain Coltan, Tantalum or Tungsten. We can however also confirm that based on the surface finish specified by our customers, our products may contain Tin and / or Gold.
Features - Amphenol Antenna Solutions
Always attach the antenna using all mounting points. Do not install the antenna with the connectors facing upwards. BOTTOM VIEW - CONNECTOR DIAGRAM OMNI 24.0 IN FIXED TILT. MOUNTING KITS Select from the following mounting options when ordering. Mounting kits for canister antennas are ordered as a separate line item.
ACCESS PORT DESCRIPTION (CONNECTORS)
Mechanical Distance Between Mounting 0 mm (Only one point) Wind Load (at 150 km/h) Calculation 150 km/h Frontal 40 N Rear 55 N Lateral 13 N Operational Wind Speed 160 km/h Survival Wind Speed 200 km/h Radome color White Radome Material UPVC SHIPPING (8 in 1 Box) Dimensions 1120 mm x 310 mm x 340 mm Weight 15 kg Volume 0.11 m³ 2-Port Antenna ...
PROTIMETER - amphenol-sensors.com
laborious and impractical process for surveying a building, for it would take several hours at each point. Protimeter Readings Are Meaningful Fortunately this is not the only method. The relative readings of a Protimeter moisture meter measure only the
R-VPX Evolution 2.0 VITA 46.30 Connectors | R-VPX VITA 46 Connector ...
Improving off original Vita 46 standards, Amphenol’s R-VPX Evolution 2.0 is the next generation of high-speed ruggedized backplane connectors. R-VPX Evolution 2.0 series connectors are designed and optimized to achieve data rates in excess of 25 Gb/s, meeting VITA 46.30 requirements.
696-900 / 696-900 MHz - Amphenol Antenna Solutions
2-Point Mounting and Downtilt Bracket Kit 36210006 40-115 mm 1.6-4.5 in 4.1 kg 9 lbs 696-900 / 696-900 MHz Quoted performance parameters are provided to offer typical, peak or range values only and may vary as a result of normal testing, manufacturing and operational conditions. Extreme
696-960 / 696-960 MHz - Amphenol Antenna Solutions
3-Point Mounting Bracket Kit Antenna cannot be mechanically downtilted. MKS09P04 50-115 mm 2.0-4.5 in 14.5 kg 32 lbs s 696-960 / 696-960 MHz QUAD334C0000 x Twin Band | Quad Port | Panel Antenna | (2x) X-Pol | 33° / 33° | 15.3 / 15.3 dBi | Variable Tilt Quoted performance parameters are provided to offer typical, peak or range values only and ...
696-960 MHz - amphenol-antennas.com
3-Point Mounting Bracket Kit MKS09P02 50-115 mm 2.0-4.5 in 4.1 kg 9 lbs 3-Point Mounting & Downtilt Bracket Kit MKS09T02 50-115 mm 2.0-4.5 in 6.4 kg 14 lbs s 696-960 MHz CX063X25 x00 Single Band | Panel Antenna | X-Pol | 65° | 16.8 dBi | Variable Tilt Quoted performance parameters are provided to offer typical, peak or range values only and ...
Amphenol Network Solutions > Product
Your shopping cart is empty. Product Qty Amount; From: Until:
Amphenol Network Solutions > Products > Cable Management > WaveTrax ...
The two-inch WaveTrax to FiberGuide Trough Adapter connects WaveTrax trough to FiberGuide and most other manufacturer's legacy raceway systems. The snap-together WaveTrax raceway system from Amphenol Telect reduces time spent on installations and retrofits.
MIL-DTL-38999 Series II - JT Connectors - Amphenol Aerospace
Amphenol® MIL-DTL-38999 Series II Connectors were developed to meet the needs of the aerospace industry and provided the impetus for the development of the MIL-C-38999 specifications, which later was superseded by MIL-DTL-38999.
Level Plus - Temposonics
pulse and converts it to an electrical pulse. The distance from a reference point to the float is determined by measuring the time interval between the initiating current pulse and the return pulse and precisely knowing the speed of these pulses. The time interval is converted into a pro-portional 4 to 20 mA loop output signal. Figure 2.2