Search Results for as_path
M4244 SERIES - amphenol-aerospace.com
This pin is used as a return path for SYNC IN, SYNC OUT and INHIBIT IN. ared Sibrava | +1 (607) 643-1845 | jsibravaamphenol-aao.com amphenol-aerospace.com 7 TYPICAL CONNECTION DIAGRAM Single Converter Operation Parallel connection operation. ared Sibrava | +1 (607) 643-1845 | jsibravaamphenol-aao.com
AirMax VSe 25GB/S BACKPLANE CONNECTOR SYSTEM - Amphenol CS
path for up to 25Gb/s per differential pair with the flexibility of an open pin field design. The connectors also feature backwards mating-compatible interfaces to existing AirMax VS® connectors with minimal changes to connector footprints. The connectors combine FCI technologies for a shieldless
LNA-GPS line amp-... - AMPHENOL PROCOM
DC path between output and input: Add to quote: Application Example 1: How to connect the LNA-GPS line amp-SMA-SMA as preamplifier for a passive GPS antenna to compensate high loss in long coax cable downleads. DC supply voltage is inserted on the signal line at the GPS receiver by the junction box JB1-1G (to be ordered separately). ...
HF 5000 - AMPHENOL PROCOM
Land installations. In land installations, we recommend the vertical HF 5000 antenna to be mounted on a short ø45 - 65 mm mast tube which either is driven 6 - 8 feet in the ground or cast into the ground, to be able to cope with the occurring antenna wind load at the particular location.The free height of the mast tube shall be a few feet above the ground.
HF 5000 - AMPHENOL PROCOM
Land installations. In land installations, we recommend the vertical HF 5000 antenna to be mounted on a short ø45 - 65 mm mast tube which either is driven 6 - 8 feet in the ground or cast into the ground, to be able to cope with the occurring antenna wind load at the particular location.The free height of the mast tube shall be a few feet above the ground.
Connector series M12x1 X-coded | NOW also available as version with ...
Therefore it is possible to completely map the transmission path of a device installed in the field and the associated processing unit using CONEC connectors. NEW * NEW * NEW with M12 bayonet quick locking. For applications that require connectors that can be securely locked without visual contact or tools, CONEC offers one connector field ...
HDLC Series Connector Assemblies - TPC Wire
P urpose ly built to withstand the most challenging industrial conditions. It maintains identical shell dimensions, contact layouts, and electrical performance characteristics as the standard MIL-C-5015 connector while incorporating application-specific enhancements like the 3/4 turn reverse bayonet coupling system, rubber-coated coupler, and a robust strain relief system.
conec connector | Amphenol Global Search | Amphenol
The connector series includes socket connector versions incl. SMT and THR variants, a field attachable connector with crimp termination as well as overmoulded axial and angled connectors. Therefore it is possible to completely map the transmission path of a device installed in the field and the associated processing unit using CONEC connectors.
AirMax VS2 BACKPLANE CONNECTOR SYSTEM - Amphenol CS
AirMax VS2® connectors provide a migration path from AirMax VS® for speeds up to 20Gb/s, providing margin of safety for typical 802.3ap system performance with the flexibility of an open pin field design. The connectors leverage AirMax VS® and VSe® design features and technology to achieve improved
airmax vr | Amphenol Global Search | Amphenol
Next-generation AirMax VSe ® connectors provide a migration path for up to 25Gb/s per differential pair with the flexibility of an open pin field design. The connectors also feature backward mating-compatible interfaces to existing AirMax VS. 10122665-101LF.
Glossary of RF Terms - Amphenol RF
The measure of how much better a material is than air as a path for magnetic lines of force. Air is assumed to have a permeability of 1. Permittivity Relative Synonym term for relative dielectric constant Er. Phase Shift Change in phase of a voltage or current after passing through a circuit or cable.
HF 5000 - AMPHENOL PROCOM
Land installations. In land installations, we recommend the vertical HF 5000 antenna to be mounted on a short ø45 - 65 mm mast tube which either is driven 6 - 8 feet in the ground or cast into the ground, to be able to cope with the occurring antenna wind load at the particular location.The free height of the mast tube shall be a few feet above the ground.
10124588 | Amphenol Global Search | Amphenol
The ExaMAX ® high-speed orthogonal connector system is designed to enable superior 25Gb/s electrical performance and provide a path to 56Gb/s in anticipation of further increases in bandwidth requirements. The 6-Pair orthogonal right-angle header connector solution further expands the range of applications supported by the ExaMAX ® connector ...
5G Networks Brochure 2024 | Amphenol
family for a seamless upgrade path to 224Gb/s. UltraPass™ OverPass™ Cable . Assemblies. 224G CONNECTION DIRECTLY FROM CHIP . SITE TO EXTERNAL PORTS. UltraPass™ enables arrayed connector layouts . for near-chip and on-package IO solutions, providing the highest differential pair count .
401–00 4-Wire Line Amplifier - Charles Industries
3.2 Transmit Voice Path Voice energy from the drop equipment or facility enters the 401–00 on T (pin 55) and R (pin49) and is processed as in the receive path description of the preceding paragraphs. Subsequently, it exits the 401–00 via Tl (pin 41) and R1(pin 47) which are connected to the facility transmit pair. 3.3 SX Lead Signaling Path
The Fastest Path to Wireless Charging with Amphenol and NuCurrent
The need for a streamlined and efficient upgrade path for existing Qi Certified products has never been more urgent and customers can look forward to a hassle-free transition to the new standard. Tags: Wireless Charging Wireless Power Qi Qi2 NuCurrent. Latest. Edge Computing: ...
cpc s2s connector | Amphenol Global Search | Amphenol
The Omni-Path verified DAC copper cables, in collaboration with Intel, are offered to address the needs of the majority of the inter-cabinet and short reach intra-cabinet cable connections while minimizing cable bulk and cable routing issues.
HF 7500-3 - AMPHENOL PROCOM
ATU. The ATU shall be mounted on the mast tube with the antenna terminal upwards, just below the bottom end of the antenna whip. The HF 7500-3 antenna feeder connection and the ATU antenna terminal are connected as direct as possible with a short open feeder wire, which in fact is a single piece of medium-gauge copper wire, self-supported or supported by some porcelain insulators.
SUSTAINABILITY REPORT - Amphenol
2021 and we are on the path to achieving the remaining six goals with a target of 2022. We also began evaluating our decarbonization strategy and took steps to increase the percentage of our electricity sourced from renewables while simultaneously shifting more of our non-renewable fuel consumption toward natural gas and away from diesel.
pctel | Amphenol Global Search | Amphenol
With PCTEL’s automated network testing solution, you can ensure in-building communications coverage while saving time and money. Test multiple public safety, cellular, and private networks simultaneously using grid or path-based methods.