Search Results for bwc means
Amphenol Connector Basics Terminology Guide - amphenol-aerospace.com
Extraction/Removal Tool - A handheld tool used for removing a contact from a connector. Fiber Optic Termini - Comparable to electrical pin and socket contacts, except they transmit data optically through fibers instead of electrically through wires. Connector: A device providing electrical or signal connection. It consists of a plug and receptacle.
Glossary of RF Terms - Amphenol RF
Direct Current (DC) An electric current which flows in only one direction. Dissipation Unusable or lost energy, such as the production of unused heat in a circuit. Distortion An unwanted change or addition to a signal or waveform when it is amplified. This definition excludes noise which is an extraneous signal super-imposed on the desired signal.
High Voltage Wire Connector | High Voltage Connector Designers
Silicone over-molded connectors: Our knowledge of, and equipment for, silicone over-molding ensure optimal bonding with silicone jacketing on HV wire to help create small, flexible, and capable HV cable assemblies Multiple latching options: Ensuring secure connections through various means, including: Friction-fit Wire snap-latch Quarter-turn ...
Connectors | Products | Amphenol
Amphenol has been designing and manufacturing electrical and electronic connectors since the company’s inception in 1932. For nearly a century, we’ve been helping customers transmit power, data and signal in the harshest environments, from subsea applications to the outer reaches of space and everywhere in between.
BNC Adapters - Amphenol RF
Amphenol RF offers a wide array of both in-series and between-series BNC adapters in straight and right-angle configurations. 50-ohm and 75-ohm impedance BNC adapters are available with and without panel mounting features.
Current control acc. to UL 2367 - Lutze
As a 'Supplementary Protection Device', the LCOS-CC is an intelligent solid state relay circuit breaker that prevents wires and connected devices from overloading and short-circuiting. LÜTZE offers the current control LCOS-CC in two different versions: as a 1-channel, and a 2-channel version.
Below Grade Enclosure Selection Guide - Charles Industries
Amphenol Charles Industries delivers superior protection solutions for underground equipment and buried network components. We ofer a wide selection of enclosures to safely house fiber optics, meter/junction boxes, wireless network materials, trafic signals, and more.
Compact Connectors for Advanced True Wireless Stereo Technology
With the advent of Bluetooth technology, earbuds for audio began to mark such a change, and the term “True Wireless Stereo (TWS) gained popularity with this. But, what does this really mean? What is the technology behind this? And how does Amphenol support this advanced design and technology? Let’s
Conformal Sensor Measures Ammunition Pressure Through Cartridge Case - PCB
Sensor Measures Ammunition Pressure Through Cartridge Case The conformal ballistic pressure sensor was developed out of a need to standardize and improve measure. Inc. Bob Metz, Director, PCB Aerospace & Defense Division The conformal sensor measures ammunition gun cham.
Problems Faced During Application - ardentconcepts.com
Problems Faced During Application A major defense contractor needed a reliable, high speed (12 Gbps) connector solution that would allow them to easily replace or upgrade expensive Circuit Card Assemblies (CCA’s). These CCA’s were mounted to a motherboard and had a number of expensive components and IC’s like FPGA’s. Each motherboard contained 9 of these CCA’s. Soldering to the ...
Repair and Maintenance Returning Equipment Contact Information ... - PCB
calibration and battery replacements where applicable, our products require no user maintenance. Clean electrical connectors, housings, and mounting surfaces with solutions and techniques that will not harm the material of construction. Observe caution when using liquids near devices that are not hermeticall
IEWC Global Solutions - Gemeco
IEWC offers an unparalleled customer experience that supports the success of your projects and helps ensure the growth of your company. Keep up-to-date on product news and the latest offers.
Examining Type SH, Type MV, Concentric Neutrals Medium ... - TPC Wire
Concentric neutrals are a design feature that can be incorporated into medium voltage cables to enhance their electrical performance, particularly in long-distance power transmission scenarios. The choice of cable type depends on the specific requirements of the electrical system and the application at hand.
What is Insertion Loss and how is it specified? - Amphenol RF
Insertion Loss, expressed in dB is defined as 10*log (Po/Pi) where Po= Power Out and Pi=Power In. There are 3 main causes of Insertion Loss: Reflected losses are caused by the VSWR of the connector. Dielectric losses are caused by the power dissipated in the dielectric materials (Teflon, rexolite, delrin, etc.).
Model 1408-02ADB FATIGUE RATED LOW PROFILE LOAD CELL, DUAL BRIDGE ... - PCB
g figure and table give the general outline dimensions of the dual bridge fatigue-rated load cells. Dual bridge fatigue-rated load cells manufactured by PCB Load and Torque, Inc. are guaranteed to last 100 million fully reversed cycles (full tension through full compression). These load cells feature high accuracy with resistance to off-center loading, extraneous bending and side-loading ...
Digital Temperature Sensors vs. NTC Thermistors
From Thermometrics, Inc., learn more about the features, benefits and common applications of Digital Temperature Sensors versus NTC Thermistors. NTC Thermistors – NTC stands for Negative Temperature Coefficient, meaning they reduce in impedance as temperature increases resulting in an analog voltage which varies with temperature.
Basic Definitions - Accelerometers - PCB
Acceleration is the rate of change of velocity. Measurement units for acceleration include m/s2, ft/s2, and g. An accelerometer is a sensor, or transducer, which is designed to generate an electrical signal in response to acceleration (or deceleration) that is applied along (parallel with) its sensitive axis.
HOW RUGGED ELECTRICAL WIRE & CABLE CAN HELP BOOST ROI IN YOUR OPERATIONS
TPC Wire and Cable products have a jacket that is 25% thicker and doesn’t support combustion, which means our jackets actually dissipate heat, concentrating the impact strictly on the affected part of the cable.
Wireless networks need to gear up for more than IOT - amphenol-ns.com
Mark Zuckerberg and Elon Musk are betting on it. Two weeks ago, Zuckerberg — better known as the CEO of social media giant, Facebook — said at the F8 Conference in San Jose that we won't be using phones, tablets, TVs or anything else with a screen by 2026. Data will instead be projected straight into our eyes as we type with our brains. We'll be wearing Facebook-developed and branded smart ...
General Piezoelectric Theory - PCB
To generate a useful output signal, our sensors rely on the piezoelectric effect. ("Piezo" is a greek term which means "to squeeze.") When the piezoelectric elements are strained by an external force, displaced electrical charge accumulates on opposing surfaces.