Search Results for charles barkley new deal
Charles 4”x9” Fiber Splice Trays - Charles Industries
Charles Fiber Splice Trays accommodate up to 24 single fusion splices, two mass fusion splices (12 fiber ribbons) or up to 12 mechanical splices per tray. The tray’s unique design allows it to be removed from the pedestal without disturbing previously spliced fibers, providing technicians greater flexibility when
Disturber_Mitigation_Application_Note r2
attention to this disturbance issue, as the “upgrade” to new services could actually downgrade their existing ones. Example – RT DSLAM Deployment ... Charles Industries, Ltd. 5600 Apollo Drive Rolling Meadows, Illinois 60008-4049 Telephone: 847.806.6300 FAX: 847.806.6231.
Buried Cable Pedestal Installation Instructions - Charles Industries
CPLS (Charles PEDLOCK Splice) CPLM (Charles PEDLOCK Magnum) Note: Failure to follow this procedure could result in the pedestal not performing properly. Step Action 1. Remove the dome and backboard or bracket from the pedestal and set them aside for later use. If not already installed, seat the drop wire channel into the stays inside the base.
CMPH CROSS-CONNECT SERIES INSTALLATION GUIDE Section CMPH-75CC-801
030-300377 Rev. A Section CMPH-75CC-801 − CMPH CROSS-CONNECT SERIES INSTALLATION GUIDE − 0905I1P1 2 8. Find and remove red plastic bag.Remove the red bag labelled “moisture barrier ” hanging on one of the frame’s splice bars or brackets.Set it aside for later use. 9. Charles offers some CMPH models which include Optional - Replacement or rehabilitation mountings only.
Charles Mounting Kit 97-002549x-A General ... - Charles Industries
Charles Industries’ SH52-48xxxx series. Figure 1 shows the kit components . Hardware is not pictured. -NOTE- Hereafter, the Charles 97-002549x-A mounting kit will be referred to as the kit.
Charles Fiber Splitter Trays (CFST) - Charles Industries
Distribution Optical (BDO) pedestals; or fiber cabinet such as the Charles Fiber Interconnect Terminal (CFIT), Charles Fiber Building Terminal (CFBT) or a Charles Universal Broadband Enclosure (CUBE). The splitter tray kit includes a PLC splitter mounted in either a 4”x6” or 4”x9” Charles Fiber Splice Tray.
3603-02 and 3603-32 Line Interface Units Mode 3 ESF (LIU–3E)
The Charles Industries 3603-02/32 Line Interface Units (LIU-3E) are common equipment plug–in units for the Charles Industries 360 and 363 D4 Digital Carrier Terminals (also known as channel bank assemblies). The 3603-02 (Equipment Issue 2) is functionally identical to 3603-32 and differs only in front-panel screening and mounting orientation.
Charles Universal Broadband Enclosure CUBE-RL21221AH5 General ...
Charles Industries’ Universal Broadband Enclosure (CUBE ) product line that is not included in the family document, LT -RL21221xxx. Figure 1 shows a closed front view of the enclosure. -NOTE- Hereafter, the Charles Universal Broadband Enclosure CUBE- 21221AH5 will
Charles Fiber Pedestal Replacement Parts
Charles Fiber Pedestal Replacement Parts Replacement parts and ancillary items for Charles BDO-EG and CFDP Series Fiber Buried Distribution Pedestals BDO-EG Series Pedestal Parts Component Description BDO203-EG BDO204-EG BDO205-EG BDO 6-EG Dome, outer (A) Dome, for square base, self latching lock, 811 warning label
Fiber Rack Solutions (CFRS) - Charles Industries, LLC
Charles Fiber Rack Solutions (CFRS) provide flexible, multi-functional panels for patch, splice and splitter requirements within virtually any application. The efficient design of the splice area and bulkhead allows for maximum density while using just 1RU, 2RU or 4RU of valuable rack space.
Charles Replacement Door Kit 97-MP1412FLPUDK General Description and ...
The new door has a hinged door panel to access the interior of the CUBE. Figure 1 Kit Door . LT-MP1412FLPUDK Page 2 of 3 1 st Printing 2. INSTALLATION 2.1. Inspecting the Product The kit is shipped in a carton. Unpack the unit and dispose of the packaging material. ... The Charles warranty is limited to the operation of the CUBE
www.charlesindustries.com
www.charlesindustries.com
Z24 High Heat Node Pedestal Housings - Charles Industries, LLC
New R-PHY optical nodes are being engineered to dissipate 160Watts of power; significantly greater than prior generations of pedestal housings were designed to accommodate. Pedestals that cannot accommodate 160W can result in network outages or shorter equipment lifespans due to over-heated equipment.
ADRENALINE DISTRIBUTION INTERFACE INSTALLATION GUIDE
See Table 1 to perform a new CMPH enclosure installation (without AdrenaLine units). See Table 4 to install line-powered AdrenaLine units inside the CMPH. Table 3 describes a new CMPH installation with stakes. For replacement or rehabilitation application instructions , call Charles for more details.
STS 3192–9B Bridging Office Repeater Installation Guide
Charles Industries, Ltd. offers a standard repair or exchange service for units either in- or out-of-warranty. With this service, units may be shipped to Charles Industries for either repair and quality testing or exchanged for a replacement unit, as determined by Charles Industries. Follow the Repair Service Procedure below to return units
Charles Universal Broadband Enclosures (CUBE) RL 2003 Series
Charles Universal Broadband Enclosures (CUBE) RL 2003 Series INNOVATIVE ENCLOSED SOLUTIONS™ Charles Industries, Ltd. Phone: (847) 806-6300 Fax: (847) 806-6231 Web: www.charlesindustries.com For additional product information, please visit www.charlesindustries.com All measurements in inches. OG-OSP028-K16
Charles Universal Composite Pad (CPAD)
INNOVATIVE ENCLOSED SOLUTIONS™ Charles Industries, LLC An Amphenol Company Phone: (847) 806-6300 Fax: (847) 806-6231 Web: www.charlesindustries.com Charles Universal Composite Pad (CPAD) Lightweight Buried Mounting Pad for Standby Generators 2-Bay Modular Macro Pad 2-Bay Modular Macro Extension Pad Conjoined Pad and Extension Pad ANCRKT (18 ...
Z24 Generation II Low-Profile Housing with Extended Depth Base
Charles Thermal Management Experts are available to consult with you on your specific application’s heat dissipation needs, including thermal modeling of equipment as would be housed. Please contact your account representative for details. Z24 Generation II Low-Profile Housing with Extended Depth Base Pedestal Housing for Next Generation CATV ...
Charles Composite Mounting Pads - Charles Industries
charlesindustries.com q (LEVPIW.RHYWXVMIW 11(½&PP7MKLXW7IWIVZIH½TIGMûGEXMSRWYFNIGXXS(LERKI D-OSP175-I24 Product Dimensions CPAD-S0BUNI2014 CPAD-S1BUNI2629
4 3 2 1 - charlesindustries.com
charles industries, ltd. www.charlesindustries.com 9.00 ground line 39.35 14.0 26.2 29.5 17.0 3.5 27.8 12.8 23.7 9.2 16.6 34.5 this is the property of charles industries ltd. and shall not be.125 cmph-75sfn-cl 1 of 2 reproduced, copied or used in any manner detrimental to their interests. a cmph-75sfn/cl size b 1 note: requires two mounting stakes