Search Results for coaxial cable inner
Coaxial Cable Guide - Amphenol RF
A coaxial cable, often referred to as coax cable, is a type of electrical cable that consists of a central conductor, an insulating layer, a metallic shield, and an outer insulating layer. It is commonly used for transmitting radio frequency (RF) signals, video signals, and data signals.
ICA12-50JPL - 1/2" ClearFill - RFS Technologies
RFS Technologies coaxial cable's solid inner and outer conductors virtually eliminate intermods. Intermodulation performance is also confirmed with state-of-the-art equipment at the RFS Technologies factory.
LCF12-50J 1/2" CELLFLEX® Low-Loss Foam-Dielectric Coaxial Cable
CELLFLEX® coaxial cable's solid inner and outer conductors virtually eliminate intermods. Intermodulation performance is also confirmed with state-of-the-art equipment at the RFS Technologies factory.
LCF12-50JFN - 1/2" CELLFLEX - RFS Technologies
CELLFLEX ® coaxial cable's solid inner and outer conductors virtually eliminate intermods. Intermodulation performance is also confirmed with state-of-the-art equipment at the RFS Technologies factory.
ABS Coaxial Cable Product Information Sheet Type: T10625JB
Cable Ordering Information Part Number Description NEC / CE Listing 750625JB00BK00100001 T10625JB Characteristics Material Detail inches mm Inner Conductor Copper Clad Aluminum 0.136 3.45 Dielectric Foamed Polyethylene 0.563 14.3 Outer Conductor Seamless Aluminum Tube 0.625 15.9 Floodant Underground --- ---
L-2092-N.fm - Amphenol Aerospace
the inner coaxial portion of the cable. A. 1. Slide outer crimp ferrule over cable inner jacket as shown. 2. Strip cable inner jacket and inner flat braid as illustrated. Ends must be cut cleanly and at right angles to the axial plane of the cable. The cable must not be deformed while making cuts. 3. Carefully unravel and flare the inner flat ...
ABS Coaxial Cable Product Information Sheet Type: TX10860JB
Cable Ordering Information Part Number Description NEC / CE Listing 750860JB00BK00100001 TX10860JB Characteristics Material Detail inches mm Inner Conductor Copper Clad Aluminum 0.203 5.16 Dielectric Foamed Polyethylene 0.828 21.0 Outer Conductor Seamless Aluminum Tube 0.860 21.8 Floodant Underground --- ---
Braided Cables RG 58 A/U-XLL - AMPHENOL PROCOM
RG 58 A/U-XLL is a ultra low loss coaxial cable. The inner conductor consist of stranded bare copper wires and the cable has a double braid shield. The jacket material is flame retardent. All used materials are free of halogens. ECE R118.02 approved cable. Max. HF-power/W.
CELLFLEX® 1/2 low loss flexible cable; flame retardant/ halogen free ...
CELLFLEX® coaxial cable's solid inner and outer conductors virtually eliminate intermods. Intermodulation performance is also confirmed with state-of-the-art equipment at the RFS Technologies factory.
What’s the Difference Between 50 Ohm and 75 Ohm Coaxial Cable?
It is the coaxial cable’s physical characteristics that will determine its impedance. According to Wikipedia, “The characteristic impedance of the coaxial cable (in Ohms) is determined by the dielectric constant of the inner insulator and the radii of the inner and outer conductors.”
Braided Cables RG 58 A/U-L - AMPHENOL PROCOM
RG 58 A/U-L is a coaxial cable with stranded tinned copper wire and with a tinned copper wire braid shield. The material specification of the outer jacket is classified as Low Smoke Zero Halogen (LSZH) material.
L-1256-P.fm - Amphenol Aerospace
Assemble inner contact assembly over cable center conductor until rear of inner contact assembly butts against cable inner core. Cable center con-ductor must be visible through the inspection hole in the inner contact wire well. 2. Crimp inner contact using tool and positioner listed in table on back. 3.
LCF14-50J - 1/4" CELLFLEX® Low-Loss Foam-Dielectric Coaxial Cable
CELLFLEX® coaxial cable's solid inner and outer conductors virtually eliminate intermods. Intermodulation performance is also confirmed with state-of-the-art equipment at the RFS Technologies factory.
Amphenol Aerospace
Ends must be cut cleanly and at right angles to the axial plane of the cable. The cable must not be deformed while making cuts. 3. Flare outer braid, then strip cable dielectric as shown. 1. Assemble inner contact assembly over cable center conductor and cable dielectric until inside bore of bushing butts against cable dielec tric. 2.
Coaxial Cable Installation Instruction - RFS Technologies
Provide the cable inner conductor with a chamfer using the deburrer of the tool. For this purpose insert cable inner conductor into the chamfer tool, press the tool carefully turning it a few times.
Amphenol Aerospace
** Terminates the inner coaxial portion of the indicated cables. *** (A or B) Designates positioner cavity. Using insertion tool (part number M81969/8-09 or M81969/14-04), insert contact assembly into rear connector grommet hole. Contact must be aligned with hole and not inserted at an angle.
7/8 Air Dielectric Cable - RFS Technologies
Air dielectric coaxial cable's solid inner and outer conductors virtually eliminate intermods. Intermodulation performance is also confirmed with state-of-the-art equipment at the RFS Technologies factory.
Amphenol Aerospace
Carefully slide outer contact assembly over inner contact assembly and under cable outer braid until inner contact butts against insulator shoulder as illustrated.
ICA12-50JPLB - 1/2' ClearFill ® Line Plenum-Rated Air-Dielectric ...
RFS Technologies coaxial cable's solid inner and outer conductors virtually eliminate intermods. Intermodulation performance is also confirmed with state-of-the-art equipment at the RFS Technologies factory.
LCF78-50JA - 7/8' CELLFLEX® Premium Attenuation Low-Loss Foam ...
CELLFLEX® coaxial cable's solid inner and outer conductors virtually eliminate intermods. Intermodulation performance is also confirmed with state-of-the-art equipment at the RFS Technologies factory.