Search Results for company operations director
Model 261B11 | PCB Piezotronics
Model 261B11:Triax force link, charge, 1000 lb (Fz), 500 lb (Fx,y), 15 pC/lb (z), 32 pC/lb (x,y), ground isolated
EU RoHS II Certificate of Conformance - amphenol-aerospace.com
Operations and Commercial Air Division hereby acknowledges the referenced product is in conformity with the following: Directive 2011/65/EU (as amended) Directive 2015/863/EU pertaining to the addition of four phthalates Product compliance assessments are based on AAO and ACAD data and Material Declarations received from our
Model 130d20 | PCB Piezotronics (en)
3425 Walden Avenue Depew, NY 14043. Sensorline SM 716.684.0001. info@pcb.com +1 800-828-8840
Quantum Computing TR Multicoax Series - Amphenol Ardent Concepts
Specifications subect to change without notice S Patent Numbers 6,787,709, 6,909,056, 7,126,062, 7,556,503, 8,926,342. Ardent Concepts 2020 Revision 3/2020
Model 422E38 In-line charge converter, 0.1 mV/pC, +/-2.5V output, -5% ...
%PDF-1.4 %âãÏÓ 2 0 obj >/Font >/ProcSet[/PDF/Text/ImageB/ImageC/ImageI]/XObject >>>/Group >/Annots[61 0 R 62 0 R 63 0 R]>> endobj 23 0 obj >stream xœ½=koÜ8 ...
PCB Product Finder for Load Cells (en)
3425 Walden Avenue Depew, NY 14043. Sensorline SM 716.684.0001. info@pcb.com +1 800-828-8840
SGX - SGX Sensortech Sensor
Head office. Switzerland, Courtils 1, 2035 Corcelles-Cormondreche +41 (0) 32 732 16 70. contact@sgxsensortech.com
EU RoHS II Certificate of Conformance - amphenol-aerospace.com
Operations and Commercial Air Division hereby acknowledges the referenced product is in conformity with the following: Directive 2011/65/EU (as amended) Directive 2015/863/EU pertaining to the addition of four phthalates Product compliance assessments are based on AAO and ACAD data and Material Declarations received from our
Model 378C01 ICP Microphone System Installation and Operating Manual - PCB
60 0.02 Pa Business Office 80 0.2 Pa Shop Noise 94 1 Pa Large Truck 100 2 Pa Jackhammer 120 20 Pa Airplane Take-Off 140 200 Pa Threshold of Pain At very high-pressure amplitudes, the microphone’s diaphragm will start to distort the measured sound pressure. The maximum rated sound pressure level of a microphone is expressed as the amplitude at ...
Trex-Onics® High-Flex Ultra Coil Retractile Cord - TPC Wire
Trex-Onics® High-Flex Ultra Coil Retractile Cord exhibits a unique design that provides a very durable yet lightweight retractile cord while preserving superior coil retention and snappiness.
Model 354C03
%PDF-1.4 %âãÏÓ 2 0 obj >/Font >/ProcSet[/PDF/Text/ImageB/ImageC/ImageI]/XObject >>>/Group >/Annots[63 0 R 64 0 R 65 0 R]>> endobj 25 0 obj >stream xœ½=koÜ8 ...
Marine Sensors | Engine Management
Thermometrics Sensor Assemblies | JS8746 Harsh Environment Temperature Sensor. Thermometrics JS8746 Harsh Environment Temperature Sensor has been designed to address all aspects of temperature measurement for HVAC control systems in the container-ship market, in addition to industrial applications, such as compresors, condensing units, heat pumps, air conditioning.
MTC-HD – High Density MT Ferrules with 6 Insert Arrangements
Next-generation fiber optic circular connector with high-density MT ferrules.
0.21mm Super Low Profile FPC connector - Amphenol CS
F01C series is a 0.21mm pitch right angle Non-ZIF FPC connector with an autolock mechanism and surface mount termination. It has a high density design and low height 0.5mm. It features a cable thickness of 0.18mm and provide high retention force with lock
Model 9100-MPPA01 | PCB Piezotronics
Proximity probe adaptor kit, supports probes with common case threads ranging from M6 to 3/8". Includes Mitutoyo micrometer (metric) and 9100-PPA02 nickel plated 4140 steel target *TMS*
120-Channel 10G Rugged Ethernet Switchbox - Amphenol Aerospace
Business Unit Director +1 (607) 643-1845 jsibrava@amphenol-aao.com Description: Amphenol’s Rugged 120 Channel Ethernet Switch Box provides an unmatched level of flexibility to meet any system requirement. The switch box is a 120 port standalone Ethernet Switch box that is configurable for system connectivity, speeds, port types, and ...
Amphenol-Air LB | Company
Flexibility and strong customer focus are the fundamental success factors for the Saarlouis-based company. The technical competence of the company’s internal development team, the Amphenol sales and distribution network that is active worldwide, and efficient logistics enable Amphenol-Air LB to provide custom solutions which meet the highest ...
News - Page 4 of 4 - Amphenol
The U.S. optical and electronics manufacturing company plans to develop development and business units in addition to manufacturing. István Decsi, deputy mayor ... (Wire to Board) Expansion Amphenol Industrial Operations has expanded its WTB (wire-to-board) portfolio with the addition of a right-angle mating pin option in both the 2.4 and 3.6 ...
Model 340A16 | PCB Piezotronics (en)
3425 Walden Avenue Depew, NY 14043. Sensorline SM 716.684.0001. info@pcb.com +1 800-828-8840
PCTEL to Participate in 8th Annual Intellisight Investor Conference on ...
BLOOMINGDALE, Ill. --(BUSINESS WIRE)--Aug. 9, 2019-- PCTEL, Inc. (Nasdaq: PCTI) announced today that it will participate in the 8th Annual Intellisight Conference on Wednesday, August 14 in Minneapolis . Interested parties can view a live webcast of the Company’s presentation at