Search Results for concentration of measure
Telaire Demand Control Ventilation Q&A - amphenol-sensors.com
is not a direct measure of IAQ. It is an excellent measure of effective ventilation (mechanical ventilation plus infiltration). The higher the CO 2 concentration the lower the ventilation. When indoor CO 2 levels are very high (above 1800 ppm), ventilation is low (below 7 cfm/person) and other contaminants can build up, causing irritation and ...
TSW-10 Turbidity Sensor - amphenol-sensors.com
The TSW-10 module measures the turbidity (amount of suspended particles) of the wash water in washing machines and dishwashers. An optical sensor for washing machines is a measuring product for a turbid water density or an extraneous matter concentration using the refraction of wavelength between photo transistor and diode.
SGX-4NH3-300 Datasheet - SGX Sensortech
GAS CONCENTRATION SGX-NH3-300 Carbon Monoxide 500ppm 0 ppm Hydrogen Sulphide 25ppm 30 ppm Sulphur Dioxide 20ppm -6 ppm Nitric Oxide 50ppm 0 ppm ... as the accuracy of calibration and measurement cannot be ensured. 5) The cross sensitivities are including but not limited to the gases stated in the table. It may
TSW-10 Turbidity Sensor - amphenol-sensors.com
The TSW-10 module measures the turbidity (amount of suspended particles) of the wash water in washing machines and dishwashers. An optical sensor for washing machines is a measuring product for a turbid water density or an extraneous matter concentration using the refraction of wavelength between photo transistor and diode.
Temposonics
VDC Start measurement 5 60% 0 5 60% 30% 0 End measurement t VDC * * Depends on measurement length of waveguide t. 45 µs - 108 µs 30%. Period puls width modulation 19 µs* VDC Start measurement 5 60% 0 5 60% 30% 0 End measurement t VDC * * Depends on measurement length of waveguide. 36.1 21.2 Stroke length 18.2 16 2.2 1.8 Ø23 Ø4 Null zone ...
TSD-10 Turbidity Sensor - amphenol-sensors.com
The TSD-10 module measures the turbidity (amount of suspended particles) of the wash water in washing machines and dishwashers. An optical sensor for washing machines is a measuring product for a turbid water density or an extraneous matter concentration using the refraction of wavelength between photo transistor and diode.
MG, MG1, MGA User’s Guide – Amphenol Sensors
We believe that making sustainable choices in the way we conduct our business creates short-term and long-term value for our stakeholders. We do not create long-term value by merely complying with regulations, but we go beyond compliance to find ways to green our operations and our products to ensure continuity of the material and human resources that we need to operate the business.
TSW-10 Turbidity Sensor - amphenol-sensors.com
The TSW-10 module measures the turbidity (amount of suspended particles) of the wash water in washing machines and dishwashers. An optical sensor for washing machines is a measuring product for a turbid water density or an extraneous matter concentration using the refraction of wavelength between photo transistor and diode.
Telaire T6703 Series CO2 Module - amphenol-sensors.com
• All units are factory calibrated to measure CO2 concentration at 0-2000 and 0-5000 ppm • Custom connector headers available Applications • HVAC – OEM rooftop units • HVAC – Heat Exchangers • HVAC – Outside air transmitters • Automotive – Heavy truck/tractor cabin • Agriculture – Greenhouse and indoor growing
Thermometrics TSD-10 Turbidity Sensor - amphenol-sensors.com
The TSD-10 module measures the turbidity (amount of suspended particles) of the wash water in washing machines and dishwashers. An optical sensor for washing machines is a measuring product for a turbid water density or an extraneous matter concentration using the refraction of wavelength between photo transistor and diode. By using an optical
SGX-7NH3-100 Datasheet - SGX Sensortech
GAS CONCENTRATION SGX-7NH3-100 Carbon Monoxide 500ppm 0 ppm Hydrogen Sulphide 15ppm <30 ppm Sulphur Dioxide 20ppm -6 ppm Nitric ... as the accuracy of calibration and measurement cannot be ensured. 5) The cross sensitivities are including but not limited to the gases stated in the table. It may
Thermometrics 165D6042P003 turbidity and temperature sensor
The 165D6042P003 module measures the turbidity (amount of suspended particles) of the wash water in washing machines and dishwashers. An optical sensor for washing machines is a measuring product for a turbid water density or an extraneous matter concentration using the refraction of wavelength between photo transistor and diode.
ZTP-148SR Thermopile IR Sensor - Amphenol Sensors
We believe that making sustainable choices in the way we conduct our business creates short-term and long-term value for our stakeholders. We do not create long-term value by merely complying with regulations, but we go beyond compliance to find ways to green our operations and our products to ensure continuity of the material and human resources that we need to operate the business.
BA1010-2 - Amphenol Antenna Solutions
Omnidirectional Fiberglass Antenna, 154-174, 2.1dBi, N Female
PROTIMETER - amphenol-sensors.com
Indeed, the instrument measures moisture in wood and wood-moisture-equivalent (WME) in building materials other than wood. It is possible, therefore, to mark on the scale of a Protimeter moisture meter indications of “safe”, ... Concentration of salts in a party wall in which ris-ing damp has persisted for 80 years. The figures show the ...
Smart Board with Metal Oxide Sensor For Ozone Monitoring - SGX Sensortech
{M00000240002<024} // Measurement string, ozone concentration // is set to 0 in calibration mode Operation Status Master { C M Heater of sensor 1 M Overheating of sensor } OZ-47 { C M Heater of sensor 1 M Overheating of sensor } This command drives the heating of the ozone gas sensor. In initial mode (after reset), sensor is operated.
Telaire Air Quality Sensors
All units are factory calibrated to measure CO 2 concentration levels up to 5000ppm, while maintaining accuracy across the range. T6715 The new T6715 is the smallest most accurate dual channel CO 2 sensor available on the market today. Telaire dual channel technology allow self calibration in applications where ABC logic will not work. i.e.
Thermometrics TST-10 Turbidity Sensor - amphenol-sensors.com
The TST-10 module measures the turbidity (amount of suspended particles) of the wash water in washing machines and dishwashers. An optical sensor for washing machines is a measuring product for a turbid water density or an extraneous matter concentration using the refraction of wavelength between photo transistor and diode. By using an optical
Thermometrics TST-10 Turbidity Sensor - amphenol-sensors.com
The TST-10 module measures the turbidity (amount of suspended particles) of the wash water in washing machines and dishwashers. An optical sensor for washing machines is a measuring product for a turbid water density or an extraneous matter concentration using the refraction of wavelength between photo transistor and diode. By using an optical
Thermometrics TSW-10 Turbidity Sensor - amphenol-sensors.com
The TSW-10 module measures the turbidity (amount of suspended particles) of the wash water in washing machines and dishwashers. An optical sensor for washing machines is a measuring product for a turbid water density or an extraneous matter concentration using the refraction of wavelength between photo transistor and diode. By using an optical