Search Results for concentration of measure
PROTIMETER - amphenol-sensors.com
Concentration of salts in a party wall in which ris-ing damp has persisted for 80 years. The figures show the percentage by weight of chloride plus nitrate. The shaded area is heavily contaminated. (Redrawn from Building Research Establishment Digest 245. revised 1987) How to Measure Moisture in Buildings
PS1&PS4-CO-10%-MOD CarbonMonoxideModule Datasheet - SGX Sensortech
Humidity measurement range: (10 ~ 95)% RH non-condensing Relative error: ± 2% ... The storage environment should keep the air clean, no pollution gas, no acetone, no high concentration organic gas, no dust, no smoke; 3. Avoid storage with alcohol (ethanol), perfume, sodium silicate and polyurethane liquids or solids; 4. Avoid high temperature ...
Telaire Air Quality Sensors
All units are factory calibrated to measure CO 2 concentration levels up to 5000ppm, while maintaining accuracy across the range. T6715 The new T6715 is the smallest most accurate dual channel CO 2 sensor available on the market today. Telaire dual channel technology allow self calibration in applications where ABC logic will not work. i.e.
CO2 Archives - Amphenol Sensors
We believe that making sustainable choices in the way we conduct our business creates short-term and long-term value for our stakeholders. We do not create long-term value by merely complying with regulations, but we go beyond compliance to find ways to green our operations and our products to ensure continuity of the material and human resources that we need to operate the business.
Telaire Air Quality Sensors
All units are factory calibrated to measure CO 2 concentration levels up to 5000ppm, while maintaining accuracy across the range. T6715 The new T6715 is the smallest most accurate dual channel CO 2 sensor available on the market today. Telaire dual channel technology allow self calibration in applications where ABC logic will not work. i.e.
Unmanned Aerial Vehicle (UAV) - Amphenol Sensors
Amphenol Sensors serves the UAV industry by providing high quality sensor and measurement solutions that are designed to meet the unique and demanding requirements of Consumer, Commercial, Medical, and Military drone applications. ... Temperature & Concentration Sensors. High accuracy; Continuous monitoring; Meets highest worldwide emissions ...
Telaire Air Quality Sensors
All units are factory calibrated to measure CO 2 concentration levels up to 5000ppm, while maintaining accuracy across the range. T6715 The new T6715 is the smallest most accurate dual channel CO 2 sensor available on the market today. Telaire dual channel technology allow self calibration in applications where ABC logic will not work. i.e.
SSI Technologies, LLC
Pressure measurement technology translates force from an induced pressure into an electrical signal. SSI's family of pressure sensors use piezoresistive technology for its sensor signal processing to measure pressure. SSI Technologies, LLC full line of Pressure Sensors is sure to fit your automotive, industrial or commercial application needs.
Medical - Amphenol Sensors
We believe that making sustainable choices in the way we conduct our business creates short-term and long-term value for our stakeholders. We do not create long-term value by merely complying with regulations, but we go beyond compliance to find ways to green our operations and our products to ensure continuity of the material and human resources that we need to operate the business.
2-sip | Amphenol Global Search | Amphenol
All units are factory calibrated to measure CO 2 concentration levels up to 5000ppm. T6703 The Telaire T6703 CO 2 Module is configured for applications where CO 2 ... The 3-in-1 data logger from the Kaye ValProbe RT product line offers the capability to measure critical parameters such as CO 2 (carbon dioxide), relative humidity (RH), and ...
Telaire Air Quality Sensors
All units are factory calibrated to measure CO 2 concentration levels up to 5000ppm, while maintaining accuracy across the range. T6715 The new T6715 is the smallest most accurate dual channel CO 2 sensor available on the market today. Telaire dual channel technology allow self calibration in applications where ABC logic will not work. i.e.
Telaire Air Quality Sensors
All units are factory calibrated to measure CO 2 concentration levels up to 5000ppm, while maintaining accuracy across the range. T6715 The new T6715 is the smallest most accurate dual channel CO 2 sensor available on the market today. Telaire dual channel technology allow self calibration in applications where ABC logic will not work. i.e.
WiFi Natural Gas Module Datasheet - sgxsensortech.com
module and the concentration of gas when configured to access a wireless network type 802.11 b/g/n. The estimated maintenance-free operation on 3xAA (2800mAh) batteries is 6 months, with one ... (in measurement mode, battery operated) ~120mA avg (in wireless transmission cycle) Transmission USB (RS232, CDC Class), WiFi (WROOM-02, 802.11
surlok plus | Amphenol Global Search | Amphenol
Search Results for surlok plus AR50CH Airducer® Ultrasonic Transducer - Airmar The ultrasonic AR50CH brings proven dependability to level, flow and distance measurement applications. ... For example, a B260-10F is a B260 MM base transducer and cable, plus a 10F adapter cable for Furuno 10-pin equipment. A B260-8G is the same transducer ...
ECVQ-EK3 Electrochemical and Pellistor Gas Sensor Evaluation Kit
thermal conductivity) gas sensors, automatically measure the sensor outputs and calculate gas concentration levels. Sensors can be monitored automatically via the USB ... sensor has a linear response to concentration, a basic calibration can be performed using the supplied software to give a concentration reading in ppm, %volume or %LEL
Pellistor Application Note 1 Pellistor Sensor Technology & Applications
The signal produced is proportional to the gas concentration up to the lower explosive limit, or LEL. The sensor will detect all combustible gases and vapours, although the response to higher hydrocarbons ... As these sensors measure gases in the 0 - 100% LEL range, they are routinely fitted in instruments used in applications where combustible ...
Pressure & Temperature Combination Sensor - Amphenol Sensors
We believe that making sustainable choices in the way we conduct our business creates short-term and long-term value for our stakeholders. We do not create long-term value by merely complying with regulations, but we go beyond compliance to find ways to green our operations and our products to ensure continuity of the material and human resources that we need to operate the business.
Telaire T67XX CO2 Sensor Module - Amphenol
MEASURE ON DEMAND MODE USING I2C ... reference value is the lowest concentration to which the sensor is exposed. ABC Logic requires continuous operation of the sensor for increments of at least 4 hours each. Note: Applies when used in typical residential ambient air. Consult Amphenol Advanced Sensors if other
Application SpotlightApplication Spotlight
Carbon Dioxide (CO2) Beverage Dispenser Monitoring and Alarming Application SpotlightApplication Spotlight Carbon Dioxide (CO2) gas occurs naturally in the earth’s atmosphere in concentrations of ~300-400 parts per million (ppm). At this level, CO2 is harmless since the gas is neither toxic, nor explosive. CO2 gas can pose a health hazard, however, in confined or poorly ventilated areas ...
Sensor selection guide - Wilcoxon Sensing Technologies
Displacement sensors are used to measure shaft motion and internal clearances. Monitors have used non-contact proximity sensors, such as eddy probes, to sense shaft vibration relative to bearings or other support structures. ... concentration, intrinsically safe sensors are incapable of causing ignition; this greatly reduces the risk of explosions.