Search Results for conemu show git branch
MH-Series with CANopen Safety (Document part number 901997)
CANopen protocol uses Emergency Objects to inform that the sensor has entered a state of error, or that a state of error has ended. Any Error state will also be visible in the SRDO through Status byte and the position data being set to zero.
Absolute, Non-Contact Position Sensors Protocol Manual MH ... - Temposonics
Temposonics® MH Protocol Manual CANopen I 8 I 7.1.4 Reset_Node indication (9),(10),(11) Through this service the NMT Master sets the state of the selected NMT Slave(s) from any state to the „reset application“ sub-state.
Operation Manual E-Series Embedded Analog - Temposonics
2 Temposonics® E-Series Embedded Analog 1. Introduction 1.1 Purpose and use of this manual The content of this technical documentation and of its various anne-xes is intended to provide quick information on mounting, installation
Amphenol’s High-Performance COM-HPC Connectors
COM-HPC, or Computer-on-Module for High-Performance Computing, is an open standard for integrating advanced computing capabilities into compact modules. It enables high-speed data transfer and efficient power management and addresses the increasing demands for performance in applications like IoT, medical, datacom, and industrial automation.
Open Compute Project Solutions - Amphenol CS
Amphenol offers a comprehensive portfolio of plug-and-play interconnects ranging from 50A to 1000A catering to Open Rack ORv2 and ORv3 specifications, to empower businesses to achieve cost savings, seamless implementation, and enhanced energy efficiency.
Operation Manual TempoGate Smart Assistant - Temposonics
Temoate ® smart assistant Operation Manual I 3 I 1. Introduction 1.1 Purpose and use of this manual 1/ The term “qualified technical personnel” characterizes persons who • are familiar with the safety concepts of automation
Charles Universal Broadband Enclosure CUBE-PM524xx Series General ...
This document provides general information for the CUBE-PM524xx family of the Charles Industries’ Universal Broadband Enclosure (CUBE) product line. Supplemental documentation that ships with the CUBE contains more detailed information about the models. Figure 1 shows closed front views of the enclosure, with and without the battery compartment.
Mini Cool Edge IO – The Ideal Solution to Transmit Next Generation High ...
Mini Cool Edge IO 0.60mm pitch connector functions as an internal high-speed connector that supports up to 56G PAM4 and aims at facilitating high-speed signal transmission in Data Centers, Network Routings, and Telecommunications. It offers more advanced and powerful features over the existing interconnect solutions.
Operation Manual T-Series Analog - Temposonics
7. Cable entry temperature and branching point temperature may reach 104 °C (219 °F) and 116 °C (241 °F) respectively. Select suitable cable and entry device. 8. For field wiring, use cables suitable for the service temperature range of −40 °C (−40 °F) to +116 °C (241 °F). 9. Do not open when energized. Open the sensor only as shown in
Lanlink NMEA 2000 To Ethernet Gateway - Gemeco
LANLink is a NMEA to ethernet gateway which enables the boat’s NMEA data to integrate onto the router network - allowing connected devices and apps to take advantage of the data. LANLink is available in two versions suitable for NMEA 0183 and NMEA 2000 respectively.
AllDisc Combi MIMO Wifi-7 GNSS Antenna - PCTEL
AllDisc Combi MIMO Wifi-7 GNSS Antenna platform can be configured to support several antenna systems: Cellular LTE / 5G, GPS/Glonass/Galileo and MIMO WiFi 6E in a low profile casing with durable design IP6K9K.
Direct Current (DC) Monitor - Gemeco
Examples of DC power sources that can be monitored with the DCM100 include batteries, alternators, solar panels, and wind generators. The DCM100 can also be used to monitor DC loads like inverters, windlasses, DC refrigerators, or any DC branch circuit.
Data Sheet - Temposonics
Temposonics® GT is a sensor with double or triple redundancy. Two or three independent measuring systems are integrated in one sensor housing. In particular the sensor is suitable for enhanced safety appli-cations. The waveguide is installed in a pressure-resistant high-grade steel rod.
Enclosed Yagi MIMO Antennas for WiFi Applications - PCTEL
These enclosed Yagi MIMO Antennas are suited for long range broadband wireless access applications. They provide highspeed directional WiFi coverage and optimized data throughput in a rugged, low profile housing. They are ideal for point-to-point installations in challenging environmental settings. Questions?
Data Sheet ER CANopen - Temposonics
Branch Office Phone: +39 030 988 3819 E-mail: info.it@temposonics.com FRANCE Branch Office Phone: +33 6 14 060 728 E-mail: info.fr@temposonics.com UK Branch Office Phone: +44 79 21 83 05 86 E-mail: info.uk@temposonics.com SCANDINAVIA Branch Office Phone: + 46 70 29 91 281 E-mail: info.sca@temposonics.com CHINA Branch Office
ExaMAX2® Connector System: Elevating Performance and ... - Amphenol CS
In this blog, we delve into the remarkable features, benefits, and significance of ExaMAX2 ®, the next-generation connector system that promises to redefine the standards of data transmission. Unveiling ExaMAX2®: A Revolution in Data Transmission.
PCIe Gen 5 CEM Connector & Add-In Card PCB Design Optimizations
Amphenol is proud to announce that Yifan Huang and Stephen Smith will present a technical paper titled “ PCIe Gen 5 CEM Connector and Add-In Card PCB design optimizations ” at DesignCon 2019. Li Ying, from Nvidia, will present along with the Amphenol team regarding Nvidia’s high-end 32Gb/s GPU add-in card design.
Magnetostrictive Liquid Level Transmitters with ... - Temposonics
3 Modbus Interface Manual LP Series 1. Contact information United States General Tel: +1-919-677-0100 Fax: +1-919-677-2343 E-mail: info.us@mtssensors.com
Operation Manual Level Plus - Temposonics
Level Plus ® 5H QH0(® Operation Manual I 3 I 1. Contact information United States General Tel: +1-919-677-0100 Fax: +1-919-677-2343 E-mail: info.us@temposonics.com
Gen Z – The Next Gen Computing Architecture - Amphenol CS
Gen Z is a new open-system interconnect consortium aiming at providing advanced memory access to data and device. Gen Z physical layer leverages IEEE-802.3 and PCIe specification.