Search Results for cp2102 driver install
USB To Serial Interface Cable - gemeco.com
• Easy way to install an additional RS232 serial port, Frees up Serial/RS232 ports for other uses • Full compliance with USB specification v1.1 • Supports automatic handshake mode
Software Downloads | Support - PCTEL
Firmware updates are available for scanning receivers under warranty. Download the latest utilities, software, drivers & more for your PCTEL products, devices, and software.
USB To Serial Gateway 0183, RS422, RS232 - Gemeco
Advanced technology for safe, reliable and simple connection of your NMEA 0183, RS422 and RS232 devices to your PC’s USB port. The USG-2 converts a USB port into a bi-directional serial port suitable for connecting to a marine standard NMEA 0183 data bus. It provides a far safer connection when compared to standard USB to serial converters.
Handbook LCON – Programmable Converters - Lutze
The document contains instructions for installing the application PACTware, HART-DTM-driver, Lütze DTM-driver and the installation of the USB service cable. The software can be downloaded for free on the Lütze website: www.luetze.de Following options are offered as zip files: - Analog / Analog Converter 750320 / 751320 LCON AA DFDT 806210
87520-0010BLF | USB 2.0 | Amphenol
Click on the Check Sample (if available) button to check the allowed sample quantity in the cart. You can also purchase additional quantity in the cart or buy directly using the Buy Now button below. The information below is for reference only. For more technical details, refer to product specification and application specification.
VITA Developer Kit - SV Microwave
Ideal for prototyping and production-level testing, this ruggedized and durable kit features a backplane, multiport module, ruggedized VITA RF Cable Assemblies, Screws and Driver Tool, Contact Installation and Removal Tools and more.
124018402112A | USB 3.2 GEN2 | Amphenol
Amphenol is one of the leading manufacturers of USB Type C 3.1. Contact us today for more details of USB Type C 3.1, part number 124018402112A.
Gateway NMEA 2000®/USB - Gemeco
USB Interface Modes: NMEA 0183 (With Maretron-Supplied Windows® Drivers), Native NMEA 2000® (For Use With N2KView and N2KAnalyzer) Supported Operating Systems: Windows XP, Vista, 7, 8 and 10 (32-bit and 64-bit)
Installation Guide Temposonics
Installation guide: 1. Use the enclosed CD-ROM for the driver-installation of the CAN-USB adapter. 2. Download the latest version of the Test-Software (MTS_CANTest- Interface_Vxxx.exe) and the detailed installation and operation instructions from the login area of our website (http://www.mtssensor.de/login.html). 3.
Telaire T6613/T6615 Series Development Kit - Amphenol
A third party vendor supplies the device drivers for the USB communications software. The Setup Wizard should automatically load their driver installation software. However, if the software has to be loaded manually, then you can find that installation program in the default installation directory under the subdirectory VCP Driver. Run the
AIRMAR Technical Support
AIRMAR ISO Certification (PDF Download) Supplier Change Notification (PDF Download) Supplier Corrective Action Request (PDF Download) Supplier Quality Support Manual (PDF) DISCOVER. Videos. What is XID? AIRMAR Certified Installers. Installer Finder. WeatherStationWX.com
ALDC Software Installation Quick Start - Amphenol Antenna Solutions
Setting up the ALDC software involves three steps: downloading, extracting, and then installing. ALDC software v2.0 for Microsoft Windows. The best way to obtain the latest software is to download it from the Amphenol Antennas Web site.
NMEA 2000®U200 USB Gateway - AIRMAR EMEA
Airmar’s converter allows the NMEA 2000® data coming from the PB and WX series WeatherStations®, and G2183, H2183, and GH2183 sensors to be displayed on a PC via an available USB port. This will allow the sensor’s data to be viewed in the WeatherCaster™ PC Software or other PC based navigation software.
Charles Universal Broadband Enclosure CUBE-PM4110-A General Description ...
Visually inspect the unit for damages prior to installation. If the equipment was damaged in transit, immediately report the extent of the damage to the transportation company.
Installing the Sensor - Amphenol
Basic Installation 1. Separate the case into its front and rear sections. 2. Secure the rear section of the case to the wall or junction box using the supplied screws, and make necessary wire connections. 3. Select Voltage or Current output option and Voltage range (0-10 V or 0-5 V) using the SW1, switches #1 and #2 as shown on the
NMEA 2000®U200 USB Gateway - Gemeco
Airmar’s converter allows the NMEA 2000® data coming from the PB and WX series WeatherStations®, and G2183, H2183, and GH2183 sensors to be displayed on a PC via an available USB port. This will allow the sensor’s data to be viewed in the WeatherCaster™ PC Software or other PC based navigation software.
Installing Mosa2 - marport.com
If Mosa2 is not already installed on the computer, you need to install it to configure the sensor. Calibrating the Catch Sensor You need to calibrate the catch sensor to make sure you have correct catch measures.
Driving Safe with LV214 and USCAR Standards - Amphenol CS
LV214 is an essential industry specification that regulates the automobile industry. Along with USCAR, LV214 plays a significant role in determining the quality of automotive components. This blog will focus on USCAR and LV214 and explore the products from Amphenol that are qualified to meet standards and specifications.
Coaxial Cable Splitters CPS2-200 - AMPHENOL PROCOM
The CPS series of power splitters are manufactured using high quality coaxial cable and connectors. The CPS power splitters use quarter wave coaxial cable transformer sections to match two or more loads to one source.
20021121-00020C4LF | Minitek127® | Amphenol
Minitek127 ®, Board to Board connector, Unshrouded vertical header, Surface Mount, Double Row, 20Positions, 1.27mm (0.5inch) pitch. We may offer limited quantity of sample for this part. Click on the Check Sample (if available) button to check the allowed sample quantity in the cart.