Search Results for device id apk
RF Coaxial Connectors, Adapters and Cable Assemblies | Amphenol RF
Amphenol RF is the world’s largest manufacturer of coaxial connectors for use in radio frequency, microwave, and data transmission system applications. Headquartered in Danbury, Connecticut, USA, Amphenol RF has global sales, marketing and manufacturing locations in North America, Asia and Europe.
RET Control Units - Amphenol Antenna Solutions
In addition, each RET ID (Serial Number) will use the first (most left) character to indicate the colour of the corresponding frequency band of the antenna. This helps greatly during site commissioning by the ease it provides to distinguish between the RET devices shown by the AISG controller in the device list.
N2KView Vessel Monitoring Software - Gemeco
If you want to run N2KView® software on your vessel’s computer, you will need either a Maretron USB100 or an IPG100, which are necessary to get sensor information from the NMEA 2000® network to the computer. There is also a mobile version of N2KView® which runs on iPhone or iPad, or an Android device. See N2KView Mobile for details.
RET Control Units - Amphenol Antenna Solutions
In addition, each RET ID (Serial Number) will use the fi rst (most left) character to indicate the colour of the corresponding frequency band of the antenna. This helps greatly during site commissioning by the ease it provides to distinguish between the RET devices shown by the AISG controller in the device list.
Z05 & Z06 Series Vented Vertical Pedestals | Outdoor Fiber Pedestal ...
Indoor Cabinets (CUBE ID Series) Indoor Battery Racks – Modular (CIBR-M) Indoor Battery Racks – Bay Rack (CIBR-R) Indoor Security Shrouds; Cabinet Accessories. ... Z08 Series Active Device Low Profile Pedestals See Products. Z24 High Heat Node Pedestal Housings See Products. Z02 Series Pedestal Housings See Products. R02 Series Pedestal ...
RF INTERCONNECT SOLUTIONS FOR CAMERA & VISION SYSTEMS - Amphenol RF
and outside of the vehicle or body of the device. Standard vehicles and next-generation consumer products may contain more than eight cameras now. In autonomous and self-driving vehicles this includes HD, 4K, stereo and thermal imaging cameras. Similarly, industrial and manufacturing applications use vision systems with multiple cameras to help
Amphenol Assembletech
This cable assembly connects a MHL-enabled portable device to an MHL HDTV, and its small form factor makes it easy to carry around with your mobile device. This cable assembly features: 1.1080p HD video . 2.Digital audio . 3.Simultaneous charging to the mobile device . 4.TV remote access and control on mobile device Mechanical Performance. 1.
CFITH-144 Compact Fiber Hub | High-Capacity Fiber Distribution Hub
Optimize your fiber network with the CFITH-144 Compact Fiber Hub from Charles Industries. Ideal for compact, organized, and scalable fiber solutions. Enquire now!
0183 To N2K Gateway w/PC Interface (USB) - Gemeco
The device supports every available PGN in the NMEA 2000 standard. View converted NMEA 0183 data on Actisense NMEA Reader. The device sports the largest conversion library of any gateway. Easily interface with a wide range of PC applications via the NGX-1, such as TimeZero (NMEA 2000) and OpenCPN (NMEA 0183).
ALDC_UM - Amphenol Antenna Solutions
1.1 device for trouble shooting. Purpose: Used to set the number of digits in the device serial number (from the far right) that the scan routine looks at during a scan operation. NOT an applicable setting for the AISG 2 device. MUST INCREASE the [Scan Length] value if multiple devices have serial numbers with the same last three far right digits.
Contact | Commercial Moisture Meters - Protimeter
Europe & Asia Address: Crown Industrial Estate Priorswood Road Taunton, UK TA2-8QY Phone: +44 (0)1823 335200 Fax: +44 (0)1823 332637
RET Control Units - amphenol-antennas.com
The MDCU (Multiple Device Control Unit) is the electronic module that allows the remote control of the electrical downtilt (RET) in Amphenol antennas with factory embedded motors. For a multiband ... In addition, each RET ID (Serial Number) will use the fi rst (most left) character to indicate the colour of the
ATN3000 Class 3 Aton - Gemeco
The DigAtoN is available as a Class 1 device (transmit only) or a Class 3 device (transmit and receive). Class 1 devices require a local AIS base station to be operating in the same area as the AtoN whereas Class 3 devices can internally allocate slots for transmission allowing them to be placed anywhere.
Complete End-to-End Solution - amphenolrf.com
often mounted on the outside of a device by means of an RF connector. They are engineered for indoor and outdoor use with robust designs available for harsher environments. External antennas can use either the monopole or dipole design and are typically used for higher power transmission and reception. They are ideal for
Contents
primarily on software. For instance, there are mobile apps that help drivers to find better gas prices nearby, improve fuel economy, and even call for emergency assistance in the event of an accident. While software is an important part of the future of connected cars, hardware is an equally vital and highly profitable segment of this industry.
Concealment Solution | Concealment Shrouds for Small Cell & DAS
Z08 Series Active Device Low Profile Pedestals; Z01 Vertical Broadband Pedestal; B04 Series Non-Louvered Vertical Broadband Pedestals; B05 & B06 Series Vertical Broadband Pedestals; Louvered Low-Profile Housings; Z14 High Heat Node Pedestal Housings; Z24 High Heat Node Pedestal Housings; Z05 & Z06 Series Vented Vertical Pedestals; Z02 Series ...
Software Solutions - Amphenol Antenna Solutions
Resources Resources Software Solutions Download the latest Software and Firmware. Should you have questions, Amphenol's Technical Support teams are ready to assist. Network Element Manager Software: NEM-ALD-W The NEM-ALD-W is designed to discover any device connected to an Antenna Line Device (ALD) network. It is
Model TO670A01 Echo® Wireless Vibration Sensor, 916 MHz, with ...
FCC ID: ZOC-IMI670A01 . This device complies with part 15 of the FCC Rules. Operation is subject to the following two conditions: (1) This device may not cause harmful interference, and (2) this device must accept any interference received, including interference that may cause undesired
Ferret Lite IP67 WiFi Inspection Camera Kit - Gemeco
Connects to your smart device; Rechargeable; IP67 rated (Dust-proof & Waterproof) Wireless range up to 50' Digital Zoom; Adjustable bright white LEDs; Save photos & videos to smart device; 60-90 mins Operating Time; Suitable for pulling cable; 1.5 hrs charge time; Fixed Focus; Specifications
Amphenol (Maryland) PCH Sensor Revision 1 - Wilcoxon Sensing Technologies
2. Device Identification Manufacturer Name: Wilcoxon Model Name(s): PCH420V-M12, PCH420V-R6 Manufacture ID Code: 24,744 (0x60A8) Device Type Code: 58,092(0xE2EC) HART Protocol Revision 7.5 Device Revision: 1 Number of Device Variables 4 Physical Layers Supported Bell202 Physical Device Category Sensor, Vibration, Velocity