Search Results for direction administrative def
Model 202B ICP® quartz force ring, 10k lb comp., 0.5 mV/lb ... - PCB
Definition of Terms and Symbols The following symbols may be used in this manual: DANGER Indicates an immediate hazardous situation, which, if not avoided, may result in death or serious injury. Manual 21354 Rev E ECN 50523 CAUTION Refers to hazards that could damage
FAQ - Amphenol Socapex
Data storage on external disk, exchange of HD video streams (camera, recording), transmission of high-definition images, communication with digital devices, all with 5Gbit/s transfer speed.
... Does the USB3 Amplifier have a connection direction?
N-Type Straight Clamp Plug RG-8 RG-213 RG-225 50 Ohm
Thread Direction: Standard: You May also be Interested in. N-Type Panel Mount Jack 4-Hole Flange Solder Cup 50 Ohm 172119-11. N-Type Straight Clamp Jack RG-58 RG-141 Times LMR-195 50 Ohm 000-35025-RFX. N-Type Panel Mount Plug 4-Hole Flange Round Post 50 Ohm 172353.
SMA Straight Crimp Plug RG-55 RG-142 RG-223 RG-400 50 Ohm
Thread Direction: Standard: You May also be Interested in. SMA PCB Through Hole Straight Jack 50 Ohm 901-10112. SMA Panel Mount Jack 4-Hole Flange Round Post 50 Ohm 901-10375. SMA Straight Crimp Plug 1.13 mm Micro-cable 50 Ohm 132393. SMA Panel Mount Plug 4-Hole Flange Female Contact 50 Ohm 132160.
N-Type Straight Clamp Plug TRC-75 75 Ohm | 082-B0101-1356 - Amphenol RF
Thread Direction: Standard: You May also be Interested in. N-Type Straight Crimp Plug RG-6 50 Ohm 172202. UG-1186/U N-Type Straight Clamp Jack RG-8 RG-213 RG-225 50 Ohm 082-313. N-Type Panel Mount Jack 4-Hole Flange Round Post 50 Ohm 082-6330.
Model Y691a51/04 Platinum BNC Termination Box Installation and ...
Definition of Terms and Symbols The following symbols may be used in this manual: DANGER Indicates an immediate hazardous situation, which, if not avoided, may result in death or serious injury. Manual 21354 Rev E ECN 50523 CAUTION Refers to hazards that could damage
SHORT-FORM PRODUCT CATALOG - Wilcoxon Sensing Technologies
2 info@wilcoxon.com buy.wilcoxon.com 301 330-8811 +1 (301) 330-8811 1-800-WILCOXON info@wilcoxon.com wilcoxon.com buy.wilcoxon.com Wilcoxon Sensing Technologies @WilcoxonSensing Contents Applications 6
SMA Panel Mount Plug 4-Hole Flange Round Post 50 Ohm
Thread Direction: Standard: You May also be Interested in. SMA Right Angle Crimp Plug Belden 1855A 50 Ohm 132272. SMA Panel Mount Jack 2-Hole Flange Round Post 50 Ohm 901-10142. SMA Right Angle Panel Mount Jack 4-Hole Flange Round Post 50 Ohm 0.280 Post 0.158 PTFE 132318-18.
Model 3743G1150G Accelerometer, VC, 50g, triaxial, differential, screw ...
Definition of Terms and Symbols The following symbols may be used in this manual: DANGER Indicates an immediate hazardous situation, which, if not avoided, may result in death or serious injury. Manual 21354 Rev E ECN 50523 CAUTION Refers to hazards that could damage
SMA Panel Mount Right Angle Jack 4-Hole Flange Solder RG-405 0.086-inch ...
Thread Direction: Standard: You May also be Interested in. SMA Straight Crimp Jack RG-174 RG-188 RG-316 Times LMR-100A 50 Ohm 132117SS. SMA PCB End Launch Jack 50 Ohm 132322. SMA Right Angle Clamp Plug 1/4-inch Helical Corrugated 50 Ohm 132FPRH1.
12-Channel (3657-80) and 6-Channel (3657-81) 2-Wire Foreign Exchange ...
Section 365-780-202 2 1. GENERAL 1.1 Document Purpose This document provides general, installation and testing information for the 12-Channel and 6-Channel 2-Wire
Repair and Maintenance Returning Equipment Contact Information ... - PCB
Definition of Terms and Symbols The following symbols may be used in this manual: DANGER Indicates an immediate hazardous situation, which, if not avoided, may result in death or serious injury. Manual 21354 Rev E ECN 50523 CAUTION Refers to hazards that could damage
Model 352A72 ICP® Accelerometer Installation and Operating Manual
Definition of Terms and Symbols The following symbols may be used in this manual: DANGER Indicates an immediate hazardous situation, which, if not avoided, may result in death or serious injury. Manual 21354 Rev E ECN 50523 CAUTION Refers to hazards that could damage
Model 352A24 Platinum Stock Products; Miniature, lightweight (0.8 ... - PCB
Definition of Terms and Symbols The following symbols may be used in this manual: DANGER Indicates an immediate hazardous situation, which, if not avoided, may result in death or serious injury. Manual 21354 Rev E ECN 50523 CAUTION Refers to hazards that could damage
Transducer operation in hazardous areas - Wilcoxon Sensing Technologies
The definition of hazardous area is further broken down into subcategories by Article 500 of the National Electrical Code® in order to define conditions which can cause ignition of the combustible atmosphere. These categories include combustible gases, such as acetylene, hydrogen, or methane, plus suspended dust and particulate such as ...
Ampehnol All Sensors Products | All Sensors
Pressure Max: 1 Units: IN H2O Operating Temperature:-25 to 85 C Supply Voltage: 5 VS Honeywell PN: Supply Voltage: 5 VS
3632-80 12 Channel and 3632-81 6 Channel Office Channel Unit—Data Port
Section 363-280-201 1. GENERAL 1.1 Document Purpose This document provides general, installation, and testing information for the 12 and 6 Channel Office Channel
360-80 T1 Channel Bank RELEASE NOTES - charlesindustries.com
and causes flicker of the LEDs and broken audio on the voice cards in all directions. 4. T1 Controller (3603) / Voice Units - Half size E&M, FXO & FXS - The tone test (beep) isn't available on the SNMP interface. Full size E&M, FXO & FXS - Enabling the tone test for 1 channel will block test availability to all other channels 5.
Model 3743F1150G Accelerometer, VC, 50g, triaxial, damped ... - PCB
Definition of Terms and Symbols The following symbols may be used in this manual: DANGER Indicates an immediate hazardous situation, which, if not avoided, may result in death or serious injury. Manual 21354 Rev E ECN 50523 CAUTION Refers to hazards that could damage
Model 086D05 Modally Tuned® Impulse Hammer w/force sensor and ... - PCB
Definition of Terms and Symbols The following symbols may be used in this manual: DANGER Indicates an immediate hazardous situation, which, if not avoided, may result in death or serious injury. Manual 21354 Rev E ECN 50523 CAUTION Refers to hazards that could damage