Search Results for dlss override
1710-2690 / 1710-2690 MHz - Amphenol Antenna Solutions
(manual override). RET Module The RET module is factory installed and does not need to be ordered separately. Part Number for AISG v1.1 protocol: MDCU-A0000 One unit installed in 6175100A Part Number for 3GPP/AISG v2.0 protocol: MDCU-G0000 One unit installed in 6175100G
RET Control Units - Amphenol Antenna Solutions
remain visible and manual change of the tilt is still possible (manual override, the controller will read the new tilt setting). The module has one male AISG connector, which is the control access, and one female AISG connector to allow the link of a separate RET antenna in daisy-chain. Technical Data Input control port
Importing a 3D Component onto a PCB Launch Model - Amphenol RF
component or enable materials override in the HFSS design settings. Note that although the internal geometry is hidden, it will still simulate as normal. 8 A small amount of solder is already modeled on the center pin, but if an accurate solder
RET Control Units - Amphenol Antenna Solutions
all the tilt indicators remain visible and manual change of the tilt is still possible (manual override, the control-ler will read the new tilt setting). The module has one male AISG connector, which is the control access, and one female AISG connector to allow the link of a seperate RET antenna in daisy-chain. Technical Data Input Control Port
gs-20-0327 - Amphenol CS
key features are present, it is possible to forcibly override these features. Forces greater than 30N should be avoided when inserting the plug. If the plug stops before being fully installed, confirm proper orientation prior to completing mating. Proper orientation is achieved when the latch of the plug is aligned with the latch windows of the ...
Importing a 3D Component onto a PCB Launch Model - Amphenol RF
component or enable materials override in the HFSS design settings. Note that although the internal geometry is hidden, it will still simulate as normal. 8 A small amount of solder is already modeled on the center pin, but if an accurate solder
Telaire Demand Control Ventilation Q&A - Amphenol
trol. Many economizer controllers will override the demand controlled system if free cooling is available during periods of low occupancy. What are the energy savings versus no control at all? What is the payback? Typical energy savings range from $0.10 to $0.50 per square foot depending on ventilation require-
RET Control Units - Amphenol Antenna Solutions
possible (manual override, the controller will read the new tilt setting). Technical Data Input control port Two male AISG 8 pin connectors (type IEC60130-9 Ed 3.0) for control data and power supply of each internal sub-unit. Daisy chain port None (daisy chain of RET units by external splitter)
RET Control Units - amphenol-antennas.com
possible (manual override, the controller will read the new tilt setting). Technical Data Input control port Two male AISG 8 pin connectors (type IEC60130-9 Ed 3.0) for control data and power supply of each internal sub-unit. Daisy chain port None (daisy chain of RET units by external splitter)