Search Results for dr. martin richman
Press - Lutze Inc.
Wolfsburg - numerous invited guests, including the German Federal Minister for Education and Research, Prof. Dr. Johanna Wanka, obtained information on the specific implementation of the research work ... July 11, 2013 . Read more . NEW: 100 A power package for Din rail mounting
mm - amphenol-cs.com
Dr B.Beirinckx 2002/06/30 0.X 0.3 size Scale TOLERANCES UNLESS OTHERWISE SPECIFIED www.fciconnect.com ISO 1302 ISO 406 ISO 1101 mm ROHS INFORMATION: surface 0.8 tolerance std projection-This product meets European Union Directives and other country regulations as described in GS-22-008.
How MIL-DTL-38999 has Advanced Military Technology
Amphenol Aerospace, under the Bendix Corporation, was instrumental in the development of MIL-DTL-38999. Bendix leveraged their extensive experience producing circular connectors dating back to World War II to spearhead the design of MIL-DTL-38999 Series I, Series II and Series III.
Wilcoxon Welcomes New Director of Sales - Wilcoxon Sensing Technologies
April 11, 2022 — Frederick, MD – Wilcoxon Sensing Technologies, an Amphenol company, announces the appointment of Chris Kramm to the position of Director of Sales, responsible for leading and growing the company’s condition monitoring business. Chris has been involved in the introduction and sales of new condition monitoring products and services for more than […]
Naval Defense - Amphenol Socapex
naval defense The technical challenges of interconnect systems. Compliance with Military Standards: Many defense naval projects require compliance with specific military standards, such as MIL-DTL-38999, which impose stringent requirements on connector performance and durability. Electromagnetic Interference (EMI): EMI can be a significant issue in naval vessels due to the presence of various ...
SpaceVPX VITA 78 Connector | Rectangular Connectors | Products ...
VITA 78 connectors, also known as SpaceVPX are specifically designed for use in space-based electronic systems. Amphenol’s VITA 78 SpaceVPX connectors leverage OpenVPX architecture and technology and are designed and tested for extreme space environments, extreme temperatures and vibration.
Duplex Filters DPF UHF/33-DR 3000 - AMPHENOL PROCOM
The DPF UHF/33-DR 3000 is a 6-cavity duplex filter designed to be built into the Motorola DR 3000 duplex base station/repeater. The DPF UHF/33-DR 3000 can be adjusted within the complete 406 - 470 MHz band. The duplexer can delivered with a 5 - 16 MHz spacing.
ETV38999 - Amphenol Aerospace
DR ˚ ˚ BSC ˚ CR BSC ˚ BR BSC ˚ AR BSC ˚ MAIN KEYWAY Shell Size Key & Keyway Arrangement Identification Letter AR° or AP° BSC BR° or BP° BSC CR° or CP° BSC DR° or DP° BSC 9 N* 105 140 215 265 A 102 132 248 320 B 80 118 230 312 C 35 140 205 275 D 64 155 234 304 91 131 197 240 11, 13, and 15 N* 95 141 208 236 A 113 156 182 292 B 90 ...
Split-Pair Quadrax Contacts - Amphenol Aerospace
Environmental Sealing: IAW connector specification Corrosion Resistance: 500 hours salt spray EMI Shielding: 360 degree shielding on each pair Mating Cycles: 500 cycles Voltage Rating: 500 Vrms max @ sea level Dielectric Withstanding Voltage: 500 VAC RMS sea level Temperature Range:-65C to 175C Data Rate: 6.5 Gbps. Voltage Rating: 500 Vrms max. @ sea level, DWV 1000 VAC rms between all inner ...
Centaur Blind Mate Rectangular | Products | Amphenol Aerospace
The Centaur, a Greek mythological creature, utilized the advantages of a human upper body and equestrian lower body to flourish. Like the mythological creature, Amphenol's Centaur interconnect utilizes the advantages of our extensive legacy of Mil-Spec connectors and the latest in high-speed contact and connector technology.
12 Channel 10/100/1G Base-T Managed Switch - Amphenol Aerospace
Amphenol's RESMLAC-12EMG-F35 is a MIL-STD rugged, Enhanced Managed military-grade Gigabit Ethernet switch, offering 12 Gigabit Ethernet Ports. Developed for harsh environment applications, the RESMLAC-12EMG-F35 features mechanical packaging enhancements designed for MIL-STD-810F airborne and ground environmental compliance and high reliability.
Market Connector: Achieving Commercial Viability for eVTOL Aircraft ...
Where: The development of eVTOL systems is taking place internationally as cities across the globe anticipate onboarding Urban Air Mobility (UAM) and Regional Air Mobility (RAM) into their transportation infrastructure. As of the start of 2024, there are more than 200 cities in more than 50 countries worldwide with plans to launch UAM and RAM initiatives.
Non-Environmental EMI/RFI - Amphenol PCDAmphenol PCD
Description: Offering 360-degree electromagnetic and radio frequency noise isolation shielding in addition to standard features available with the Non-Environmental type.
USA - AK - Process Technology, Inc. - Temposonics
1910 S. Stapley Dr. 41d80d34-c7c1-4f81-b908-4022fc5ff077. Global Contacts Toggle Sub Menu. Contact Authorized Repair Centers Request Information Toggle Sub Menu. Newsletter Suspension of Sales to Russia, Belarus, Donetsk and Luhansk. In light of the Russia-Ukraine conflict we have ceased the supply of our products to Russia, Belarus and the ...
Flexible Printed Circuit Board Solutions - Amphenol PCD
Description: Instruments engineered to provide a reliable method to fasten flexible printed circuit boards, and customized to fulfill the specific requirements of each project.
Peter Avitabile | PCB Piezotronics
Dr. Avitabile holds a Ph.D., MS, and BS in Mechanical Engineering from the University of Massachusetts Lowell, University of Rhode Island, and Manhattan College. He has 35 years of industrial and university experience in finite element modeling, experimental structural dynamic modeling, correlation of analytical and experimental data ...
Model DR | PCB Piezotronics
3425 Walden Avenue Depew, NY 14043. Sensorline SM 716.684.0001. info@pcb.com +1 800-828-8840
RADSOK® | Contacts | Products | Amphenol Aerospace
RADSOK® technology is based upon a stamped and formed flat grid, uniquely twisted into a hyperbolic geometry to provide robust, high-density contact to the mating pin contact.Most pin and socket technologies rely upon spring (beam element) properties of the contact elements, which tend to weaken over time. Unlike most other pin and socket solutions, the RADSOK® also utilizes the tensile ...
PCB > Learn > Videos
3425 Walden Avenue Depew, NY 14043. Sensorline SM 716.684.0001. info@pcb.com +1 800-828-8840
Overcoming Obstacles of Deep Space Travel - Amphenol Aerospace
It goes without saying that space is the most challenging operational environment known to man. As humanity embarks on a new era of space exploration, the threats to modern spacecraft and space launch systems are only going to grow as missions extend further and further out into space and embark into new environments like Mars and the lunar south pole — the site of future manned missions to ...