Search Results for earth or grounding testing
BDO BACKBOARD INSTALLATION GUIDE - Charles Industries
Verify/prepare earth ground. Always follow local codes and company practice when grounding cables/equipment. Per local company practice, verify the presence of an earth ground at the pedestal base. If earth ground is not present and local practice requires one, prepare one at this time. Do not connect earth ground to the backboard
CFDP EPS SERIES BACKBOARD CABLING INSTALLATION GUIDE - Charles Industries
The CFDP is a double-protected (dome within a dome), above-grade, pedestal that offers superior OSP protection against floods, fire, dirt, weather, insects, and impact for fiber-optic, buried, distribution cable splices and customer ser-vice drops in FTTP deployments.
− CMPH INSTALLATION GUIDE − Section LTCMPH-75-X-801
- GROUNDING WARNINGS - Always follow local codes and company practices for performing proper cable and site bonding and grounding, and perform all bonding and grounding prior to other electrical, fiber, and communications connections. - CABLE DAMAGE WARNINGS - Be careful not to damage any buried cables or service wires while digging either to ...
Model 1630-03C MANUAL S-BEAM LOAD CELLS Installation and ... - PCB
gh accuracy makes them ideally suited for critical weighing applications. S-type load cells are typically used to measure tensile loads, however, compression loads can also be measured when comp. ssion loads are guided and any resultant extraneous loads are mini.
Electromagnetic shakers operating guide - Wilcoxon Sensing Technologies
Make sure that any piezoelectric shaker being driven is properly grounded to a good earth ground. Disconnect the power cord at its source before connecting or removing any cables. To reduce the risk of electric shock, do not remove the power amplifier cover. No user-serviceable parts are inside.
Models N7FS, N8FS, and N8HFS Matching networks operating guide
Make sure that any piezoelectric shaker being driven is properly grounded to a good earth ground. Disconnect the power cord at its source before connecting or removing any cables. To reduce the risk of electric shock, do not remove the power amplifier cover. No user-serviceable parts are inside.
Model EX1503D01 Intrinsic Standard 300 psi port Installation and ...
Routine calibration of sensors and associated instrumentation is necessary to maintain measurement accuracy. We recommend calibrating on an annual basis, after exposure to any extreme environmental influence, or prior to any critical test.
ROTOR GROUND FAULT PROTECTION - PCB
Accumetrics’ EFREM – Earth Fault Resistance Monitor, RHM – Rotor Health Monitor, and GDS – Ground Detection System offer superior ground fault protection of motors and generators. Systems monitor for insulation faults on the field windings of generators and synchronous motors with brushless exciters.
Piezoelectric shaker operating guide - Wilcoxon Sensing Technologies
Make sure that any piezoelectric shaker being driven is properly grounded to a good earth ground. Disconnect the power cord at its source before connecting or removing any cables. To reduce the risk of electric shock, do not remove the power amplifier cover. No user-serviceable parts are inside.
Charles Multi-Purpose Housing (CMPH Installation Instructions
15. Prepare earth ground. Always follow local codes and company practice when preparing earth ground and when grounding cables or equipment. If an earth ground is not present at the CMPH site and local code or practice requires an earth ground, prepare one now. Attach ground lug on the ground plate (Step 21) using a ground wire of proper gauge ...
Charles Pedestal Base CFO-BAS-X-801 General ... - Charles Industries
Always follow local codes and company practice when preparing earth ground and when grounding cables/equipment. Per local company practice, prepare an earth ground for the pedestal at or near the base.
PA8HF power amplifier Operating guide - Wilcoxon Sensing Technologies
Make sure that any piezoelectric shaker being driven is properly grounded to a good earth ground. Disconnect the power cord at its source before connecting or removing power amplifier cables. To reduce the risk of electric shock, do not remove the power amplifier cover. No user-serviceable parts are inside.
Model HT354C10 Triaxial, thru-hole mtg, ceramic shear, miniature ... - PCB
Triaxial, thru-hole mtg, ceramic shear, miniature ICP® accel., 10 mV/g, 2 to 8k Hz, ground isolated, 5 ft. integral cable, +325 F operating temp Installation and Operating Manual For assistance with the operation of this product, contact the PCB Piezotronics, Inc. Toll-free: 716-684-0001 24-hour SensorLine: 716-684-0001 Fax: 716-684-0987
Electromagnetic shakers operating guide Models F3, F4, F5B, F10
Make sure that any piezoelectric shaker being driven is properly grounded to a good earth ground. Disconnect the power cord at its source before connecting or removing any cables. To reduce the risk of electric shock, do not remove the power amplifier cover. No user-serviceable parts are inside. Refer all servicing issues to Wilcoxon Research, Inc.
AC 2306–FL Six-Slot T1 Mini Repeater Apparatus Case - Charles Industries
The AC 2306–FL provides an installer grounding screw terminal at the bottom of the case for connection to earth ground (refer to Figure 5). The terminal is equipped with a 1/4” stud nut and washer and should be connected to an earth ground with a 14-gauge (minimum) wire.
Telemetry Systems | PCB Piezotronics
The Earth Fault Resistance Monitor (EFREM) and the Rotor Health Monitor (RHM) provide wireless rotor ground fault and temperature monitoring for generators and motors. The systems replace older slip ring contact ground fault detectors on any synchronous generator or motor.
Wilcoxon Research PA8HF power amplifier Operating guide
Make sure that the power amplifier is properly grounded to a good earth ground. 2. Make sure that any piezoelectric shaker being driven is properly grounded to a good earth
AEROSPACE GROUND TEST - PCB
Ground testing of rotary wing aircraft and space launch vehicles follows the same pattern. Testing and structural modeling must correlate on the ground to assure structural integrity and safety in subsequent flight tests.
SENSORS FOR SEISMIC TESTING AND INFRASTRUCTURE MONITORING - PCB
PCB® and Endevco® offer a diverse portfolio of sensors used for smart infrastructure worldwide, designed to measure earth tremors, foot, automobile and bridge traffic, trains and other seismic events that impart low frequency vibration. These vibratory loads accumulate as stress and may degrade the structures built to support them.
Seismic Sensors for Infrastructure Testing and Monitoring
PCB® sensors for infrastructure testing and monitoring are used by design engineers worldwide. We have thousands of seismic vibration sensors in stock, ready to ship, with lifetime warranty. Find, compare, and shop sensors and accessories online. Call 800.828.8840 24/7 or request a quote.