Search Results for effective thermal conductivity
MIL-ST Fiber Optic Connectors
Thermal shock MIL-STD-1678, Method 4020 Vibration MIL-STD-1344, Method 2005 Temperature humidity DOD-STD-1678, Method 4030 ... Whenever there is a need for superior cost-effective fiber optic systems and products that will stand up to demanding operating environments, you can rely on AFSI for engineering know-how, top-quality products and ...
Bantam Bayonet Lightweight Aerospace Connectors
Shell Conductivity: 2.5 mΩ max at 1.5 VDC and 1A: Insulation Resistance: 5000MΩ min at 500VDC for 1 min: Contact Resistance: 22mΩ max at 1A: Mating Cycles: 500 cycles: Vibration: 10-500-10 Hz, 180 mins applied on 3 axes: Thermal Shock: 5 cycles between -55°C & 125°C for an elapsed time of 70 mins: 5 cycles between -65°C & 150°C for an ...
LOCC-Box: First choice for circuit protection - Lutze Inc.
The LOCC-Box systems are installed in terminal boxes that control and monitor the district heat stations. The largest grids can comprise dozens of district heat stations and cover several square kilometres. It is therefore important to have effective and reliable protection for the various outputs (24 V DC) of a terminal box.
ExtremePort Z-Link Connector - Amphenol CS
design that is cost-effective, highly modular, scalable, and extremely easy to repair. TARGET MARKETS. ... § Thermal Shock: EIA-364-32, Method A Test condition 1, -55˚C to 85˚C (10 cycles) APPROVALS & CERTIFICATION ...
Critical Care Sensors | Respiratory / Sleep Apnea
Thermal Validation & Monitoring. Critical Care Sensors for Respiratory / Sleep Apnea. ... NovaSensor NPA Series of Surface-Mount Pressure Sensors is provided in a miniature size as a cost effective solution for applications that require calibrated performance. The sensor is intended for printed circuit board mounting and delivered in tape and ...
NovaSensor NPC-1210 Medium/Low Pressure Sensor
Thermal Accuracy–Span %FSO -0.5 — 0.5 3, 5, 8 Thermal Accuracy–Zero %FSO -0.5 — 0.5 3, 5, 8 Temperature ... The NPC-1210 series of solid-state pressure sensors are designed to provide a cost effective solution for applications that require calibrated performance over a wide temperature range. Keywords: Amphenol Advanced Sensors; NPC ...
General Fluid Temperature Sensor - Amphenol Sensors
We believe that making sustainable choices in the way we conduct our business creates short-term and long-term value for our stakeholders. We do not create long-term value by merely complying with regulations, but we go beyond compliance to find ways to green our operations and our products to ensure continuity of the material and human resources that we need to operate the business.
Custom Sensors for Product Integration | PCB Piezotronics
When your sensor requirements are not met by a commercial off-the-shelf product, partner with a reliable, cost-effective supplier with a history of success. PCB Piezotronics, Inc. has a proven track record in supporting mission- critical applications with sensors designed to detect, monitor, and quantify vibration, shock, force, pressure ...
P51 Pressure Sensor - Amphenol Sensors
We believe that making sustainable choices in the way we conduct our business creates short-term and long-term value for our stakeholders. We do not create long-term value by merely complying with regulations, but we go beyond compliance to find ways to green our operations and our products to ensure continuity of the material and human resources that we need to operate the business.
Industrial Hygiene | PCB Piezotronics
PCB ® manufactures sensors used by design engineers and predictive maintenance professionals to test and measure vibration, pressure, force, acoustics, load, and shock in research and development as well as industrial applications.. Divisions of PCB
SAS/PCIe® 5.0 (U.2 & U.3) Connectors - Amphenol CS
§ Thermal Shock: 10 cycles between -55°C to +85°C. per EIA 364-32, test condition I § Mixed Flow Gas: Expose ½ samples unmated for 7 days and then mated for 7 additional days; the other ½ samples are exposed mated for 14 days. per EIA 364-65, class II Exposed mated for 14 days. per EIA 364-65, class II A SPECIFICATIONS
Protimeter Moisture Meters
it was also an effective fungicide widely used in Continental Europe in wood preservatives. 1954: Protim Services Ltd was formed to undertake remedial work in buildings, such as wood treatment. 1955: Protim Ltd was formed by Gallwey to produce and sell only timber preservative chemical solutions. By this time, it was understood that the moisture
LUMINUS - amphenol-airlb.de
Thermal Shock-65˚C to 200˚C Vibration 30G Sinusoidal; 43.96G Random Shock 300G, 3msec, Half-Sine Salt Spray 5% Salt Spray @ 95˚C for 48 Hours Humidity 10 Days @ 25˚C to 65˚C, 90% - 95% RH Seal Rating IP67 RoHS & REACH Compliance Yes Fluid Immersion Lubricating Oil per Mil-Prf-7808 Cleaning Compound per Mil-Prf-87937, Alkaline Base
Coolant Temperature Sensor - Amphenol Sensors
We believe that making sustainable choices in the way we conduct our business creates short-term and long-term value for our stakeholders. We do not create long-term value by merely complying with regulations, but we go beyond compliance to find ways to green our operations and our products to ensure continuity of the material and human resources that we need to operate the business.
Termination Instructions - Amphenol Aerospace
L-Ref Number Part Number Subject Description; L-410 5015 5015 MS-E,F Series Connectors MIL-C-5015
Medical Archives - Amphenol Sensors
We believe that making sustainable choices in the way we conduct our business creates short-term and long-term value for our stakeholders. We do not create long-term value by merely complying with regulations, but we go beyond compliance to find ways to green our operations and our products to ensure continuity of the material and human resources that we need to operate the business.
Telaire CO2, Humidity and Temperature Products - Amphenol Sensors
We believe that making sustainable choices in the way we conduct our business creates short-term and long-term value for our stakeholders. We do not create long-term value by merely complying with regulations, but we go beyond compliance to find ways to green our operations and our products to ensure continuity of the material and human resources that we need to operate the business.
Automotive Sensors | HVAC
Thermal Validation & Monitoring. Automotive Sensors | HVAC Applications. Thermometrics Sensor Assemblies | SUF005A001 Dual Solar Sensor ... NovaSensor NPA Series of Surface-Mount Pressure Sensors is provided in a miniature size as a cost effective solution for applications that require calibrated performance. The sensor is intended for printed ...
H2-Low Pressure Sensor LPS - Amphenol Sensors
We believe that making sustainable choices in the way we conduct our business creates short-term and long-term value for our stakeholders. We do not create long-term value by merely complying with regulations, but we go beyond compliance to find ways to green our operations and our products to ensure continuity of the material and human resources that we need to operate the business.
Rugged Leap® On-BoardTransceiver (12TRx)
fastest, smallest and most cost effective optical transceiver module in the military and aerospace industry. Data-rates up to 16Gbps per channel ; 12 channels 192Gbps total throughput requires: 1‘‘x1‘‘ ofboard space 3.5W ofpower Case operational temperature [-40°C;+85°C] Shock MIL-STD 883: Method 2002.4 (500g; 1ms)