Search Results for equal rights amnedment
As of: January 29, 2025 Amphenol
Our Global Human Rights Policy unites our core policies related to human rights and reflects our belief in the principles stated in the UN Guiding Principles on Business and Human Rights, OECD Guidelines for Multinational Enterprises, Universal Declaration of Human Rights, and the International Labour Organization . As of: January 29, 2025
Anti-Human Trafficking and Slavery Statement - Amphenol Antenna Solutions
Amphenol has several policies that reflect our commitment to eradicate human trafficking and slavery in our operations and supply chain. In 2020, Amphenol issued its Global Human Rights Policy, which reflects our global commitment to human rights and the integration of this commitment into our operations and supply chains.
Anti-Human Trafficking/Slavery Statement - Halo Technology
Internal accountability standards help ensure compliance with Amphenol's policies. Annually, management employees are required to complete training and certify compliance with the COBCE. Amphenol's RLP sets forth our respect and support for human rights, and our SCOC and SRLP apply the same concepts to our suppliers.
Amphenol Supplier Responsible Labor Policy (EN)
Amphenol is committed to respecting human rights in our global operations and supply chain. This Supplier Responsible Labor Policy sets forth standards to ensure that supplier working conditions are safe and that workers are treated with dignity and respect.
LEV Charging Connectors and Inlet | Power Solutions | Amphenol
This standard aims to ensure interoperability between different brands of electric vehicles and charging infrastructure, making it easier for consumers to charge their e-scooters at public charging stations. IEC 62196-6 / IS 17017-2-6 (TYPE 6) FOR LEV CHARGING.
BEAD/BABAA Compliance BEAD/BABAA Compliance - charlesindustries.com
Charles Industries plays a vital role in supporting the BEAD (Broadband Equity, Access, and Deployment) program by offering BABAA-compliant products. With over 30 years of experience in broadband and optical network infrastructure, Charles Industries is uniquely positioned as a U.S. manufacturer with five operational facilities.
Understanding the Endevco Variable Capacitance Accelerometer Electrical ...
In addition to the output signal there can be a bias present, in some instances up to 3.6 volts, which will be detailed later in this paper. Endevco VC accelerometers are ideally suited for operation with piezoresistive bridge signal conditioners found in many modern data acquisition systems.
Amphenol Communications Solutions Pioneers Innovation: Launches Two ...
Type 6 Charging Gun and Inlet: Streamlining EV Charging, One Plug at a Time. The Type 6 Charging Gun and Inlet, also called the LEV Charging Connectors and Inlet is design compliant with IEC 62196-6/IS17017-2-6 standard with 2 power and 5 signal configurations. This connector can carry a continuous current up to 100A with 10,000 mating cycles.
Amphenol Corporation - Financials - SEC Filings - SEC Filings Details
PDF Format Download (opens in new window) Excel Format Download (opens in new window) XBRL Format Download (opens in new window) XBRL Format Download (opens in new window)
Press-fit Connectors: Challenges in Circuit Board Assembly - Positronic
Attaching electrical contacts to printed circuit boards (PCB) is a complex process. Establishing solid, reliable connections on a somewhat delicate and often crowded circuit board, without damaging or compromising it, constitutes a technical challenge.
F331-1A7H1-21018-E200 | Flex 0.50mm | Amphenol
Amphenol is one of the leading manufacturers of Flex Connectors. Contact us today for more details of Flex 0.50mm, part number F331-1A7H1-21018-E200.
Exploring Autolock FFC/FPC Connectors - Amphenol CS
Among these innovations, Amphenol's Autolock FFC/FPC (Flexible Flat Cable/Flexible Printed Circuit) connector stands out. With its ingenious design, robust features, and versatile applications, this range of products provide secure connections, excellent retention force, and effortless auto-locking mechanisms.
Learn About Connector Termination Styles - Amphenol CS
Most applications require a particular type of termination to match design requirements. This article provides insight into the common type of connector terminations. Though-hole terminations were very common in the early days, where the connector contacts or leads pass through a hole in the PCB.
Item # AJ-156, Audio Jack - Amphenol NEXUS Technologies
Browse Item # AJ-156, Audio Jack in the Amphenol NEXUS Technologies catalog including Item #,Item Name,Description,Number of Contacts,Application,Overall Diameter,Overall Length,Standard,Alternate P/N,Connector Style,Contact Types,Strain Relief,Shell
The Next Generation Auto Standard - Amphenol CS
Amphenol ICC’s Minitek MicroSpace ™ Crimp-to-Wire connector platform's unique design enables LV214 Severity-2 and performs at 1.8, 1.5 and 1.27mm pitch. It has many advantages over its USCAR certified counterparts. The Minitek MicroSpace ™ has an operating temperature of 130̊ C which makes it suitable to be even used inside an engine.
DIN 41612; Up with Robust Design Improvements - Amphenol CS
DIN 41612 is a comprehensive backplane offering from Amphenol ICC with a legacy of nearly five decades. With a broad range of DIN 41612 styles; these connectors has an edge over other backplane connector solutions in terms of mass deployment specifically in Industrial and Instrumentation sectors.
The Brain of Modern Vehicles: Understanding Car Computing
By analyzing data from the engine and other components, the CCU can make adjustments that improve fuel efficiency and reduce emissions, contributing to a more sustainable driving experience. Car computing represents a convergence of various electronic systems that work together to enhance vehicle performance, safety, and user experience.
PCIe® Gen 7.0 Doubles Data Rate to 128 GT/s For Data-Intensive Markets
PCIe ® Gen 7 will deliver a raw bit rate of 128 GT/s, enabling bi-directional data transfer rates of up to 512 Gb/s when configured as x16. Compared to the PCIe ® 6, which had only 64 GT/s raw data rate and up to 256 Gb/s via x16 configuration. The specification employs PAM4. This is the same as the PCIe ® 6.
Amphenol @ 2024 OCP Global Summit
Amphenol, a leading global provider of interconnect solutions, is set to participate in the 2024 OCP Global Summit. Amphenol will be showcasing its high-end technology contributing to the Open Compute technology, engaging in dynamic dialogues, conducting demos and interactive sessions.
RAM Advancements - From SDR to DDR4 and More - Amphenol CS
Most applications are rolling out the previous version to update with DDR4, as this advanced version offers many advantages over the others. With a data rate of 2GB to 16GB, it enables large capacity subsystems. The DDR4 standard allows for DIMMs of capacity, up to 64GB when compared to a maximum of 16GB per DIMM of DDR3.