Search Results for errorbar plot
ISO 9001:2015 - Amphenol CS
961 (Plot 88A), Jalan Perindustrian Bukit Minyak, Kawasan Perindustrian Bukit Minyak, MK 13, 14100 Simpang Ampat, Pulau Pinang, Malaysia. Bureau Veritas Certification Holding SAS – UK Branch certifies that the Management System of the above organisation has been audited and found to be in accordance with the requirements of
Board-to-Board - SV Microwave
The below plots show typical VSWR variation from DC to 18 GHz for an SMP Female-Female bullet under radial and axial misalignment conditions. Figure 4: Effect of Radial Misalignment (degrees) on VSWR for an SMP Female-Female Bullet
PCB Piezotronics | Measure vibration, pressure, force, and more
PCB Piezotronics | Measure vibration, pressure, force, and more
Amphenol Aerospace
CutplaneTemperature Plot: Mid-width of Aldrin Sandia Config., 23°C • There is a 2°C temperature gradient from the Aldrin top case to the primary frame. • There is a 1°C temperature gradient from the CPU top case to the primary frame. • These temperature gradients are significantly lower than the baseline.
ADVANCED BOLT TORQUE AUDIT YIELDS BOLT TENSION DATA - PCB
Figure 1: Clamp Load-Angle Plot Figure 2: Torque Angle Plot Figure 3: Torque-Tension Combined Scaled Plot . 3 The torque and clamp load plots match up precisely when the ordinates are scaled. This relationship for the linear portion of the torque-angle curve can be used to directly calculate the
Echo® Wireless Vibration Monitoring System - PCB
Stand-alone Echo® Sensors and EchoPlus® Junction Boxes can be mixed and matched as desired. EchoPlus® and optional RV Echo® provide a raw vibration output via cable to a data collector for detailed fault analysis. Echo® Monitoring Software provides standard monitoring features such as: machine status, reports, trend plots and email alerts.
Proximity Probe Cabling Errors Ebook - pcb.com
and the orbit plot of the shaft to determine if the shaft is out of balance or misaligned. Sometimes loading causes a vibration issue with the shaft. When those situations arise, unexpected outages occur that can cost companies millions of dollars. Proximity probes are most commonly checked through the API 670 method of static calibration.
MachineryMate 800 operating guide - Wilcoxon Sensing Technologies
motors, fans and bearings). The meter displays vibration frequency plots and allows vibration severity and bearing condition to be monitored. The MAC800 also has an optional strobe attachment for determining machine speed and optional Bluetooth connected headphones for listening to bearing noise. 1.1 Control buttons
Microphone & Acoustics FAQ | PCB Piezotronics
Frequently Asked Questions Microphones & Acoustics. Get your most commonly asked acoustics questions answered. Section I: Definitions and Terminology Section II: Microphone Recommendations Section III: Calibration and Testing Section IV: Specification Clarifications Section V: Specialty Microphone Applications Section VI: Maintenance and Handling If you don’t see the answer to your question ...
FASTENER TESTING SYSTEMS - PCB
of-turn plot, signature analysis can be used to evaluate bolted joints for loss of preload due to settling, creep and relaxation, or vibration and dynamic loading. In addition, joint strength problems such as thread strip and embedment of bearing surfaces and material yield within the bolted joint are easily identified.
FOR THREADED FASTENER TESTING FASTENER DRIVE SYSTEMS - PCB
for data reports and plots. pcb.com | 1 716 684 0001 RS SERIES FASTENER DRIVE SYSTEMS Available in a variety of speed and torque configurations Complete system provides precise and accurate torque and speed required for threaded fastener testing System can be supplemented with torque multipliers to extend torque or speed range
PCB Piezotronics | Measure vibration, pressure, force, and more
Trend plots Status Alarms Reports Echo' sensor configuration utilities MS SOL Server 2005 Actual distances can vary widely based on conditions Typical Configuration I EchoPlus@ Wireless Junction Box Receiver has DHCP or static IP addressing Optional high gain antenna EchoT Receiver Monitored Machinery Wired Sensor Traditional. Wired Sensor
Fastener Testing | PCB Piezotronics
Tightening, audit, and release angle signatures for a given bolted joint can be displayed and printed. After careful review of the applied torque vs. angle-of-turn plot, you can use signature analysis to evaluate bolted joints for loss of preload due to settling, creep and relaxation, or vibration and dynamic loading.
MachineryMate 200 operating guide - Wilcoxon Sensing Technologies
motors, fans and bearings). The meter displays vibration frequency plots and allows vibration severity and bearing condition to be monitored. 1.1 Control buttons Turn the meter on by pressing the POWER button. The unit will automatically turn off if not used for 1 minute (this time period can be increased up to 60 minutes using the Setup Wizard).
Model EX600B14 | PCB Piezotronics
Calibration of industrial accel. with full frequency response plot and NIST-traceable certificate: 1: 081A99: Socket head cap screw, 8-32 x 0.5" long, 18-8 stainless steel: 3: Product Documents. Product Specifications Product Manual Product Drawing CSA Certificate of Conformance ATEX ...
Calibration of Industrial Accelerometers for PDF - PCB
on the calibration service required) to develop a sensitivity plot. In the case of a test sensor being tested at multiple frequencies, the calibration service confirms the linear sensitivity response of the test sensor over the useable frequency range during pre-calibration.
Detecting Rolling Element Bearing Faults Using the ECHO Wireless ... - PCB
Figure 7 – True Peak Acceleration Trend Plot of Faulted Bearing . The True Peak Acceleration trend plot (Figure 7 above) clearly shows high amplitudes exceeding the alarm levels of the faulted rolling element bearing. When the bearing was replaced, the vibration smoothed out well below the warning alarm level.
PERFORMANCESPECIFICATION ISOTRON TRIAXIAL ACCELEROMETER 7253D-XXX - PCB
the magnitude of constant current, as shown in Load Capacitance vs. Frequency Plot. • Bias decoupling capacitor CBD and load resistor RL can be determined from: 1 . where f is the lowest frequency of interest. f-3 dB = 2 π RL CBD . CONNECTION DIAGRAM, EACH CHANNEL: C CABLE CURRENT SOURCE C R ACCELEROMETER + - - BD + L C:
Cooling Tower Application Study - Wilcoxon Sensing Technologies
Finally, a waterfall plot tracked throughout the year showed the continuous increase in amplitude of both the gear-mesh frequency and sidebands. The gearbox was replaced at the first opportunity and replaced with a spare while repairs were made. (page 3)
TORQUE-ANGLE-TENSION TESTING & ANALYSIS OF THREADED FASTENER ... - PCB
Variety of Plots – After the test is completed, rundown data and plots may be viewed on the computer display, printed as hard copy, and/or saved for later data analysis. Numerous configurable plots can be generated. Complete Test Systems – A complete torque-tension test system will typically include a rotary torque-angle transducer,