Search Results for fci asia
FIBER OPTIC SOLUTIONS
Amphenol Fiber Systems International, Inc. 1300 Central Expressway North, Suite 100 Allen, TX 75013 Phone: 214.547.2400 - 800.472.4225 Fax: 214.547.9344
Amphenol-BSI Overview - Wilcoxon Sensing Technologies
— Asia Test Design Services Printed Circuits Connectors PCBA, Backplane & Integration Cable, Bus Bar & Power Design expertise Assembly agility Test excellence ABSI has the unique ability to leverage all of Amphenol’s Interconnect products and design technology to produce best in class vertically Integrated systems solutions
Press-Fit Connectors - Positronic The Science of Certainty
As you might have guessed from their name, press-fit connectors are pressed through properly dimensioned plated-through holes on a printed circuit board (PCB). This technology is an alternative to the soldering method and offers a number of advantages over its more traditional counterpart.
Amphenol at ODCC Summit 2022
The annual ODCC Summit is one of China’s leading Data Center events. Amphenol as an active member of the ODCC Committee will showcase our latest technologies, solutions, and achievements in the China data center industry this year. The 2022 ODCC Summit will be held in Beijing International Conventi
Meet Us at ODCC Summit 2021 - Amphenol CS
Open Data Center Committee (ODCC) Summit is one of China’s leading Data Center events. ODCC is a voluntarily formed non-profit social organization constituted by the enterprises and organizations associated with data center. They focus on creating an open data center platform in China that promotes infrastructural development and standardization of Internet along with improving the process ...
About - Amphenol
Amphenol is one of the world’s largest providers of high-technology interconnect, sensor and antenna solutions. Our products Enable the Electronics Revolution across virtually every end market, including Automotive, Broadband Communications, Commercial Aerospace, Defense, Industrial, Information Technology and Data Communications, Mobile Devices and Mobile Networks.
Heavy Duty, Multi-Pin, Plastic or Metal Connectors, Cable Assemblies ...
America and Asia, our Team will work with you to design the most cost-efficient and reliable interconnect system available. 1 of 4 IP67 IP69K IP65 IP68 A Series™ - Specifications Overview (See individual Series for exact specs) IP Rating Range IP65, IP67, IP68, IP69K (in mated condition) Max. Current Amperage Range 7.5A - 180A
암페놀-대신전자정밀(주)
About Us. 암페놀-대신전자정밀(주)는 Amphenol Corporation의 한국 법인으로, 산업용, 군수용, 이동 통신 및 철도 차량용 커넥터를 주력 제품으로 생산하고 국내 시장 뿐만 아니라 수출 및 해외 암페놀 법인의 제품을 한국 시장에도 공급하는 공식 자회사입니다.
Amphenol at ECOC Exhibition 2022
Optical fibers are being redefined with the continuous requirement for increased bandwidth. This evolution is showcased at the ECOC Exhibition. The European Conference on Optical Communication (ECOC) continues to be Europe's largest Optics event and one of the most esteemed events on optical communi
Amphenol at OCP China Day 2022
Come visit us at OCP CHINA DAY, Booth #B09 at the Beijing Kerry Hotel, on August 10th, 2022. Please use our special invite code “AMPHENOL” to register for the conference.
Amphenol New Product Updates – March 2021
The FLB series cover couples with the base to provide IP66 protection (per IEC 60529) for the mated photocell/control assembly. Domes are available in Grey, Clear, Red, Black, White and Translucent colors in 35mm, 50mm, 60mm, 75mm, 100mm & 130mm heights. The mating gaskets and O-rings on the bases ensure IP66 rating performance to protect equipment from moisture ingress.
Come Visit Amphenol at OCP Global Summit 2022
Amphenol is excited to exhibit at the 2022 OCP Global Summit, the largest gathering of key decision-makers, executives, engineers, developers, and suppliers who support open source and open collaboration in hardware and software.. The theme for this year is “Empowering Open”. From hyperscalers to enterprises and government, today everyone is looking at open collaboration from researching ...
Sensors for Healthcare Applications Becton Dickinson (BD)
Asia ROW Europe FINLAND % Sales By Region PUERTO RICO MACEDONIA SWITZERLAND (1) POLAND (1) INDONESIA. Amphenol Confidential & Proprietary Amphenol Divisions Confidential –Not for Distribution 4 Amphenol AICC Information Communications Commercial 110+ Companies 40+countries Over 74,000 Employees AMAO Military ...
Learn More about Connector Mating Cycles - Amphenol CS
The mating cycles of a connector are directly related to its resistance. If a connector has a low threshold, it indicates fewer mating cycles, while the ones with higher threshold will have a longer life in terms of mating.
Ø11mm “FCI”interface airbag connector (CA291B) - Airbag connector and ...
As a member of Amphenol Automotive products group, Amphenol Automotive Connection Systems (Changzhou) Co., Ltd., established in 2004, is a wholly owned subsidiary of Amphenol Group in China. Through more than 10 years of efforts, our company has formed six major business units and ten major product groups, including airbag connectors and harnesses, automotive buckle harnesses, automotive ...
DDR SDRAM - Evolution of High-Performance Volatile Memory - Amphenol CS
DDR- SDRAM stands for Double Data Rate - Synchronous Dynamic Random Access Memory and it is a common type of memory used-organized RAM in most of the processors.
Connectors - Positronic The Science of Certainty
Since 1966, Positronic has provided highly reliable and efficient connectivity solutions to customers around the world. Our catalog includes power, D-subminiature, circular, rectangular, and custom connector products and accessories, as well as value-added services.
Fundamentals of Board-to-Board Connectors - Amphenol CS
Board-to-board (BTB) connectors are one of the most popular forms of connectors that connect signals between two printed circuit boards (PCBs) without a cable.
The Evolution of PCI Express® - Amphenol CS
Earlier in 2019, PCIe® introduced its latest version, PCIe® 5.0, with 32GT/s transfer rate and 30Gb/s throughput per lane. It also has improved signal integrity and is backward-compatible with CEM connectors for add-in cards.
Components of a Control Cabinet - Amphenol CS
Control cabinets are vertical enclosures with servo drives and other electromechanical components that control or monitor machinery and factory systems associated with it. The control cabinet is a stainless steel box, which can either be wall-mounted or a standalone module on the floor.