Search Results for film once
Model 117B25 CONFORMAL BALLISTICS PRESSURE SENSOR Installation ... - PCB
Once the proper thickness spacer is found, removal and re-installation now becomes a routine matter. 3.0 INSTALLATION 3.1 PORT PREPARATION Prepare mounting port in accordance with installation drawing 117-20 (XX)-90 supplied as part of this manual. NOTE: The installation port for the 117B is identical to that for the 117A.
Repair and Maintenance Returning Equipment Contact Information ... - PCB
Thick Film Substrate O O X O O O Wires O O O O O O Cables X O O O O O Plastic O O O O O O Solder X O O O O O Copper Alloy/Brass X O O O O O This table is prepared in accordance with the provisions of SJ/T 11364. ... Once communication is established, the indicator box will turn green and the software will read the
Model 685B0001A11 Electronic vibration switch, internal ICP ... - PCB
terminate the wire in the correct location. Once connected, tug lightly on the wire to confirm connection is secure. Pin Location Diagram- Models with Internal Accelerometer and Triac Relays Pin Category Description 1 AC Power + Power 2 - Power/Common 3 Earth Ground (Also connect to enclosure safety lug) 4 Alarm Output Main Terminal 1
Model 691C42 Vibration Switch Box Installation and Operating Manual - PCB
corner. Once the mounting brackets are positioned properly, they should then be fastened to the box with the provided screws. Hardware for fastening the mounting brackets to the installation surface are to be provided in the field. Painted steel and stainless steel boxes include two factory-installed mounting brackets on the top and bottom of ...
Model 117B118 CONFORMAL BALLISTICS PRESSURE SENSOR Installation and ...
Once the proper thickness spacer is found, removal and re-installation now becomes a routine matter. 3.0 INSTALLATION 3.1 PORT PREPARATION Prepare mounting port in accordance with installation drawing 117-20 (XX)-90 supplied as part of this manual. NOTE: The installation port for the 117B is identical to that for the 117A.
Fiber Optic Terminus End Face Quality Standards
Mode) Terminus Type Radius of Curvature Fiber Height Apex Offset Physical Contact 7 to 25mm +50nm to -125nm <50um Angled Physical Contact 7 to 12mm +100nm to -100nm < 50um
Model 117B104 Conformal ballistics pressure sensor, 50 Caliber ... - PCB
Once the proper thickness spacer is found, removal and re-installation now becomes a routine matter. 3.0 INSTALLATION 3.1 PORT PREPARATION Prepare mounting port in accordance with installation drawing 117-20 (XX)-90 supplied as part of this manual. NOTE: The installation port for the 117B is identical to that for the 117A.
Model 699B02 Hand Held Shaker Installation and Operating Manual - PCB
Thick Film Substrate O O X O O O Wires O O O O O O Cables X O O O O O Plastic O O O O O O Solder X O O O O O ... Continuous Use Option Switch: In this mode, once the shaker is turned on, it does not shut off until the On/Off button is depressed a second time. The default position of this switch is Auto; the unit turns off
Model 685B0011A11 Electronic vibration switch, internal ICP ... - PCB
terminate the wire in the correct location. Once connected, tug lightly on the wire to confirm connection is secure. Pin Location Diagram- Models with Internal Accelerometer and Triac Relays Pin Category Description 1 AC Power + Power 2 - Power/Common 3 Earth Ground (Also connect to enclosure safety lug) 4 Alarm Output Main Terminal 1
Model 480B21 3-channel, Battery-powered, ICP® Sensor Signal ... - PCB
[6]Use BNC's or Triax connector, not both at once. Cover all unused connectors with black ESD protective caps. [7]See PCB Declaration of Conformance PS024 for details. Date: 03/02/2020 Date: 03/02/2020 Date: 03/02/2020 Date: 03/02/2020 15125 Entered: RB Engineer: CPH Sales: KK Approved: DY Spec Number: 3425 Walden Avenue, Depew, NY 14043
Model 685B1001A41 Electronic vibration switch, remote 100 mV/g ... - PCB
terminate the wire in the correct location. Once connected, tug lightly on the wire to confirm connection is secure. Pin Location Diagram- Models with Internal Accelerometer and Triac Relays Pin Category Description 1 AC Power + Power 2 - Power/Common 3 Earth Ground (Also connect to enclosure safety lug) 4 Alarm Output Main Terminal 1
Model 394C06 Platinum Stock Product Handheld shaker, 1g at 159.2 ... - PCB
Continuous Use Option Switch: In this mode, once the shaker is turned on, it does not shut off until the On/Off button is depressed a second time. The default position of this switch is Auto; the unit turns off automatically after 90 seconds. Peak/RMS Selection: If a 100 mV/g sensor is on the shaker table, and the unit is in peak mode, then the
Brian Engle - amphenol-sensors.com
amounts of electrical energy. During charging a degraded cell with a diminished capacity presents a danger that once it has reached its full charge it will become overcharged while the rest of the cells in the pack reach their full charge. This can cause temperature and pressure build -up within the cell and possible damage.
IMI Sensors: Industrial Monitoring Instrumentation - PCB
IMI Sensors, a division of PCB Piezotronics, is a global designer and manufacturer of industrial vibration monitoring instrumentation such as accelerometers, vibration transmitters and switches.
Model 117B13 Installation and Operating Manual - PCB
Once the proper thickness spacer is found, removal and re-installation now becomes a routine matter. 3.0 INSTALLATION 3.1 PORT PREPARATION Prepare mounting port in accordance with installation drawing 117-20 (XX)-90 supplied as part of this manual. NOTE: The installation port for the 117B is identical to that for the 117A.
Model 117B25 Conformal ballistics pressure sensor, 356 T S & W, 9 ... - PCB
Once the proper thickness spacer is found, removal and re-installation now becomes a routine matter. 3.0 INSTALLATION 3.1 PORT PREPARATION Prepare mounting port in accordance with installation drawing 117-20 (XX)-90 supplied as part of this manual. NOTE: The installation port for the 117B is identical to that for the 117A.
Model 117B44 Installation and Operating Manual - PCB
information must be taken only once and only with increasing pressure. A repeat run on the same cartridge case will not yield the same values as the initial run due to work hardening of the cartridge case metal. Figure 4 At the lower pressures, the sensor has very little output because there is a certain amount of clearance between
Automotive manufacturing accelerometer applications
– Once initiated, it will spread with continued operation – It will always be accompanied by a marked increase in vibration • Remedied by replacing the bearing or redesigning with a bearing that has a greater calculated fatigue life 10 Automotive manufacturing accelerometer applications Sept. 2017 | Wilcoxon Sensing Technologies proprietary
Protimeter MMS3 | 4-in-1 Moisture Meter with Infrared
Gross Weight: Instrument only with batteries. 10.9 oz (309 g) Regulatory Compliance: CE RoHS ETL UKCA. Plug-In Surface Temperature Probe (BLD5806) Range: 32°F to 158°F (0°C to 70°C)
Model 117B22 Installation and Operating Manual - pcb.com
information must be taken only once and only with increasing pressure. A repeat run on the same cartridge case will not yield the same values as the initial run due to work hardening of the cartridge case metal. Figure 4 At the lower pressures, the sensor has very little output because there is a certain amount of clearance between