Search Results for fluke 124b recording time base limit
Selecting & Installing Accelerometers - PCB
which limits its application in high shock environments. The compression design is generally the simplest and easiest to under-stand. The crystal, quartz or ceramic, is sandwiched between the seismic mass and the base with an elastic pre-load bolt. Motion (vibration) into the base squeezes the crystal creating an output. Compression designs
SCU User Guide Version 3 - Amphenol Antenna Solutions
The System Time Setting function is used to set the system date and time. It is important to set the system date and time correctly as this information will appear on the Access Log report and the Site Summary report. The time is 24-hour format. 1. Click the [Set] button on the System Time Setting to initiate the
Piezovelocity transducer - wilcoxon.com
Vibration limit 250 g peak Shock limit 5,000 g peak Electromagnetic sensitivity, equiv. in/sec 50 µin/sec/gauss Sealing hermetic Base strain sensitivity 0.0005 in/sec/μstrain Weight 145 grams Case material 316L stainless steel Mounting 1/4-28 tapped hole Output connector 2 pin, MIL-C-5015 Mating connector R6
Level Plus - Temposonics
MTS Sensors Level Plus® Liquid-Level Transmitters M-Series Model MG Digital Transmitter Operation and Installation Manual, Document Number 550791 Revision N (EN) 02/2016 GERMANY GENERAL: Tel.: +49-2351-9587-0 Fax:+49-2351-56491
Home-Run Configuration Installation Instruction Instruction
of an earth ground at the pedestal base. If earth ground is not present and local practice requires one, prepare one at this time. Do not connect earth ground to the backboard until it is reattached to the base. Preparing the Feed Cable (Tail of the Terminal Block) 7 . Choose proper sized terminal block. Per local company practice, use a correct-
Temposonics
6 Temposonics® R-Series SSI Operation Manual Temposonics® R-Series SSI Operation Manual Measurement contents (optional: box no. 20) Note: Choose “9” in box no. 18 and 19. 1 Position measurement 2 Differentiation measurement 4 3 Velocity measurement 4 Position measurement + temperature measurement (only with data length = 24 bit)
355M73 ICP® ACCELEROMETER Revision: C - pcb.com
Overload Limit ± 5000 g pk ± 49,050 m/s² pk ... Base Strain Sensitivity 0.008 g/µε 0.08 (m/s²)/µε [1] Electrical Excitation Voltage 20 to 30 VDC 20 to 30 VDC Constant Current Excitation 2 to 20 mA 2 to 20 mA Output Impedance ≤ 300 Ohm ≤ 300 Ohm Output Bias Voltage 8 to 12 VDC 8 to 12 VDC Discharge Time Constant 0.07 to 1.0 sec 0.07 ...
Force FAQ | PCB Piezotronics
Frequently asked questions about PCB’s Quartz Force Sensors.
Network Management System and ICB Management System Software User’s Guide
Login Time Out Set the amount of time the system will wait before logging the user out auto-matically. Change Supervisor Password Change the supervisor password. The Default password is 123. The maxi-mum password length is 6 characters. Log file store date Select the number of days to keep the log file. The system will automatically
Temposonics
B Base unit for threaded flanges »M« and »T« (replacement only) M Threaded flange with flat-face, M18×1.5-6g T Threaded flange with raised-face, ¾"-16 UNF-3A GB with pressure fit flange J Housing material stainless steel 1.4305 (AISI 303), rod material stainless steel 1.4301 (AISI 304) Pressure fit flange Ø 21 mm, Ø 12.7 mm rod, 800 bar
High frequency IEPE accelerometer - PCB
Warm-up time (to 10% of final bias level) sec < 3 Environmental characteristics Temperature range -67˚F to +257˚F (-55˚C to +125˚C) Humidity Hermetically sealed Sinusoidal vibration limit g pk 2000 Shock limit [1] g pk 10 000 Base strain sensitivity Screw mounted eq. g pk/μ strain 0.8 Adhesive mounted eq. g pk/μ strain 0.0004
Model 3741B122G DC Response Accelerometer Installation and ... - PCB
the limit requirement of GB/T 26572. Lead is present due to allowed exemption in Annex III or Annex IV of the European RoHS Directive 2011/65/EU. 1 General ... stability over time. Compared to standard strain gages, silicon sensor accelerometers have a much higher gage factor. The sensor element of the 3741 series features a
STRAIN GAGE LOAD CELL - PCB
Overload Limit 37.5 klb 167 kN Load Limit(Side Force, F X or F Y) 12.5 klb 56 kN [3] Load Limit (Bending Moment, M X or M Y) 12.5k in-lb 1412 N-m [3] Load ... Model M084A101 TENSION LOAD BASE W/ M33X2 THD. Entered: DMW Engineer: JSD Sales: JC Approved: GLB Spec Number: Date ...
Model 356A44
%PDF-1.4 %âãÏÓ 17 0 obj > endobj 178 0 obj >/Font >/ProcSet[/PDF/Text]>> endobj 180 0 obj > endobj 170 0 obj >stream H‰´WM¯ · ¼ï¯àq÷0#~“s”"E± ' µ† >9± C àäà¿Ÿênr†äÎì{zÙ@ ßÌN³Yì.v _½ÿhÔÏÿ9½¹ž^]¯V uýé¤Õ2ÛÅ%5•¿Z…”fã•ós´êú+L~>M³ ~ÑCV×ßOߟ¿ùëeòËœÏß]¦ æpþËe2 ÓÎ×Ë”\ûÃ{XFX*ú²ÌËùO—iqøá[Xè0ûó;250 ...
Model 607A11/M020BZ Platinum Swiveler® Industrial ICP ... - PCB
O: Indicates that said hazardous substance contained in all of the homogeneous materials for this part is below the limit requirement of GB/T 26572. X: Indicates that said hazardous substance contained in at least one of the homogeneous materials for this part is above the limit requirement of GB/T 26572.
Model 378A12 | PCB Piezotronics
Model 378A12:1/4-inch pressure prepolarized 377A12 microphone, with 1/4-inch preamplifier 426B03 and TEDS programmed
Model 3711B1250G MEMS DC accelerometer, 40 mV/g, +/-50 g range, 0 ... - PCB
Model 3711B1250G MEMS DC accelerometer, 40 mV/g, +/-50 g range, 0 to 1000 Hz, integral cable Installation and Operating Manual For assistance with the operation of this product,
www.pctel.com
We would like to show you a description here but the site won’t allow us.
Intrinsically safe certified accelerometer 780A-IS
Vibration limit 500 g peak Shock limit 5,000 g peak Electromagnetic sensitivity, equiv. g, max 70 µg/gauss Sealing hermetic Base strain sensitivity, max 0.0002 g/μstrain Sensing element design PZT, shear Weight 62 grams Case material 316L stainless steel Mounting 1/4-28 UNF tapped hole Output connector 2 pin, MIL-C-5015 style Mating connector ...
Model M222B ICP® Force Sensor Installation and Operating Manual - PCB
for analysis or recording. ICP sensors, are powered from a separate constant current source, operate over long ordinary coaxial or ribbon cable without signal degradation. The low impedance voltage signal is not affected by triboelectric cable noise or environmental contaminants. Figure 1 - ICP Sensor System Schematic