Search Results for heat traced
All About QSFP Cables, Connectors, and More - Amphenol CS
Optional heatsinks and light-pipes are available. These get assembled with the cage to move heat away from the QSFP module or to get access to network activity, respectively. The heatsinks come in fin and pin styles and have three available heights: 4.2mm, 6.5mm, and 13.5mm.
SIGNAL TRANSMISSION ON LONG CABLE LENGTHS SENSORS - PCB
Step 3: Trace horizontally from the vertical axis position determined in Step 2 to an intersection with the ... the cable goes directly to power the internal electronics and will create heat. This may cause the sensor to exceed its maximum temperature specification. For this reason, do not supply excessive current over short cable runs or when ...
OverPass™- The High Speed Solution - Amphenol CS
Amphenol’s OverPass ™ cable system offers a broad range that allow customers to efficiently take high speed signal from near the ASIC to anywhere in their system.. Amphenol’s OverPass ™ cable system allows for the transfer of high-speed signals to twinax cables shortly after they are launched from the ASIC. This enables a simple, low-loss, direct link to pluggable modules or anywhere ...
Super-Trex® Ultra-Gard™ Portable Cord - TPC Wire
Flame and heat resistant. Extreme all-weather flexibility. Resources. Super-Trex® Ultra-Gard™ Portable Cord. Download Product Showcase - Super-Trex® Ultra-Gard™ Portable Cord. Watch Now Steel Coil vs. Super-Trex® Ultra-Gard™ Watch Video ...
Navigating the Speed of Tomorrow: Unveiling 224G High-Speed Solutions
Key features of OSFP1600 include its integrated heatsink design for superior thermal performance, capable of dissipating over 30 Watts of heat, and full backward compatibility with OSFP800. Additionally, it introduces cabled-connector footprints alongside the traditional surface mount (SMT) connector, enhancing deployment flexibility.
High Bandwidth Connectors for New Technologies - Amphenol CS
Even the slightest mismatches in impedance can lead to signal loss at high frequencies, which in turn will bring the performance of the application upside down. Furthermore, with increased signal density and data rates, the power density also spikes, increasing heat levels significantly, leading to thermal and cooling issues and related challenges.
Amphenol NAFI + UHD CONNECTORS
0.100” x 0.050” staggered grid - High density optimizes trace routing through the backplane Compliant press-fit termination of backplane connectors - Provides a gas-tight interface with the printed circuit backplane without ... Resistance to Solder Heat EIA-364-56 Procedures 3 & 4 Vibration (sinusoidal) MIL-DTL-202 Method 204, Test Condition G
Cordsets & Jacket Materials | Amphenol TPC Wire & Cable
Amphenol TPC offers a wide variety of cordset assemblies in various lengths and jacket materials to make replacing electrical control devices quick and simple.
Amphenol’s Connectivity Solutions for AI and ML
With multiple interface choices, AI and ML designers can optimize parameters such as signaling speed, density, and heat management according to their specific requirements. The extensive selection of high-speed external interfaces, including SFP, QSFP, QSFP DD, and OSFP, as well as cabled backplane interfaces like ExaMAX ® and Paladin ®.
Load Coils and Load Coil Cases - charlesindustries.com
inside each case are protected from moisture, heat, dirt and impact. 770-XXXX/XXX- XXMH SPXX’X Pair Count: 0025 = 25 Pair 0050 = 50 Pair 0100 = 100 Pair 0200 = 200 Pair 0300 = 300 Pair 0400 = 400 Pair 0450 = 450 Pair 0600 = 600 Pair 0900 = 900 Pair Coil Type 656-66 = 66mH 662-88 = 88mH Cable Stub Length 10 = 10 ft. 15 = 15 ft. 20 = 20 ft. 25 ...
Whip Antennas GF 401/... - amphenolprocom.com
If removal of antenna installation is necessary, a quick dismantling procedure leaves no trace of the installation. NOTE GF antennas are not suitable for car models with windows having heat reflective coating. Specifications. Electrical; Model: GF 401/... Frequency: 450 MHz band covered by three tunable models: Antenna Type: ½ λ Mobile ...
Whip Antennas GF 402/... - AMPHENOL PROCOM
If removal of antenna installation is necessary, a quick dismantling procedure leaves no trace of the installation. NOTE GF antennas are not suitable for car models with windows having heat reflective coating. Specifications. Electrical; Model: GF 402/... Frequency: 450 MHz-band covered by two tunable models: Antenna Type ...
Whip Antennas GF 402/... - AMPHENOL PROCOM
If removal of antenna installation is necessary, a quick dismantling procedure leaves no trace of the installation. NOTE GF antennas are not suitable for car models with windows having heat reflective coating. Specifications. Electrical; Model: GF 402/... Frequency: 450 MHz-band covered by two tunable models: Antenna Type ...
Microsoft Word - gs-12-390_a.doc
5.10 RESISTANCE TO SOLDER HEAT SECTION 6 TEST MATRIX PDS: Rev :A STATUS:Released Printed: Jan 28, 2011. Type PRODUCT SPECIFICATION NUMBER GS-12-390 TITLE PAGE REV. ... 2.5.5 Pad and trace design: pad and trace design shall follow PCI Express standard as depicted in customer drawing. PDS: Rev :A STATUS:Released Printed: Jan 28, 2011.
A Custom Wire & Industrial Cable Supplier | Amphenol TPC Wire
A Custom Wire & Industrial Cable Supplier | Amphenol TPC Wire
PS1&PS4-H2-4%-MOD HydrogenModule Datasheet - SGX Sensortech
will cause abnormal fluctuations in the trace data of the sensor, but generally it can fully adapt to the new environment and be stable within 5-10 minutes. 6. Maintain • The maintenance of the Hydrogen detection module is mainly for accuracy calibration. Generally, the solid polymer Hydrogen sensor does not
Whip Antennas GF 151 - amphenolprocom.com
If removal of antenna installation is necessary, a quick dismantling procedure leaves no trace of the installation. NOTE GF antennas are not suitable for car models with windows that have heat reflective coating.
Whip Antennas GF 900/1800 - amphenolprocom.com
If removal of the antenna installation is necessary, a quick dismantling procedure leaves no trace of the installation. NOTE: GF antennas are not suitable for car models with windows that have heat reflective coating. Specifications. Electrical; Model: GF 900/1800 ... the joined parts may be heat-treated with a warm-air gun.
200WX WeatherStation® Instrument - Airmar
Calculated dew point and heat index; GPS position, speed over ground, and course over ground; Three-axis, solid-state compass with dynamic stabilization; Three-axis rate gyro supplies rate-of–turn data; Three-axis accelerometer for best-in-class pitch and roll information; Housing IPX6 rated for water-ingress protection
Amphenol’s High-Performance COM-HPC Connectors
Amphenol connectors play a vital role in the Computer-on-Module for High-Performance Computing (COM-HPC) standard, which is designed to meet the increasing demands for high-speed data transfer and efficient power management in embedded systems. These connectors are engineered to support a wide range of applications, from industrial automation to military and medical devices, making them ...