Search Results for how does dlss work
5G Network Testing - Dynamic Spectrum Sharing - PCTEL
Dynamic Spectrum Sharing (DSS) technology allows operators to dynamically allocate bandwidth between 4G and 5G traffic requirements. With DSS, operators can deploy 5G more quickly while minimizing disruptions for 4G users. Watch this video to learn more about DSS and how operators can effectively test networks that use DSS technology.
GMT fuse panels: The unsung heroes - Blog - amphenol-ns.com
GMT fuse panels do a lot of work for fiber optic networks in a small footprint. They let engineers and technicians monitor network temperature, fuse and bus power stability.
Staying in time - Data acquisition and transmission with R-Series V SSI ...
How does SSI work? With SSI, the data is transmitted serially, whereby the controller specifies the time of the polling. During data transmission, the procedure described below is carried out (Fig. 1):
More on Radiation Patterns - Beamwidth - PCTEL
There are a few parameters that can be used to do this. The first is “3-dB Beamwidth” or “Half-Power Beamwidth”. The 3-dB Beamwidth is the angle between the points on the pattern where the gain is down from the peak by 3-dB.
Signal Conditioning Basics | PCB Piezotronics
For this reason, do not supply excessive current over short cable runs or when testing at elevated temperatures. Experimentally Testing Long Cables To determine the high frequency electrical characteristics involved with long cable runs, two methods may be used.
How Do Bandpass Filters Work? Real World Applications & More - Q Microwave
How do Bandpass Filters Work? In a previous article, we defined bandpass filters as a filter that removes specific noise frequencies from a signal without distorting the signal or adding extra noise. They have the ability to reject both low frequency and high frequency signals.
What is Mobile Statcom? - TPC Wire
How does a STATCOM work? These systems are based on power electronics technology and are equipped with fast-acting voltage regulation capabilities. They can respond to voltage changes within milliseconds, making them ideal for grid stabilization.
Staying in time – Data acquisition and transmission ... - Temposonics
How does SSI work? With SSI, the data is transmitted serially, whereby the controller specifies the time of the polling. During data transmission, the procedure described below is carried out (Fig. 1): 1. In the idle state, when no data is transmitted, the data line and the clock line are at the high level. 2.
Tackling Indoor 5G Coverage - rfstechnologies.com
HOW DOES THE RFS TECHNOLOGY WORK? In January 2022, we expanded our HYBRIFLEX portfolio to add three additional solutions. Each targets the specific challenges and requirements in active distributed antenna system (DAS), distributed radio system (DRS) and small cells deployments to enable the delivery of indoor and cross campus 5G connectivity.
Pros and Cons of an Analog Bandpass Filter vs. Digital Filter - Q Microwave
Analog filters work with signals in their inherent form. This continuous signal processing means that the analog signal’s waveform is preserved without being chopped into discrete samples, maintaining the original signal’s integrity.
Introduction to MEMS Accelerometers | PCB Piezotronics
When coupled with microelectronic circuits, MEMS sensors can be used to measure physical parameters such as acceleration. Unlike ICP® sensors, MEMS sensors measure frequencies down to 0 Hz (static or DC acceleration). PCB® manufactures two types of MEMS accelerometers: variable capacitive and piezoresistive.
Precision in Filtering: Cutoff Frequency's Role in Lowpass Filters
How does one exclude undesired high-frequency components and facilitate the passage of essential low-frequency signals through a lowpass filter? The answer lies in the meticulous selection and implementation of the cut-off frequency.
Question: What is the Difference Between SMA and Reverse Polarity SMA ...
Male SMA and Male RP-SMA connectors both feature their threads on the inside of the connector shell, i.e. they twist onto a female SMA or RP-SMA connector that feature their threads on the outside of the shell.
Impact and Drop Testing - PCB
Impact testing is performed to determine the energy absorbed or the energy required to fracture a unit under test (UUT). Take for example a straight-line collision, such as a car crash.
High-Speed QSFP Loopback Adapter Modules De-Mystified (Pt. 1) -- The ...
To do this test correctly, you need to select the QSFP+ or QSFP28 Loopback Adapter Module whose internal specifications are designed to most closely mimic the real-world performance of the cable style and length you plan on deploying. This is a critical consideration.
D-Subminiature (D-Sub): The Best PC I/O Interconnect In History? Learn ...
Whether utilized as an interim interconnect solution for the purpose of prototyping or selected for production, the d-subminiature connector offers Engineers and System Designers numerous advantages; the most notable being its native support for connections requiring anywhere from as little as nine (DB9) to as many as 78 (HD78) conductors.
Cell Connection Systems in e-Mobility - Amphenol CS
Cell connection systems (CCS) provide high-voltage connectivity and transmit signals such as temperature and pressure sensing information to the Battery Management System (BMS). The CCS also supports monitoring and controlling the charging and discharging processes, ensuring the safety of both the battery and the vehicle.
Technically Speaking | How Does a Moisture Meter Work? - Protimeter
How does a moisture meter work? Dive into its tech, how its functionality impacts moisture inspections, and interpreting the final results.
Introduction to Piezoelectric Pressure Sensors - PCB
Piezoelectric pressure sensors measure dynamic pressure. They are typically not suited for static pressure measurements. Dynamic pressure measurements including turbulence, blast, ballistics, and engine combustion require sensors with special capabilities.
Protimeter ReachMaster Pro | Moisture Meter on Telescoping Handle
The Protimeter ReachMaster Pro takes the hard work out of moisture inspections. The only moisture meter with a telescoping handle -- which extends up to 48” (122 cm) -- the ReachMaster Pro lets you inspect those hard-to-reach spaces without additional effort.