Search Results for how often do 31b get deployed
Market Connector: Directed Energy Weapons - Amphenol Aerospace
Where Are Directed Energy Weapons Being Deployed? While many Direct Energy Weapons systems are still under development or testing, several have reached operational status and are being used in military applications.
Israel Signs $540 Million Deal to Fast-Track Iron Beam Laser Defense ...
Israel has finalized a $540 million contract with Rafael Advanced Defense Systems and Elbit Systems to accelerate the deployment of the Iron Beam laser air defense system. With this investment, the Iron Beam is slated to come online sometime in 2025.
Graybar’s National Training Conference - Charles Industries, LLC
Fiber Terminal Enclosures – Indoor. Fiber Wall Solutions (CFWS) Fiber Terminals, Building (CFBT) Fiber Building Terminal – Multi-Compartment (CFBT-D3)
BA6110-1 - Amphenol Antenna Solutions
BA6110 “Heavy Duty” is permanently affixed to a unique mounting fixture which allows mounting on top of or along-side most vertical supports. Due to their wide bandwidth, they are ideal for use as emergency backup antennas. Their size and mounting fixtures allow for easy storage and fast installation.
TACBeam® | Fiber Optic Connector | Fiber Systems
The connector is available in both single mode and multimode versions, can be configured to support one to four fiber optic channels using a common insert and has been designed to accept a wide variety of cables to suit any application.
Amphenol TACBeam - Amphenol Fiber Systems International (AFSI)
Expanded beam technology expands and collimates the optical signal through the connector interface path, resulting in a diameter many times that of the original beam. The optical beam is then refocused into the core of the receiving fiber. The larger beam diameter improves insertion loss performance in the presence of dust and debris.
USB 3.1 Gen 1 - GSB31X & GSB32X Series - Amphenol CS
SuperSpeed USB will deliver 10x the data transfer rate of Hi-Speed USB, as well as improved power efficiency. With 5Gb/s signally rate, SuperSpeed USB 3.1 has a Sync-N-Go technology that minimizes user wait time. No device polling and lower active and idle power requirements are other significant features of these connectors.
Universal Broadband Enclosures CISH51 Radio Shrouds
See tables on pages 3-4 for equipment needed for a given installation. Operation Temp. Range, Inside Enclosure: -40o to +149oF (-40o to 65oC) Operation Temp. Range, Outside Enclosure: -40o to +115oF (-40o to 46oC) Humidity: 0 to 95% (Non-Condensing) Altitude: Up to 6,560 Feet (2000 Meters) All dimension in inches.
Amphenol Connector Basics Terminology Guide
Values are generally established for maximum and minimum forces. Contact Resistance - Maximum permitted electrical resistance of pin and socket contacts when assembled in a connector under typical service use.
M28876 Plating Transition - Amphenol Fiber Systems International (AFSI)
In 2021, the Navy released it’s new spec for M28876 connectors. The spec focused on the plating transition from the traditional CAD, or green plating, to the Black Hard Anodized (BHA), or black, plating. You may be wondering why the change? How will this affect you and impact your business?
New Boeing pylon to enable B-1B hypersonics testing
Boeing has developed an external pylon for its B-1B Lancer bomber that’s intended to enable the aircraft to be used for hypersonic missile testing. Boeing’s Load Adaptable Modular (LAM) pylon has a 7,500-pound weight capacity and would allow the B-1 to carry 50 percent more munitions.
High-Speed QSFP Loopback Adapter Modules De-Mystified (Pt. 1) -- The ...
To do this test correctly, you need to select the QSFP+ or QSFP28 Loopback Adapter Module whose internal specifications are designed to most closely mimic the real-world performance of the cable style and length you plan on deploying.
Understanding Cold Temp, Bend, & Impact Ratings for Industrial Cables
Three important factors are Cold Temperature Rating, Cold Bend Rating, and Cold Impact Rating. Each serves a unique purpose in safeguarding cables under low-temperature stress and ensuring peak performance, but it’s common for these terms to be misunderstood or used interchangeably.
Octonet Contact with Embedded 1G/10G Base-T Transformers
Amphenol’s Octonet Contact with Embedded 1G/10G Base-T Transformers integrates IEEE 802.3an/af/at/bt compliant transformers directly into the contact, enabling seamless compatibility with size 8 Quadrax-keyed MIL-DTL-38999 cavities.
More on Radiation Patterns - Beamwidth - PCTEL
There are a few parameters that can be used to do this. The first is “3-dB Beamwidth” or “Half-Power Beamwidth”. The 3-dB Beamwidth is the angle between the points on the pattern where the gain is down from the peak by 3-dB. You will often just hear “beamwidth” rather than 3-dB beamwidth.
Raytheon awarded $250 million for LEO tracking satellites
Raytheon Technologies has received a $250-million contract from the U.S. Space Development Agency (SDA) to develop seven missile warning and tracking satellites for the SDA’s planned low Earth orbit satellite network, which will be used to track advanced threats such as hypersonic missiles.
How MIL-DTL-38999 has Advanced Military Technology
The Aegis Combat System, which revolutionized naval warfare with its advanced radar and missile systems capable of tracking and engaging multiple targets simultaneously, was developed throughout the 1970s before it was first deployed on Ticonderoga-class cruisers in the early 1980s.
USMC begins testing Advanced Reconnaissance Vehicle prototypes
Among the focal points the Marine Corps will be testing include the prototypes’ command, control, communications, computer and unmanned aerial system (C4/UAS) capabilities — which are a major emphasis of the program — as well as how the prototypes navigate challenging terrain.
How small satellites are leading to big leaps in space
Launch providers have developed cost-effective solutions for deploying smallsats into orbit, allowing for more frequent and affordable access to space for small satellite developers. Satellite Swarms and Formation Flying: Smallsat constellations and formation flying missions have gained prominence.
General Dynamics and American Rheinmetall named finalists for ...
The U.S. Army has selected General Dynamics Land Systems (GDLS) and American Rheinmetall as the final two contenders for the Optionally Manned Fighting Vehicle (OMFV) program. The OMFV program is intended to replace the M2 Bradley Infantry Fighting Vehicle, which has been in service since 1981.