Search Results for how to move to thai land
Tooling Instructions - Positronic The Science of Certainty
Move contact to the hex crimp area so that the whole length of the ferrule will be crimped. (Use the upper die half with the hexagonal shape.) Squeeze handles together until ratchet releases. Pull crimped contact out of tool and inspect crimp as specified in Inspection Information for Removable Crimp Contacts.
High Voltage 38999 Connector | Products | Amphenol Aerospace
The High Voltage 38999 line of connectors is an expansion of the MIL-DTL-38999 series and is designed to provide high voltage solutions for next-generation aircraft power requirements. Future power distribution architecture is moving toward higher voltages than what standard connectors are designed to accommodate.
Ethernet Switch & Media Converter - Amphenol Socapex
The mechanical packaging is designed for MIL-STD-810 ground environmental compliance and high reliability.Each Ethernet MIL-STD switch is rugged and hardened to improve ingress, impact, and shock/vibration protection, as well as eliminate all moving parts through passive cooling.Our range of Ethernet military-grade switches feature numerous ...
High Voltage 38999 Connector | Power Products - Amphenol Aerospace
The High Voltage 38999 line of connectors is an expansion of the MIL-DTL-38999 series and is designed to provide high voltage solutions for next-generation aircraft power requirements. Future power distribution architecture is moving toward higher voltages than what standard connectors are designed to accommodate.
Solar Farm - Amphenol Aerospace
We've completed a multi-million-dollar solar farm at our former facility’s site which is the largest on-site corporate solar project in New York State to date and one of the largest on-site solar installations in the United States.
High Power Connectors | Products | Amphenol Aerospace
As we move beyond the current mil-spec standards to more custom, high-power needs, our connector designs and solutions have continued to evolve as the demand for more power increases. High Voltage and Current Requirements Are Not Going Away. In fact, they’re only going to continue growing.
The Rapid Growth of Electric Vehicles - Amphenol Aerospace
There are some obstacles surrounding commercial EV charging, but progress is moving steadily. On the other hand, making feasible charging systems for military EVs is a whole different beast. Developing adequate charging technology for military EVs – a class of electric vehicles that are projected to be much larger and require significantly ...
The Future of Ground Combat Vehicles is Electric
The technological road map will move to a fuel cell hybrid engine and, ultimately, an all-electric drivetrain. This is being done to save significant fuel and shipping costs and to gain an advantage in the field by getting rid of the noisy diesel engines – lessons learned by the U.S. and its allies. Additionally, these new drive systems will ...
Our history - Amphenol Socapex
Move from Suresne to Cluses in Haute Savoie. 1956 The first products for aviation. Since its creation, Socapex's core business is the design and manufacturing of electrical equipement for the aviation industry. 1957 Socapex is purchased by a large French group, Thomson 1958 Socapex starts manufacturing its first connectors : the TEI Series 58 ...
Military and Commercial Air Electrification: Part 1 — Harnessing Hybrid ...
Developers around the world are moving forward with implementing this technology. The U.S. military recognizes the advantages of a hybrid-electric system −such as greater range, enhanced acceleration and maneuverability, and a quieter acoustic signature−and is planning to augment the capabilities of many of its new vehicle platforms with ...
News - Amphenol Aerospace
Military, commercial, and industrial markets continue to move away from Cadmium due to known toxic carcinogens. The new AP-93 plating finish complies with all customer requirements tied to these specifications. Amphenol is also using European Union Directive 2002/95/EC RoHS as a guide to qualification for all military, commercial, and ...
High Voltage 38999 Connector | MIL-DTL-38999 Connectors | Products ...
The High Voltage 38999 line of connectors is an expansion of the MIL-DTL-38999 series and is designed to provide high voltage solutions for next-generation aircraft power requirements. Future power distribution architecture is moving toward higher voltages than what standard connectors are designed to accommodate.
Announcing our New Factory and Office Building in Frederick, Maryland ...
*Important: Please take note of our new address information below, and share it with your internal records departments, so that our move information and new building address can be accurately updated in your company's records.* New mailing/shipping and remit to address (effective October 15, 2018). Our phone and fax number will remain the same. Wilcoxon […]
Backshells, Strain Reliefs, Caps, Dummy Receptacles
Backshells, strain reliefs, caps, dummy receptacles and other D38999 connector accessories, including custom solutions for a wide variety of applications
CONNECTOR INSTALLATION INSTRUCTIONS Amphe-PV H4 Plus™ Connectors
3. the handshake moving mechanism is allowed to have lubricating oil, but cannot overflow.other part surface should be clean and without oil or oxidation. 2. specified general tolerance a. all the rounded corners radius 0.3mm min. b. burrs not to exceed 0.03mm for any surface. 1. the referenced material shall be certified compliant to the latest
High Voltage 38999 Connector | Circular Connectors | Products ...
The High Voltage 38999 line of connectors is an expansion of the MIL-DTL-38999 series and is designed to provide high voltage solutions for next-generation aircraft power requirements. Future power distribution architecture is moving toward higher voltages than what standard connectors are designed to accommodate.
Fiber Optic Media Converters - Amphenol Socapex
Amphenol Socapex proposes a large range of rugged military grade media converters with fiber. Our rugged military ethernet media converters with fiber are fully MIL-STD compliant.Fiber optic to LAN copper Ethernet converters are key equipments for fast, efficient, and secure deployment over long distance. The RES-GMC media converter with Expanded beam CTOS is particularly suitable for ...
Aerospace Connectors - Positronic The Science of Certainty
However, these connectors must also be lightweight; the higher the mass of the aircraft, the more energy is required to move it. Because lightweight materials like plastic and elastomers sometimes present outgassing issues over time, space-grade connectors must meet stringent outgas testing requirements. To qualify for aerospace deployment ...
Positronic Announces Facility Expansion
A s part of the expansion, all Missouri Positronic facilities will be transitioning into the Eldon location, which means the Campbell and Mt. Vernon facilities will close.While it is clear that the expansion of the Eldon location is a positive development for the company and its employees, the phase-down of the Mt. Vernon and Campbell locations is certainly bittersweet.
MF075 accelerometer magnetic mounting base - Wilcoxon Sensing Technologies
Features. Quickly move sensor from point to point; Raised knurling ensures comfortable grip and easy removal; 75 lbf pull strength; Nickel plated base to resist corrosion