Search Results for how to score devereux assessment
Transducer Tester and Test Block Kit - Airmar
Eliminate the guesswork and determine if a Transducer is in proper working condition quickly with AIRMAR’s TDT1000, the first Transducer diagnostic test device for use with most Transducers. Connect directly to AIRMAR’s database via the SensorCheck™ App and compare the Transducer onboard the vessel to its original, factory-approved test results.
amphenol-ns.com
We would like to show you a description here but the site won’t allow us.
Foulfree Transducer Coating - Airmar
Foulfree by AIRMAR 15ml Kit Airmar® Certified - Any marine growth or fouling on the face of a transducer can reduce sensitivity, decreasing bottom-echo returns and fish-target intensity. It can also increase the turbulence under the face of the transducer, causing aeration and therefore loss of bottom contact.
MachineryMate 200 operating guide - Wilcoxon Sensing Technologies
asy display of vibration signals. The MAC200 automatically performs vibration analysis functions based on machine running speed to help diagnose faults such as unba. umps, motors, fans and bearings). The meter displays vibration frequency plots and allows vibration severity and .
RET user guide - Amphenol Antenna Solutions
Amphenol Antenna Solutions offers its own RET control solution. The PCU-4 tool is delivered as a kit comprising of a computer software application together with a HW test interface with all the necessary cables and accessories.
Temposonics II
return pulse. A variety of interface devices use the data derived from these two pulses and generates an ana-log or digital output to repr. low waveguide. The waveguide is spring loaded within the transducer rod and exhibits the physical prop-erty of ma.
ACE-L™ - Amphenol Fiber Systems International (AFSI)
ACE-L™ - Amphenol Fiber Systems International (AFSI)
Protocol Manual MH-Series with CANopen Safety
CANopen protocol uses Emergency Objects to inform that the sensor has entered a state of error, or that a state of error has ended. Any Error state will also be visible in the SRDO through Status byte and the position data being set to zero.
SS175M Chirp-ready Tilted Element Thru-hull - Airmar
Operating at a frequency range of 85 to 135 kHz, this transducer reveals fish at medium depths of up to 457 m (1500') and delivers ultra-clear target resolution. Airmar’s Tilted Element ™ transducers have the element fixed at a 20°, 12°, or 0° angle within the housing.
5003700 - Amphenol Antenna Solutions
1-Port, Microcell Panel, VPOL, 55-80°, 698-4000 MHz, 5.0-7.5 dBi, SISO. Amphenol Antennas is your wireless communications network partner. Supporting your needs with innovative and tailored antenna solutions for optimal coverage and capacity.
Marine Antennas CXL 70-3C/... - AMPHENOL PROCOM
CXL 70-3C/… is a 3 dBd, vertically polarized, omnidirectional base station and marine antenna, which covers the 340 – 530 MHz band in 4 models with up to 10 MHz overlap. The antenna is provided with our “C” universal fixation bracket made of epoxy-coated, seawater resistant aluminium.
Installing the Sensor on the Trawl - marport.com
We recommend to install the sensor on the headrope in order to see the trawl opening and fish entering the trawl. Place sensor (1) at the centre of the net's headrope (2), facing the vessel. Install a double-mesh piece of netting (3) to stabilize the sensor.
How does Amphenol RF make certain that the VSWR of a connector will ...
Two steps are required during the design and development phase of connectors at Amphenol RF: 1. Simulation and Modeling: Once the 3-D mechanical drawings are completed, the first step in the RF design process is to model the connectors using High Frequency Structure Simulator (HFSS) software.
SS510 200 kHz Portable Survey - Airmar
Users with adjustable-frequency echosounders will be able to regulate the operating frequency and tailor the beamwidth to specific survey conditions. And the treaded stem allows portable mounting.
SMPM Male PCB Surface Mount Connector, 8-Port, FD
SV Microwave released the new SMPM Male PCB Surface Mount Connector, 8-Port, FD. This high-density connector can perform up to 40 GHz. Explore now.
Directed Field Acoustic Noise (DFAN) Testing | PCB Piezotronics
DFAN testing recreates the intense acoustic environment experienced during a rocket launch, ensuring that payloads and spacecraft components can endure the extreme noise and vibration.
STRAIN RELIEF CLAMP ACSELLS - amphenolpcd.com
Visit amphenolpcd.com ion STRAIN RELIEF CLAMP STRAIGHT; SELF-LOCK/SPIN MIL-DTL-26482 Series II; MIL-DTL-83723 Series III; AS50151; AS81703 M85049
B45 Traditional/CW Thru-hull - Airmar
The B45 is Airmar’s smallest and most economical, dual-frequency, bronze, stem transducer. It features a single, 50/200 kHz ceramic element. The included fairing streamlines the transducer and increases the performance—even at higher speeds. Find an Airmar Certified Installer/Dealer Near You!
Public Safety Network Testing Solution - PCTEL
With PCTEL’s automated network testing solution, you can ensure in-building communications coverage while saving time and money. Test multiple public safety, cellular, and private networks simultaneously using grid or path-based methods.
AT50 Airducer® Ultrasonic Transducer - Airmar
Non-contact level, flow and distance measurement is reliably delivered by the ultrasonic AT50. It includes rugged sealed construction, and PVDF housing is available for more chemically aggressive environments. The AT50 operates at 50 kHz and its sensing range is 30 cm to 15 m.