Search Results for interest rate of hecs
Amphenol Corporation Announces Pricing of Senior Notes Offering
The Additional 2027 Notes will have an interest rate of 5.050% per annum, the 2035 Notes will have an interest rate of 5.000% per annum, and the 2054 Notes will have an interest rate of 5.375% per annum.
Amphenol Corporation Announces Pricing of Senior Notes Offering
The 2027 Notes will have an interest rate of 5.050% per annum, the 2029 Notes will have an interest rate of 5.050% per annum, and the 2034 Notes will have an interest rate of 5.250% per annum.
HSIO-CA Brochure | Amphenol
Amphenol's QSFP-DD (Double Density) passive copper cable assemblies double the number of channels from 4 to 8 lanes when compared to the existing 100G QSFP cabling systems, enabling more bandwidth within the same mechanical envelope.
EMI Shielding - Amphenol Mobile Consumer Products
Typical materials used for electromagnetic shielding is sheet metal. The amount of reduction depends very much upon the material used, its thickness, the size and shape of the shielded volume, and the frequency of the fields of interest.
Amphenol Corporation Announces Pricing of $350,000,000 of Senior Notes
WALLINGFORD, Conn.-- (BUSINESS WIRE)-- Amphenol Corporation (NYSE: APH) announced today the pricing of its offering of $350,000,000 aggregate principal amount of senior notes due 2026 (the “Notes”). The Notes will have an interest rate of 4.750% per annum.
Future of High-Performance Computing and Interconnect Technologies ...
Anticipating the increased reliance of industries on HPC for data-intensive applications, this article brings to the spotlight an important report that outlines how these technologies are evolving to meet growing demands for speed, efficiency, and scalability.
D-Sub Interconnects - Still Going Strong! - Amphenol CS
Amphenol Cables on Demand offers one of the largest selections of in-stock D-Sub Cable Assemblies in the world, with numerous options to choose from to meet the demands of nearly any prospective installation scenario.
Leading the Evolution of High-Speed Interconnect -DesignCon 2025
DesignCon 2025 is a premier event focused on high-speed communications and system design. It is a must-attend event for chip, board, and systems design engineers to network, source, and stay ahead of industry change. At Booth 833, attendees can interact with our experts and explore these demos:
Model HT623C01 | PCB Piezotronics
High temperature, high frequency, industrial, ceramic shear ICP® accel, 100 mV/g, 0.8 to 15k Hz, top exit, 2-pin conn., frequency sweep ISO 17025 accredited calibration. [1] Conversion Factor 1g = 9.81 m/s². [2] 1Hz = 60 cpm (cycles per minute). [3] Zero-based, least-squares, straight line method.
Amphenol Corporation Announces Pricing of $750,000,000 of Senior Notes
WALLINGFORD, Conn.-- (BUSINESS WIRE)-- Amphenol Corporation (NYSE: APH) (the “Company”) announced the pricing of its offering of $750,000,000 aggregate principal amount of senior notes due 2031 (the “Notes”). The Notes will have an interest rate of 2.200% per annum.
High Frequency Industrial Accelerometers - PCB
Accurate measurement hinges on the sensor’s dynamic range and high frequency response. By lowering the sensitivity to 10 mV/g one is able to achieve 500 g acceleration measurement range. Accelerometers for monitoring high-speed rotating equipment.
Amphenol Corporation Announces Pricing of €500 Million Senior Notes
The Notes will have an interest rate of 0.750% per annum. The closing of the offering is expected to occur on May 4, 2020, subject to the satisfaction of customary closing conditions.
Learn to Succeed With Fibre Channel - Amphenol CS
Fibre Channel has come a long way since it was first approved as an ANSI standard in 1994 to become the trusted and reliable networking solution it is today that delivers the efficiency and speed necessary for storage to be networked and shared across multiple hosts.
High Pass Filter Applications and Best Practices to Excel in Military ...
High pass filters transmit frequencies for high-speed communication and radar systems while blocking low-frequency interference below the threshold, such as ground-based electromagnetic interference or power grid harmonics. High pass filters handle high-frequency signals in satellite uplink and downlink channels.
Amphenol Announces Pricing of $750 Million of Senior Notes
The 2020 Notes will have an interest rate of 2.200% and the 2024 Notes will have an interest rate of 3.200% per annum. The 2020 Notes are being issued at a price equal to 99.922% of their face value and the 2024 Notes are being issued at a price equal to 99.888% of their face value.
PCIe® Gen 7.0 Doubles Data Rate to 128 GT/s For Data-Intensive Markets
PCIe ® Gen 7 will deliver a raw bit rate of 128 GT/s, enabling bi-directional data transfer rates of up to 512 Gb/s when configured as x16. Compared to the PCIe ® 6, which had only 64 GT/s raw data rate and up to 256 Gb/s via x16 configuration.
Amphenol Corporation - Amphenol Reports Third Quarter 2023 Results and ...
Assuming market conditions do not meaningfully worsen as well as constant exchange rates, for the fourth quarter of 2023, Amphenol expects sales to be in the range of $3.090 billion to $3.150 billion. This represents a 3% to 5% decline over the prior year quarter.
Amphenol Corporation Announces Pricing of $400,000,000 of Senior Notes
Amphenol Corporation (NYSE: APH) (the “Company”) announced today the pricing of its offering of $400,000,000 aggregate principal amount of senior notes due 2025 (the “Notes”). The Notes will have an interest rate of 2.050% per annum.
A Deep Dive into High-Speed Computing Server Interconnect Solutions
Amphenol comes up with the EXAMAX2 ® backplane connector system supporting 112Gb/s PAM4 industry specifications. This ultra-fast interconnect technology enhances data transfer rates and reduces communication latency, enabling high-performance systems to process AI workloads more efficiently.
Amphenol Reports Record Third Quarter 2022 Results and Announces ...
For the full year 2022, we expect sales to be in the range of $12.474 billion to $12.534 billion. This represents 15% growth over 2021 and includes a 3 percentage point negative currency impact. Adjusted Diluted EPS is expected to be in the range of $2.95 to $2.97, representing 19% to 20% growth over 2021.