Search Results for introduce a to b
Add More Flexibility With New 50 Ohm SMB Cable Assembly Options
Amphenol RF is proud to introduce additional SMB cable assemblies into our wide portfolio of pre-configured RF assemblies. These 50 ohm cable assemblies feature a plug to plug configuration and are available in both RG-58 and RG-174 versions. They offer reliable electrical performance up to 4 GHz, or the limits of the cable type, and are ideal ...
INSTRUCTION MANUAL INS9800 Rev B SEP 2024 - protimeter.com
b) Press and hold / long press to turn OFF the device. c) Press to select from the menu. 2. UP / Increment : a) Navigate up through menu. b) Increment the number in configuration. 3. DOWN / Decrement : a) Navigate down through menu. b) Decrement the number in configuration. 4. Ref/ Right/ Record/ Hold : a. Press to hold and release reading while
INSTRUCTION MANUAL INS9800 Rev A OCT 2021 - Protimeter
b) Press and hold / long press to turn OFF the device. c) Press to select from the menu. 2. UP / Increment : a) Navigate up through menu. b) Increment the number in configuration. 3. DOWN / Decrement : a) Navigate down through menu. b) Decrement the number in configuration. 4. Ref/ Right/ Record/ Hold : a. Press to hold and release reading while
Temposonics II
1 INTRODUCTION 1 1.1 Theory of Operation/Magnetostriction 1 1.2 Temposonics II LDT Specifications 2 1.3 Specifications for Temposonics II LDTs over 180 inches 3 2 TEMPOSONICS II LDT INSTALLATION 4 2.1 Types of Transducer Supports 6 2.1.1 Loop Supports 6 2.1.2 Channel Supports 7 2.1.3 Guide Pipe Supports 7 2.2 Open Magnets 8
Amphenol TPC Wire & Cable Launches product Configurator
“We are excited to introduce this powerful tool to our customers,” said Tom Senkevich, Director of Marketing at Amphenol TPC Wire & Cable. “Our new product configurator is designed to simplify the selection process, allowing our customers to quickly and easily find the products they need and configure custom solutions that meet their ...
Trident UserManual en V2 - Marport
Introduction and Presentation. 6. Introduction. 7 Applications. 8 Safety Guidelines. 9 Description. 10. System Compatibility. 10 Technical Specifications. 10 Main Parts. 12. Sensor Configuration. 14. Connecting the Sensor to Mosa2. 15 Battery Information. 18 Configuring the Trawl Node. 19 Configuring the Uplink Frequency and . Power 21 Sounding ...
IBAS.01 BAS002 Manual Rev B - PCB
IBAS.01 Rev B Larson Davis Building Acoustic Source Model BAS002 Power Amplifier & Speakers Manual. ... BAS002 Introduction 1-1 CHAPTER 1 Introduction This chapter describes the features, functions, and proper care of the Larson Davis Building Acoustic Source models BAS001, BAS002, and BAS003.
TN-21 Introduction to Air Blast Measurements - Part IV
pcb.com 1 800 828 8840 Introduction to Air Blast Measurements - Part IV Getting the Signal Down the Cable TN-21 Written By Patrick L. Walter, Ph. D.
II - Temposonics
1 INTRODUCTION 1 1.1 Theory of Operation/Magnetostriction 1 1.2 Temposonics II LDT Specifications for Sensors <180 Inches 2 1.3 Temposonics II LDT Specifications for Sensors ‡ 180 inches 2 2 TEMPOSONICS II LDT INSTALLATION 3 2.1 Types of Transducer Supports 5 2.1.1 Loop Supports 5 2.1.2 Channel Supports 6 2.1.3 Guide Pipe Supports 6 2.2 Open ...
Introducing PCB Model 354A14 Case Isolated Cryogenic ICP® Triaxial ...
January 22, 2025 - Depew, NY - PCB Piezotronics (PCB®) is proud to announce the launch of our new Model 354A14 case isolated cryogenic ICP® triaxial accelerometer. This model is a relatively small size, with three individually isolated sensing elements. It has exceptional frequency response from 2.5 to 10k Hz throughout the broad operating temperature range all the way down to -320°F (-196°C).
Operation Manual Level Plus - Temposonics
Level Plus ® Tank SLAER ® Operation Manual I 3 I 1. Contact information United States General Tel: +1-919-677-0100 Fax: +1-919-677-2343 E-mail: info.us@temposonics.com
Operation Manual Level Plus - temposonics.com
Level Plus ® 5H QH0(® Operation Manual I 5 I Strap Table A table of measurement correlating the height of a vessel to the volume that is contained at that height. The transmitter can contain up to 200 points. T TEC ‘Thermal Expansion Coefficient’ - a value correlating the change in
EU-TYPE EXAMINATION CERTIFICATE - Amphenol Fiber Systems International ...
The introduction of a new cement material, Hysol ES1002, replacing the previously approved cement, Hysol ES4412; the description was amended to reflect this change. Variation 3 - This variation introduced the following change: i. The Ex-133, Ex-153 and Ex-173 products in the range were allowed to be used in a +55°C ambient
731A seismic accelerometer and P31 power unit/amplifier Operating guide
Amphenol (Maryland) Inc. d/b/a Wilcoxon Sensing Technologies 90225 Rev.E.1 10/18 Tel: +1 (301) 330-8811 Tel: +1 800 WILCOXON Fax: +1 (301) 330-8873 www.wilcoxon.com ... 1.0 Introduction The 731A seismic accelerometer and P31 Power Unit Amplifier are a unique state-of-the-art system for the measurement of
Contents
b. To fix with the adhesive tape: thoroughly clean and degrease the target surface with cleaning solvent, then dry it. Provide pressure for at least 30 . sec. on the whole surface of the support using a hard edged plastic tool of the same size as the support. Wait for at least 6 hours before hanging the charger plug. Note:
75 OHMS Coaxial Contacts - Amphenol Socapex
Amphenol Socapex introduce size 6 coaxial contacts dedicated for 75 Ohms applications. Those coax contacts are the perfect choice when the cable size can’t fit in a standard contact size. ... RG179-B/U 612127 612126 EMTEQ TFLX 125-075-01 PIC V73263 612242 612244 PIC V76261 For PC Tail version, please consult us. ...
micro-bayonet-connector-catalog-amphenol-industrial
B Socket, less contacts C Pin Crimp (machined crimp barrel D Socket Crimp (machined crimp barrel) F Socket PC Tail-Length .150 N Non Environmental 6. KEYING N 150° 210° A 150° 240° B 240° 150°C D 240° 7. OPTIONAL CODE B Shield Termination Micro Band Included-©2015 Amphenol Corporation REV:1/12/2016 Bayonet B antam Bayonet B antam
Monitoring reciprocating gas compressors with 4-20 mA LPSTM vibration ...
LPSTM velocity transducers monitor vibration caused by B imbalance energy to detect this highly damaging A machinery fault. ISO10816 recommends that peak vibration levels exceeding 0.63 inches-per-second Vibration velocity in/sec peak (mm/sec r.m.s.) Class I Class II Class III Class IV 2.5 (45) D D D 1.6 (28) D 1.0 (18) 0.63 (11.2) C 0.4 (7.1 ...
AX Series XLR Cable Connectors - Amphenol Sine
introduce an exciting contemporary look and feel to the professional audio interconnect market. They are designed to complement modern audio architecture and truly “fit” within their environment. An impressive list of features guarantees pure sound performance in the most demanding applications providing unrivalled value. Features
SCU User Guide Version 3 - Amphenol Antenna Solutions
1. Introduction The Site Control Unit (SCU) is a site controller for AISG devices installed at a cell site. It is compatible with the AISG (Antenna Interface Standards Group) standard and can control up to (24) AISGv1.1 and/or AISGv2.0 devices, such as RET (Remote electrical tilt) and TMA (Tower-mounted amplifier), at a site.