Search Results for is postfix mail good
2015-07-06 the Tug of War_Amphenol Assembletech
In order to enjoy ourselves , on June 6th, 2015, the Tug of War was held successfully in our active participation,which was an interesting competition .All of the players and cheerleaders had the good team work, and all had an unforgettable night.
Model 200B03 Impact ICP® quartz force sensor, 500 lb comp., 10 ... - PCB
calibration cycle, a good “rule of thumb” is to recalibrate on an annual basis. It is also good practice to recalibrate after exposure to any severe temperature extreme, shock, load, or other environmental influence, or prior to any critical test. PCB Piezotronics maintains an ISO- 9001 certified metrology laboratory and
Wire, Cable, & Cable Assemblies for harsh industrial use | Amphenol TPC
Wire and cable solutions for demanding applications and harsh environments. More durable products prevent electrical failure and reduce maintenance costs.
PCB PIEZOTRONICS | CONTACT US
Midwest Branch | 24350 Indoplex Circle, Farmington Hills, MI 48335 Scott Shaffer (888) 860-4595. sshaffer@pcb.com
Model M109C12 High pressure ICP® ballistic pressure sensor, 100k ... - PCB
Use good machining practice in preparation of the mounting port, paying particular attention to the seal surface. It is important that this surface be perfectly smooth and free from tool chatter marks, nicks and other imperfections which might cause leaks at high pressures. 3.3 RECESSED MOUNT The recessed installation is shown in the Recessed
Model 3741B1250G/46487-02 DC Response Accelerometer Installation ... - PCB
calibration cycle, a good “rule of thumb” is to recalibrate on an annual basis. It is also good practice to recalibrate after exposure to any severe temperature extreme, shock, load, or other environmental influence, or prior to any critical test. PCB Piezotronics maintains an ISO- 9001 certified metrology laboratory and
EXCEL|MATE CC BSM, HEV, AUTOLOK & LVRC EXCEL|MATE ECO EXCEL|MATE MSD GB ...
stall, it offers a good price-quality ratio. Multiple coding positions are available. Cable size: 25 to 70mm2 shielded wires 4 EXCEL|MATE PT EXCEL|MATE MSD Battery Pack Charger Motor PDU MCU DC/DC PTC AC HVPTB/M/2A 5 Light in weight with plastic shell / Easy to install / Reliable connection / IP68 (mat-ed), IP6K9K / Multiple coding positions
Model 903B02 Pressure Pulse Calibrator Installation and Operating ... - PCB
calibration cycle, a good “rule of thumb” is to recalibrate on an annual basis. It is also good practice to recalibrate after exposure to any severe temperature extreme, shock, load, or other environmental influence, or prior to any critical test. PCB Piezotronics maintains an ISO- 9001 certified metrology laboratory and
Model 102A04 **OBSOLETE** See 102B04 High frequency ICP ... - PCB
doubt about a calibration cycle, a good “rule of thumb” is to recalibrate on an annual basis. It is also good practice to recalibrate after exposure to any severe temperature extreme, shock, load, or other environmental influence, or prior to any critical test. PCB Piezotronics maintains an ISO-9001 certified metrology laboratory and
Model 137B27 Quartz, free-field, ICP® blast pressure pencil ... - PCB
week. Call or email with model and serial number as well as a brief description of the problem. Calibration Routine calibration of sensors and associated instrumentation is necessary to maintain measurement accuracy. We recommend calibrating on an annual basis, after exposure to any extreme environmental influence,
Model 3713E1110G Triaxial MEMS DC accelerometer, 200 mV/g, +/- 10 ... - PCB
Call or email with model and serial number as well as a brief description of the problem. Calibration Routine calibration of sensors and associated ... machinist with good machining capabilities adequately prepare the surface. Adhesive Mount: Recommended for temporary mounting of the .
Model 105C02 Subminiature ICP® pressure sensor, 100 psi, 50 mV ... - PCB
iron with only enough heat to obtain good solder joint. The electrical ground return is made to the sensor body. This connection can be made by attaching electrically to the structure or by using the metal ribbon spotwelded to the sensor body. 3.2 MODELS 105C02, C12 & C22
Validator® AVS Software 2.0 - kayeinstruments.com
Validator® AVS Software 2.0 - kayeinstruments.com
Model 105C Subminiature ICP® pressure sensor, 100 psi, 50 mV/psi ... - PCB
iron with only enough heat to obtain good solder joint. The electrical ground return is made to the sensor body. This connection can be made by attaching electrically to the structure or by using the metal ribbon spotwelded to the sensor body. 3.2 MODELS 105C02, C12 & C22
Model W113B32/003C05 High frequency Invar ICP® pressure probe ... - PCB
extreme environments it is good practice to protect cable connections with shrink tubing. It is not necessary to use low-noise cable with this sensor series. In fact, an optional Model 070B09 Solder Connector Adaptor allows the use of ordinary two-wire cable if desired. 4.0 OPERATION. It is only necessary to supply the sensor with a 2 to 20
SS505 50/200kHz, 600W, MM Transducer, DT
The SS505 is a compact, impact resistant, stainless steel stem for use on all hulls. The dual-frequency version provides good target detail in shallow-water at 200 kHz and good deep-water bottom tracking at 50 kHz. The narrow-beam 200 kHz version provides excellent bottom detail.
Model 603C01 Platinum Low-cost Industrial ICP® Accelerometer ... - PCB
doubt about a calibration cycle, a good “rule of thumb” is to recalibrate on an annual basis. It is also good practice to recalibrate after exposure to any severe temperature extreme, shock, load, or other environmental influence, or prior to any critical test. PCB Piezotronics maintains an ISO-9001 certified metrology laboratory and
Certifications - Amphenol Fiber Systems International (AFSI)
Certifications - Amphenol Fiber Systems International (AFSI)
Model 3713F1250G Triaxial MEMS DC accelerometer, 27 mV/g, 50 g ... - PCB
E-mail: info@pcb.com Web: www.pcb.com. Manual 21354 Rev E ECN 50523 Repair and Maintenance ... machinist with good machining capabilities adequately prepare the surface. Adhesive Mount: Recommended for temporary mounting of the . sensor or when the test object surface cannot be properly pre-
8551-80 Power Supply (48Vdc, 2.5A) - charlesindustries.com
output voltage to return to normal, replace the power supply with a similar unit known to be in good op-erating condition and retest. 7. TECHNICAL ASSISTANCE If technical assistance is required, contact Charles Industries’ Technical Services Center at: 847-806-8500 847-806-8556 (FAX) 800-607-8500 techserv@charlesindustries.com (e-mail) 8.