Search Results for mass helalth connector
PVDF - MSI Transducers
543 Great Rd. Littleton MA. Solutions. Custom Defense and Commercial Transducers Low Cost Transducers and Arrays ACOMMs Projectors High Temperature-Pressure Applications Synthetic Aperture Sonar Transducers Full Ocean Depth. Material Technologies. Piezocomposite Solid Ceramic PVDF Advanced Material Development. Markets. Commercial
EU RoHS II Certificate of Conformance - amphenol-aerospace.com
D38999/24ZD35PN YES CONNECTOR, ELECTRICAL, RECEPTACLE 6(c) Per review of the materials & processes utilized in the manufacture of the above -listed part number , Amphenol Aerospace Operations and Commercial Air Division hereby acknowledges the referenced product is in conformity with the following: Directive 2011/65/EU (as amended)
Thermometrics Type MA100 NTC Thermistors - amphenol-sensors.com
Thermometrics Type MA100 NTC Thermistors - amphenol-sensors.com
Model 3503A1160KG/-0003 TRIAXIAL HIGH AMPLITUDE MEMS SHOCK ... - PCB
mass. Because many such applications are coupled with battery powered conditioning and data acquisition, PCB MEMS sensors were designed with relatively high value resistors (approximately 10 times that of other devices) to maximize battery life. 4.0 Common Applications The 3500/3600 Series PR Shock Accelerometers achieve true ...
Model M601A02 Low-cost Industrial ICP® Accelerometer Installation and ...
conditioners should use higher capacity (up to 20 mA) constant current circuits in place of the diodes, particularly when driving long signal cables (see Section 5). Decoupling of the data signal occurs at the output stage of the signal conditioner. A 10 to 30 µF capacitor coupled with a resistor shifts the signal level to essentially ...
EB4885 Series - 5.00mm Spacing - EBY Electro
See our LED Connector Overview Connectors for LED Lighting. EB3400 — Lowest profile in the industry! EB3400 Blanks; EB5400 — Takes up to 14AWG; EB3100 — Low profile connectors; EB430 3.5mm centerline block; EB401 5.0mm centerline block; Board-to-Board Jumpers. LED Connection Jumpers — for EB3400; Connector Tools. See our LED-SMD ...
LiteTouch Solderless PCB Connectors Video | SV Microwave
SV Microwave is a world leader in the RF/Microwave industry. We design and manufacture RF/Microwave coaxial connectors, cable assemblies, passive components and tools.
Länder - kayeinstruments.com
About us. Kaye & Amphenol; Kaye History; Çevre ve İSG; Kalite; Hüküm ve Şartlar; News
Temp - ssi-sensors.com
SSI Technologies, LLC. Prodej a marketing Inside Sales. 3200 Palmer Drive. Janesville, WI 53546. 608-373-9262. lim@ssitech.com
LÜTZE takes over US cable manufacturer DGC - Lutze Inc.
The family company DGC Inc. based on Gardner, Massachusetts, was founded in 1983, and operates in the industrial automation market. Don Irving, founder and former company owner, will remain CEO, while managing director of LÜTZE US, Jürgen Seybold, will take over the management of DGC.
TRIM-214-C02 - Combination preparation tool, crank version, for ...
Special trimming tool makes the connector attachment easier. No further tools are required to prepare the cable for the connector attachment. This is due to the unique design of the trimming tool, which combines all necessary functions in one tool. It can be used for CELLFLEX LCF 114-50, LCF 158-50 and LCF 214-50 foam dielectric cables. ®
Shipbuilding and Marine - Milrail
Founded in 1990, Milrail is a specialty division of Amphenol TPC Wire & Cable, a leading supplier for the Railway, Mass Transit, Marine, and Industrial industries. As an ISO-9001 and Controlled Goods Certified registered supplier, we can meet industry demands with the support of our trusted manufacturers and qualified sales team.
Product Finder - Lutze Inc.
LUTZE Inc. 13330 South Ridge Drive • Charlotte, North Carolina 28273 • USA Phone: 704-504-0222 • Fax: 704-504-0223 • E-Mail: info (at) lutze.com
SS175 Medium Ultra-Wide Chirp, 1kW, 0° Tilt, Garmin 12-Pin, DT - Gemeco
Features. Depth and fast-response water-temperature sensor; 1 kW with depth tracking down to 400 m (1,300#39;) Medium frequency: 60-100 kHz. 57° to 73° beamwidth (port/starboard)
Whip & Aerial LMR, TETRA, & P25 Antennas - PCTEL
PCTEL offers secure, high-performance, durable, & flexible LMR, TETRA, & P25 antennas for mission critical communications. Learn more.
Plug monomodule With standard protection cap Polarization E
Military & Commercial Aerospace specification for rectangular modular connectors; Fully qualified and compliant with ARINC 809 specifications; Tested and qualified per EN4165 Seri
Module With angled PCB contacts (SIM 2 and 4 modules) Pin Without ...
Module With angled PCD contacts (SIM 2 and 4 modules) Pin Without peripheral sealing Contacts #20 Tin-plated without Lead (RoHS) Polarization N
Statement: Corona and delivery capability | Amphenol Precision Optics
Talk to us about your requirements. Amphenol Precision Optics GmbH Head office Phone: +49 (0)2772 57559-0
SMPS Female Termination (1/2 Watt) 8038-4007 - SV Microwave
SV Microwave has released the SMPS Female Termination (1/2 Watt) 8038-4007. Explore the product's superior features and specifications here!