Search Results for matlab get bearing and distance
Measuring displacement using accelerometers - Wilcoxon Sensing Technologies
Eddy current probes are precisely thru-hole mounted into a mechanical casing and measure two very important shaft parameters. First, eddy current probes indicate the location of the shaft relative to the casing.
Configuring Trawl Settings - marport.com
From the tab Trawl, complete Headline (H), Bridle (B) and Sweepline (S) with accurate measurements of your trawl gear. Note:If you receive neither warp lengths nor slant distances, you can select Estimate horizontal distance from depths in Trawl Modeling > Doors Positioning System.
Testing Relative Bearing Measurements - marport.com
You can test if the relative bearing measurements are correctly calculated by the door sensors.
Meggitt - Wilcoxon Sensing Technologies
There are four bearing positions, two on the pump and two on the motor. The inboard pump bearing serves the function of taking up axial thrust as well as radial force.
Downloads - Temposonics
Get all documents and software for your sensor by filling out the dropdowns below. (You need to know the series, model and output of your sensor).
Pocket Angle of Attack - marport.com
You can test if the relative bearing measurements are correctly calculated by the door sensors.
Model 625B21 Precision Industrial ICP® Accelerometer ... - PCB
The maximum measurement frequency of interest is determined by the maximum number of harmonics of an event like running speed, bearing frequencies, or gear mesh.
Model X649A03 Bearing Fault Detector PLUS Installation and ... - PCB
Figure 2 – Bearing Condition Guide for Compensated Peak Acceleration, Crest Factor and Crest Factor Plus Installation thod, consider closely the advantages and disadvantages of each technique. Typical mounting types a
Data Sheet R-Series V RF5 PROFINET (document part number: 552211)
In addition to the measured position value via the PROFINET protocol further data about the current sensor status, such as the total distance travelled, the internal temperature and the total operating hours, can be displayed for diagnostic purposes.
Accelerometer Selection Considerations - Wilcoxon Sensing Technologies
Some examples for estimating maximum frequency to be measured. This is rarely a consideration for industrial applications except for very low frequency measurements. The minimum amplitude vibration should generate a signal at least 5 times the amplifier noise present at that frequency.
Data Sheet R-Series V RM5 PROFINET (Doc Part No. 552118)
In addition to the measured position value via the PROFINET protocol further data about the current sensor status, such as the total distance travelled, the internal temperature and the total operating hours, can be displayed for diagnostic purposes.
THREADED FASTENER DESIGN AND ANALYSIS - PCB
The clamp load at the bolt yield torque is primarily a function of the material properties of the bolt, and the thread friction coefficient, μG. Underhead embedment resulting from compressive yield in the bearing area depends upon the strength of the bolt or nut relative to the clamped surface strength.
PCB Piezotronics | Measure vibration, pressure, force, and more
PCB Piezotronics — Sensors to measure vibration, acoustics, force, pressure, load, strain, shock, and torque.
IMI Sensors Displacement Sensor for Ultra Low Frequency Applications - PCB
When it comes to vibration monitoring in displacement of slow-speed machines, IMI Sensors’ Model 653A01 displacement sensor with an embeddable accelerometer is an ideal solution. (See Figure 2.) The sensor has a measurement range of 2 to 40 mil peak-to-peak and a frequency range of 1.5 to 300 Hz.
SAS | MSI Transducers
SAS arrays can be built to be modular, allowing independent models to be combined to cover multiple areas by using 1, 2, 3, etc modules, while holding critical tolerances required in SAS systems. MSI has designed and manufactured SAS systems that are operating at 6000 meter depths.
Sensors With Integral Softline Cable - PCB
SENSORS WITH INTEGRAL SOFTLINE CABLE Article by: Meredith Christman, Product Marketing Manager, IMI division of PCB Piezotronics, Depew, New York
Sensors and Shakers for Ground Test | PCB Piezotronics
Through The Modal Shop, we provide shakers for structural excitation during testing and complete GVT system rentals. To discuss specific applications, please contact us or request a quote. You can also visit our online shop to find in stock sensors.
Microsoft Word - TN-14_BFD_682A05_White_Paper.doc - PCB
IMI Sensors’1 (A Division of PCB Piezotronics, Inc.) Model 682A05 Bearing Fault Detector module is a DIN rail signal conditioner that interfaces to an ICP® accelerometer. The device converts the accelerometer signal into two industry standard 4 to 20 mA output signals.
http://specadmin.pcb.com/PCB_spec_sheet.asp?item_id=17162&model
http://specadmin.pcb.com/PCB_spec_sheet.asp?item_id=17162&model