Search Results for matlab save object
ComboStak® and PowerStak® Board-to-Board Connectors - Amphenol CS
save space and cost § Power distribution and signal control in one connector § Signal pin continues to match BergStak ® 0.80mm § Support stack height from 5mm to 20mm, power position from 2 to 10pos and signal position from 6 to 140pos § Supports a wide range of applications § Scoop proof housing with ±0.9mm misalignment tolerance §
Check Out the Latest Server Connectors at DesignCon 2020 - Amphenol CS
DesignCon being the largest chip, board, and systems event in the industry witnesses the launch of many innovative products. Amphenol ICC will be is launching three high-speed server connectors at DesignCon 2020: Right Angle PCIe ® Gen 4 CEM connectors, Gen Z 4C-HP Mini Cool Edge connectors and Double Density Cool Edge connectors.. PCIe ® Gen 4 CEM Connectors (RA)
.093 Piezoelectric accelerometer - pcb.com
for high temperature vibration measurement on mini-structures and small objects. The unit is hermetically sealed and ideal for use in extreme environments. Its light weight (3.1 gm) effectively eliminates mass loading. The accelerometer is a self-generating device that Model 2220E features Endevco’s Piezite® shear mode.
Charles Universal Broadband Enclosure CUBE-PM64412xxx General ...
LT-PM64412XXX Page 2 of 10 10 th Printing 2. PRODUCT DESCRIPTION The CUBE includes an equipment compartment with 44RU of 23” horizontal rack spacing and front and rear doors.
TN-12-0904 Air Blast Part 1 - PCB
action of blast waves with a solid object can result in reflec-tions from the object or cause the waves to reflect from, as well as diffract around the object. Figure 3 shows the reflection of strong shock waves from a reflective surface. I1, I2, and I3 represent the expanding shock wave, while the "R" contours represent the respective
Amphenol Network Solutions > INSULATOR STANDOFF KIT S 1/4-20 x 12-24
This photo is used for example purposes only and may not represent the final parts received - Contact Inside Sales to determine the final Bill-of-Materials
Temposonics
The magnet, connected to the object in motion in the application, generates a magnetic field at its location on the waveguide. A short current pulse is applied to the waveguide. This creates a momentary radial magnetic field and torsional strain on the waveguide. The momentary interaction of the magnetic fields releases
MachineryMate 200 operating guide - Wilcoxon Sensing Technologies
2.3.2 Load and Save readings Press the SQUARE button to select Load & Save. Save Reading opens a screen which allows the user to choose from one of three Memories in which to save the reading. Selecting Load Reading lets the user load a previously saved reading for further review. Demo Data loads two pre-stored demonstration vibraion data.
Data Sheet R-Series V RP5 SSI - Temposonics
electronics. The magnet, connected to the object in motion in the application, generates a magnetic field at its location on the waveguide. A short current pulse is applied to the waveguide. This creates a momentary radial magnetic field and torsional strain on the waveguide. The momentary interaction of the magnetic fields releases a torsional
Issue 1 Print 5 LT93‐INCHGR‐1 InCharger INSTALLATION INSTRUCTION ...
SAVE THESE INSTRUCTIONS. This manual contains important safety and operating instructions for the InCharger . Read the entire manual before usage. This device is not ignition protected. Avoid serious injury or death from fire or explosion. Do not install in compartment containing gasoline fueled engines or gasoline tanks, or in areas where ignition
Data Sheet T-Series – TH SSI - Temposonics
®Temposonics TH SSI Data Sheet I 3 I TECHNICAL DATA See next page for “Electrical connection” 1/ With standard one shot of 16 μs 2/ With position magnet # 201 542-2 3/ If there is contact between the moving magnet including the magnet holder and the sensor rod, make sure that the maximum speed of the moving magnet is ≤ 1 m/s (Safety requirement due to ESD [Electro Static Discharge])
IBAS.01 BAS002 Manual Rev B - PCB
BAS002 Basic Operations 1-2 Features The Larson Davis Model Building Acoustic Source has the following features: • High power and level output • Fast and easy-to-use
Improved Stiffness Specifications for Piezoelectric Force Links - PCB
4 WPL_88_1121 . Force Limited Vibration Testing: NASA-HDBK-7004C [1] speaks to the importance of using piezoelectric 3-component force sensors paired with shaker controllers that offer real-time response limiting.
Amphenol Network Solutions > Products > Fiber > Advanced Optical ...
The Amphenol Network Solutions MPO AOMs (Advanced Optical Modules) can increase fiber density and decrease your footprint. With single-mode (G.657.A BIF) or multimode (OM3 or OM4) versions available, these modules enable network planners migrate to 40/100/400/800G. The modules have a 12-fiber MPO input on the rear, terminated internally and routed to the LC duplex on the front.
Model 357B69/NC Charge Output Accel., High Temp, 3 pC/g, to 6k Hz, 10 ...
Model 357B69/NC Charge Output Accel., High Temp, 3 pC/g, to 6k Hz, 10-32 side conn, 10-32 mount, to +900 F, no cable Installation and Operating Manual
Operation Manual T-Series SSI - Temposonics
3 Temposonics® TH SSI ATEX / UK Ex / IECEx / CEC / NEC / CCC / PESO certified / Japanese approval Operation Manual 1/ The term “qualified technical personnel” characterizes persons who: • are familiar with the safety concepts of automation technology applicable to the particular project • are competent in the field of electromagnetic compatibility (EMC)
PRESSURE FUNDAMENTALS - PCB
equipped. The sensing section includes a stack of disc-shaped sensing elements preloaded in compression between upper and lower masses that are retained by an outer preload sleeve.
31758001301MOR - Amphenol Air LB
1750 series consists of Quick junction modules for signal and low current distribution, where sealing (IP66 / IP68 and IP69K), space and weight-saving are prime requirements.
Understanding the Key Trade-Offs in RF Filters - Q Microwave
In commercial applications, engineers may be able to make a trade-off in terms of power and save on costs. As illustrated, there are many considerations that go into deciding the design of a custom RF filter. Typically it’s a process of experimentation. We trade off one priority against the other until a compromise can be reached that will ...
Repair and Maintenance Returning Equipment Contact Information Safety ...
Manual 21354 Rev E ECN 50523 CAUTION Refers to hazards that could damage the instrument. NOTE Indicates tips, recommendations and important information.