Search Results for maximum vector
AR-86 Transverse Sensitivity - PCB
The vector of maximum sensitivity S in this example is tilted by angle f from the ideal vertical (z axis) direction, and decomposes to three orthogonal parts Sx, Sy and Sz. The z axis component Sz is the value normally reported as the accelerometer sensitivity.
Defense - Industries - Wilcoxon Sensing Technologies
Wilcoxon Sensing Technologies advanced sensing technology products include: Vector sensors measure the acoustic pressure and particle acceleration in three orthogonal axes.
MICROPHONE HANDBOOK - PCB
Particle velocity is a vector quantity where the direction of the vector is parallel to the motion of the transmitted wave. The SI unit for particle velocity is meters per second (m/s). Particle velocity should not be confused with either the velocity of individual molecules or the speed of sound.
SERIES 260 & 261 3-COMPONENT DYNAMIC FORCE - PCB
force measurement applications. Each utilizes an array of precision-aligned, quartz sensing crystals. Measurements along the z-axis are proportional to applied compression, tension and impact forces. Measurements along the x and y axes are proportional to shear forces that are imposed upon preloaded crystals by the test fixture. ICP ®
maximum vector | Amphenol Global Search | Amphenol
The vector of maximum sensitivity S in this example is tilted by angle f from the ideal vertical (z axis) direction, and decomposes to three orthogonal parts Sx, Sy and Sz. The z axis component Sz is the value normally reported as the accelerometer sensitivity.
How do I specify the performance characteristics of a cable assembly?
As a general rule, the maximum can be calculated by determining the Reflection Coefficient of the connectors on each end. Worst case will be the addition of the 2 reflection coefficients. Although small, some amount should be added for the cable.
4-Port Antenna
Array Y1 Y2 Connector 1-2 3-4 Polarization XPOL XPOL ... Maximum Effective Power Per Port Watts 160 W Inter/Intra Band Isolation dB > 30 Standard values based on NGMN-P-BASTA version 9.6 recommendation. Quoted performance parameters are provided to offer typical, peak or range values only and may vary as a result of normal testing ...
TN-7 Driving Long Cables - PCB
The maximum frequency that can be transmitted over a given cable length is a function of both the cable capac-itance and the ratio of the peak signal voltage to the current available from the signal conditioner according to: f(max) = 109 2πCV / (Ic-1) where: f(max)= maximum frequency (hertz) C = cable capacitance (picofarads)
10-Port Antenna - Amphenol Antenna Solutions
See details below and refer to the ordering options to see which actuators are available with this particular antenna. A single actuator individually controls the tilt of each band (no need for daisy chain cables between the bands). This module does not add any additional length to the antenna.
maximum vector | Amphenol Global Search | Amphenol
This optical transceiver comes with a maximum link length of 100m on OM4 multimode fiber and is capable of a 400Gb/s data rate with each channel transmitting up to 53.125Gb/s. The module also features outstanding BER and high sensitivity because of its reliable design and excellent coupling efficiency. ...
Understanding 3 dB 90° Hybrid Couplers - amphenolprocom.com
In the world of RF engineering, the 3 dB 90° Hybrid Coupler stands as a cornerstone for managing and manipulating signals effectively. Whether you're dealing with signal splitting, combining, or phasing, understanding the modes of operation for these couplers is essential for optimizing communication systems.
maximum vector | Amphenol Global Search | Amphenol
The R509LH is packed with a twenty-four element, low-frequency array that operates at anywhere between 28 and 60 kHz. The single, high-frequency ceramic operates at any frequency between 130 and 210 kHz and has a narrow, 8° to 4°, beam, delivering amazing target resolution and bottom detail. ... Maximum depth of 3048 m (10000') High frequency ...
Driving Long Cables | PCB Piezotronics
The nomograph below provides a simple, graphical method for obtaining the expected maximum frequency capability of an ICP ® measurement system. The maximum peak signal voltage amplitude, cable capacitance and supplied constant current must be known or presumed.
6-Port Antenna
Amphenol's RET-READY antennas are delivered with the RET Actuator already installed and pre-commissioned with all antenna parameters.
6-Port Antenna
Maximum Effective Power Per Port Watts 400 Intra Band Isolation dB > 28 (for 0°-2° tilt), > 30 Inter Band Isolation dB > 35 Standard values based on NGMN-P-BASTA version 10.0 recommendation.
maximum vector | Amphenol Global Search | Amphenol
Airmar’s TM265LH is packed with a seven-element, low-frequency array that operates between 42 and 65 kHz for excellent deep-water performance. The high-frequency ceramic operates between 130 and 210 kHz with a narrow, 10° to 6°, beam—perfect for picking apart structure and pinpointing tight-holding fish in structure. ...
TN-43 Electrical Characteristics of Endevco Variable Capacitance ...
the maximum voltage can cause permanent damage to the sensor. The 7290G accelerometer features an internal voltage reference that regulates the input excitation to a constant and stable voltage reference to support the operation of other components of the sensor.
APXVBB3L20H2 43-C-I20 - Amphenol Antenna Solutions
Array R1 R2 Y1 Y2 Y3 Connector 1-2 3-4 5-6 7-8 9-10 10 PORTS Polarization XPOL Azimuth Beamwidth (avg) 65° 65° Electrical Downtilt 2-12° 2-12° Dimensions 1998 x 469 x 205 mm (78.7 x 18.5 x 8.1 in) APXVBB3L20H2_43-C-I20 APXVBB3L20H2_43-C-I20S 65° 1998 mm INTEGRATED RET ORDERING OPTIONS Select from the following ordering options ANTENNA
maximum vector | Amphenol Global Search | Amphenol
DIN 1.0-2.3 connectors are available to perform at 50 ohm with a maximum frequency of 10 GHz as well as 75 ohm with a maximum frequency of 4 GHz. These performance specifications support high data rates for AES Audio, SD video, HD video, 3Gb/s video, and other high density digital broadcast formats.
APXVAA4L12N 43-U-I20 - Amphenol Antenna Solutions
Array R1 R2 Y1 Y2 Y3 Y4 Connector 1-2 3-4 5-6 7-8 9-10 11-12 4 PORTS 8 PORTS Polarization XPOL XPOL Azimuth Beamwidth (avg) 65° 65° Electrical Downtilt 4-18° 2-12° Dimensions 1219 x 499 x 215 mm (48.0 x 19.7 x 8.5 in) APXVAA4L12N_43-U-I20 APXVAA4L12N_43-A-I20 65° 1219 mm INTEGRATED RET