Search Results for miv valuation
Critical Care Sensors | Respiratory / Sleep Apnea
Telaire HS12SP is a bulk-resistance type of Relative Humidity (RH) Sensor providing a variable impedance value in response to the adsorbed water within the sensor’s proprietary thin-film polymer. Telaire ChipCap 2-SIP | Humidity and Temperature Sensor.
VERY HIGH FREQUENCY ICP® ACCELEROMETER - PCB
[4]Typical value. [5]Mounted resonance (nominal) without magnet. [6]Zero-based, least-squares, straight line method. [7]Typical. [8]See PCB Declaration of Conformance PS023 for details. Date: 11/04/2022 Date: 11/04/2022 Date: 11/04/2022 Date: 11/04/2022 71205 Entered: ND Engineer: gs Sales: KWW Approved: BAM Spec Number: Phone: 800-959-4464
High Speed Connectors | Products | Amphenol Aerospace
Combines our extensive legacy of Mil-Spec connectors with the latest in high-speed technology, providing both a durable and high-bandwidth system that supports data rates up to 56 Gbps in a lightweight, aluminum MIL-DTL-38999 shell.
VERY HIGH TEMPERATURE INDUSTRIAL ICP® ACCELEROMETER Revision: B - PCB
[1] Typical value. [2] Conversion Factor 1g = 9.81 m/s². [3] 1Hz = 60 cpm (cycles per minute). [4] The high frequency tolerance is accurate within ±10% of the specified frequency. [5] Zero-based, least-squares, straight line method. [6] See PCB Declaration of Conformance PS116 for details. SUPPLIED ACCESSORIES: Model 081A99 Cap Screw (3)
Model 699A06 - pcb.com
peak value is calculated by RMS * √2. The 699A06 does not measure a true peak value, but instead estimates the value mathematically based upon the RMS value. Peak to Peak (p-p) is a calculation of the difference between the highest positive peak and the lowest negative peak of a recorded sine wave. The p-p value is calculated as 2pk.
Sensor reliability impact on predictive maintenance costs
takes into account the time value of money or the effects of inflation, as the rate would have to be applied to all numbers. The "price" paid for the lower quality in this example is nearly $18,000 due to the difference between lifetime replacement costs for high quality versus low quality. That works out to almost $60 per accelerometer.
Smart Methodologies of Monitoring Reciprocating Compressors - PCB
The main purpose of any monitoring system is to protect machinery. It also provides critical data that operators and engineers can use to asses equipment condition, determine machinery availability, and
Network Management System and ICB Management System Software User’s Guide
Section 360-386-S01 5 3.1 NMS Manager Tool Bar User Login/Logout NMS System Configuration Show equipment as a list Reset screen Show equipment as icons
Centaur ExaMAX for Military | Centaur ExaMAX for Military 85 ohms ...
Centaur ExaMAX for Military I/O cable assembly and connector solutions
R-VPX Evolution 2.0 VITA 46.30 Connectors - Amphenol Aerospace
Amphenol R-VPX Evolution 2.0 VITA 46.30 Connectors: Intermateable with existing/legacy VITA 46 connectors and optimized for high-speed and harsh environments.
MLDX - Millivolt Output Low Pressure DX Series - All Sensors
Note 1: Pressure ranges in kPa are expressed as an approximate value. Pressure Range1 Proof Pressure2 Burst Pressure3 Note 2: Differential Proof Pressure: The maximum pressure which may safely be applied to one port of the product for it to remain in specification once pressure is returned to the operating pressure range.
Selecting Accelerometers for and Assessing Data from Mechanical ... - PCB
is related to its equivalent value ω n (in radians/second) as: ω n = 2πf n. Typically, an accelerometer shouldn’t be used above one-fifth its resonant frequency. At that point on the graph, device sensitivity, as a function of frequency, is 4% higher than its value near 0 Hz. Since shock pulses are composites of all frequencies, the total ...
Development of a Damped Piezoresistive MEMS High Shock Sensor - PCB
(Since Q = 1/(2ζ), if the critical damping ratio ζ has a value of 0.05, Q would be 10.) Also, since the mechanism of squeeze film damping necessarily includes structures close to the inertial mass, protective stops therefore become available. Survivability is expected to be enhanced by the prevention of over travel
R-VPX VITA 46 Connector System
Amphenol’s R-VPX VITA 46 Connector System is a ruggedized, high-speed, board-to-board interconnect system capable of data rate speeds of more than 10 Gb/s, meeting and exceeding VITA 46 standards.
Model 641B61 4-20 mA Output Velocity Sensor Installation and ... - PCB
to a value of 100 mV/IPS (±20%). Figure 3 – RV and RVVO wiring For integral cable sensors: RED 4-20mA Positive BLACK 4-20mA Negative (same as green) GREEN –RV and RVVO negative (same as black) WHITE +RV and RVVO positive Note: -The RV and RVVO Signal Negative has to be isolated from any grounding.
Model 3641A122KG PIEZORESISTIVE ACCELEROMETER Installation and ... - PCB
sensors were designed with relatively high value resistors (approximately 10 times that of other devices) to maximize battery life. 4.0 Common Applications The 3500/3600 Series PR Shock Accelerometers achieve true DC response for measuring long duration shock. For this reason, they are preferred for applications in which integration ...
EMI Filters | Products | Amphenol Aerospace
EMI is when low, medium, or high-frequency electromagnetic signals interfere with a system and cause performance degradation or malfunction. Some sources of EMI include interference from radio waves, stray transmissions, electric power lines or electric motor noise, or interference between electronic components or subsystems within the same system.
MG1 MediaGauge Series - Amphenol Sensors
We believe that making sustainable choices in the way we conduct our business creates short-term and long-term value for our stakeholders. We do not create long-term value by merely complying with regulations, but we go beyond compliance to find ways to green our operations and our products to ensure continuity of the material and human resources that we need to operate the business.
MLDX - Millivolt Output Low Pressure DX Series
Note 1: Pressure ranges in kPa are expressed as an approximate value. Pressure Range1 Proof Pressure2 Burst Pressure3 Note 2: Differential Proof Pressure: The maximum pressure which may safely be applied to one port of the product for it to remain in specification once pressure is returned to the operating pressure range.
Model M605B01 Low-cost Biaxial Industrial ICP® Accelerometer ... - PCB
Manual 21354 Rev E ECN 50523 CAUTION Refers to hazards that could damage the instrument. NOTE Indicates tips, recommendations and important information.