Search Results for moore liquid level controller
| Amphenol Socapex
back PS Series: Power Devices Solutions. Power Converters; Power Distribution Units; USB Keys & Amplifiers
NovaSensor NPP-301 Series Pressure Sensor - amphenol-sensors.com
• Pressure switches and controllers • Altimeters and barometers • Cable leak detection • Consumer appliances • Portable gauges and manometers Amphenol Advanced Sensors. NPP-301 Series Specifications Description The NPP-301 Series features silicon pressure sensors in surface mount packages. An ultra-small
Product Finder - Lutze Inc.
LUTZE Inc. 13330 South Ridge Drive • Charlotte, North Carolina 28273 • USA Phone: 704-504-0222 • Fax: 704-504-0223 • E-Mail: info (at) lutze.com
NovaSensor NPH Series Solid State Low Pressure Sensors
NPH Series - Specifications Parameter Value Units Notes Pressure Range 0 to 10 in H 2O (0 to 25 mbar) 0 to 2.5 kPa 0 to 1 psi (0 to 7 bar) 0 to 7 kPa 0 to 5 psi (0 to 0.34 bar) 0 to 30 kPa
Display Features and Modes - amphenol-sensors.com
level. If you are located at an altitude higher than 500 feet, an adjustment should be made to assure the maximum sensor accuracy. Once the elevation correction is set, it will be stored and saved in the monitor memory. To change the default setting, do as follows: 1. Press the Mode button until ELEVATION begins to blink. 2. Press Enter. 3.
Telaire T9602 Humidity and Temperature Sensor for OEM Installation
• Energy saving HVAC Control – Air Conditioning, Refrigeration, Indoor Air Quality, Vent Fans, Home Appliances, Humi/Dehumidifiers • Process Control & Instrumentation - Medical Instruments, Handheld Devices, Weather Stations, Food Processing, printers, RFID’s The T9602 offers the most advanced and cost
NPP-301 Series NovaSensor Surface Mount Pressure Sensor
• Pneumatic controls • Pressure switches and controllers • Altimeters and barometers • Cable leak detection • Consumer appliances • Portable gauges and manometers Amphenol Advanced Sensors. NPP-301 Series Specifications Description The NPP-301 Series features silicon pressure sensors
P1300 Low Pressure Sensor Die - amphenol-sensors.com
• Process control systems • HVAC • Cabin pressure, respirators Amphenol Advanced Sensors. P1300 Low Pressure Sensor Die Specifications Die dimentions (WxLxH): 2.7 mm X 3.2 mm - INa - INa + INa + INb + INa + INb - INb - INb - OUT + OUT + OUT - OUT Parameter Value Units Notes General
PRELIMINARY ISSUE - amphenolrf.com
CONFIGURATION LEVEL: Released NOTICE - These drawings, specifications, or other data (1) are, and remain the property of Amphenol corp. (2) must be returned upon request; and (3) are confidential and not to be disclosed to any person other than those to whom they are given by Amphenol Corp. the furnishing of these drawings, specifications, or
NovaSensor P111 Medium Silicon Pressure Sensor Die
• Process control systems • Pneumatic controls • Biomedical instruments • Hydraulic systems Description NovaSensor’s P111 piezoresistive pressure sensors are offered in a miniature 0.10 in x 0.12 in (2.7 mm x 3.2 mm) die. When excited with 1.0 mA, the P111 produces a millivolt output that is proportional to input pressure. The P111
P1300 Low Pressure Sensor Die - amphenol-sensors.com
• Process control systems • HVAC • Cabin pressure, respirators Amphenol Advanced Sensors. P1300 Low Pressure Sensor Die Specifications Die dimentions (WxLxH): 2.7 mm X 3.2 mm - INa - INa + INa + INb + INa + INb - INb - INb - OUT + OUT + OUT - OUT Parameter Value Units Notes General
NovaSensor NPP-301 Series Pressure Sensor - amphenol-sensors.com
• Pressure switches and controllers • Altimeters and barometers • Cable leak detection • Consumer appliances • Portable gauges and manometers Amphenol Advanced Sensors. NPP-301 Series Specifications Description The NPP-301 Series features silicon pressure sensors in surface mount packages. An ultra-small
P1300 Low Pressure Sensor Die - amphenol-sensors.com
• Process control systems • HVAC • Cabin pressure, respirators Amphenol Advanced Sensors. P1300 Low Pressure Sensor Die Specifications Die dimentions (WxLxH): 2.7 mm X 3.2 mm - INa - INa + INa + INb + INa + INb - INb - INb - OUT + OUT + OUT - OUT Parameter Value Units Notes General
High Silicon Pressure Sensor Die - amphenol-sensors.com
• Process control systems • Pneumatic controls • Biomedical instruments • Hydraulic systems The P122 piezoresistive pressure sensors are offered in a miniature 0.10 in x 0.10 in (2.5 mm x 2.5 mm) die. When excited with 1.0 mA, the P122 produces a millivolt output that is proportional to input pressure. The P122 is
P1300 Low Pressure Sensor Die - amphenol-sensors.com
• Process control systems • HVAC • Cabin pressure, respirators Amphenol Advanced Sensors. P1300 Low Pressure Sensor Die Specifications Die dimentions (WxLxH): 2.7 mm X 3.2 mm - INa - INa + INa + INb + INa + INb - INb - INb - OUT + OUT + OUT - OUT Parameter Value Units Notes General
Display Features and Modes - amphenol-sensors.com
level. If you are located at an altitude higher than 500 feet, an adjustment should be made to assure the maximum sensor accuracy. Once the elevation correction is set, it will be stored and saved in the monitor memory. To change the default setting, do as follows: 1. Press the Mode button until ELEVATION begins to blink. 2. Press Enter. 3.
Display Features and Modes - amphenol-sensors.com
level. If you are located at an altitude higher than 500 feet, an adjustment should be made to assure the maximum sensor accuracy. Once the elevation correction is set, it will be stored and saved in the monitor memory. To change the default setting, do as follows: 1. Press the Mode button until ELEVATION begins to blink. 2. Press Enter. 3.
www.amphenolrf.com
bag marking 8 rev level 'c' for motorola spec sn.k danbury and drawing 06 13 date -feb- -may -aug 53 98 98 eco 2990 47675 Ø5,69 appr jb/dr cpm/ ref 000 hole stamp 515± . 003] 5,49 min. detail 'aph ug-909/lj' c ? 50 (6.3mm) jacket stripping . insulator stripping recommended ing length 65' c temperature range packaging. a. single pack marking
Model M607A11/M010BZ Platinum Swiveler® Industrial ICP ... - PCB
with a resistor shifts the signal level to essentially eliminate the sensor bias voltage. The result is a drift-free AC mode of operation. 3.0 OPTIONAL FEATURES In addition to standard features, a variety of options are also available. When listed before the model number, the following prefix letters indicate that the
NovaSensor P111 Medium Silicon Pressure Sensor Die
• Process control systems • Pneumatic controls • Biomedical instruments • Hydraulic systems Description NovaSensor’s P111 piezoresistive pressure sensors are offered in a miniature 0.10 in x 0.12 in (2.7 mm x 3.2 mm) die. When excited with 1.0 mA, the P111 produces a millivolt output that is proportional to input pressure. The P111