Search Results for multi-trak
Human Machine Interface (HMI)- The Intelligent Interface between ...
The interface, which acts between the sophisticated pieces of machinery and the operators, is commonly known as Human Machine Interface . HMI can be any medium that helps you communicate with the connected machineries or devices from a simple mobile device like a tablet, to multi-touch-enabled control panels installed in high-end CNC machines ...
Amphenol product demonstrations at DesignCon 2023
The event will be taking place at the Santa Clara Convention Center in Santa Clara, California from Jan 31st through February 2nd, 2023. Amphenol will have an extensive array of interconnect solutions and exciting product demonstrations on display, including 224G, Automotive Ethernet, Thermal Management Solutions, and more in booth #833 at the ...
Revolutionizing Data Transmission with UltraPass™ OverPass™ Assemblies
Enter UltraPass ™ OverPass ™ Assemblies by Amphenol, a game-changing technology that is set to redefine data transmission as we know it. UltraPass ™ represents a paradigm shift in interconnect design, offering arrayed connector layouts for near-chip and on-package IO solutions. This innovation enables the highest differential pair count ...
Onboard Charger for Electric Vehicles - Amphenol CS
Apr 28, 2023. An on-board charger (OBC) is a device mounted inside the electric vehicle that converts AC power from an AC source into practical DC form, and its primary function is power conversion. This allows electric vehicles to be charged using the power outlets in our homes, eliminating the need to purchase additional equipment for power ...
Introducing Qi2 MAX: A Collaborative “Plug-and-Play ... - Amphenol CS
Amphenol and NuCurrent Collaboration - Qi2 MAXTM. Amphenol and NuCurrent's first collaborative project is a cutting-edge "plug-and-play" wireless charging module, in partnership with NXP Semiconductors. This module, known as Qi2 MAX TM - BPP and MPP Qi2 Certified, is designed to fulfill the market demand of original equipment manufacturers ...
Enabling Connector Innovations through Plating - Amphenol CS
Enabling Connector Innovations through Plating. Dec 7, 2017. Plating technology defines the mating cycles, durability and performance of connectors. GXT ®, AGT ®, and GCS ® are innovative plating solutions that create durable, reliable, and economical connectors with increased efficiency. GXT ® plating, a mix of palladium-nickel with gold ...
Amphenol's Leadership in Industrial Standards
Amphenol's Leadership in Industry Standards. Apr 13, 2022. Industry standards are agreements between designers, manufacturers, and end customers to define the requirements for products that will ensure consistency and compatibility across the ecosystem. For an interconnect supplier like Amphenol, participation in standards activities is ...
Seamless Connectivity with New Minitek® TPA Connectors - Amphenol CS
Terminal Position Assurance (TPA) is a connector design technique or a secondary locking mechanism that helps to align partially-seated terminals in the correct position inside the housing. Once the connector is mated, the TPA, which is usually snapped to rear end of the housing, helps in holding the Terminal in perfect alignment and prevents ...
BergStak® Secure Connectors with Unique Security Features
Multi-Use Connectors. The BergStak ® secure connectors are available in both multi-time-use and single-time use versions. The multi-time-use options are also available with tamper resistant screws. Both the versions are suitable for applications where security is top priority. The Multi-time-use solutions are much similar to the standard ...
CABLE APPLICATION & INSTALLATION GUIDE - TPC Wire
1. Correct Track Size Measure diameter of all track cables/hoses. Cables require 10% min. clearance from sides, separators, and other cables/hoses. Hoses require 20% min. clearance from sides, separators, and other cables/hoses. A larger track is required for application if these min. clearances can not be met. 2.
Aorora is Now on the AICC Website! - Amphenol CS
Aorora is Now on the AICC Website! Aug 26, 2019. In April, Amphenol extended our portfolio of BTB and FFC/FPC connectors with the acquisition of Aorora. Almost 400 Aorora parts are now searchable with datasheets, 2D drawings, 3D models and product specifications. Read on to learn more about the 4 key product lines. 0.50mm FFC/FPC Connectors.
Amphenol’s Connectivity Solutions for AI and ML
Amphenol’s Mini Cool Edge 0.60mm connector is well-suited for AI and ML applications due to its high density and high-speed capabilities. It meets specifications such as SFF-TA-1002, Gen Z, EDSFF, and OCP NIC 3.0, making it compatible with various industry standards. With options for the vertical, right angle, straddle mount, and orthogonal ...
Join Amphenol at Automotive World 2023
Automotive World is a leading global exhibition in automotive electronics, covering technologies like connected cars, autonomous driving, EV/HV/FCV, and MaaS. This year, 2023, the event will be held at Tokyo, Japan. Both Automotive OEMs and Tier 1 suppliers are among the 1,420 exhibitors, 70K visitors, and 170 speakers expected to attend the event.
The Zhaga Compliant Connector Solutions for LED Lighting - Amphenol CS
Zhaga compliant products are expected to accelerate the growth and adoption of LED lighting solutions globally. As a member of the Zhaga Consortium, Amphenol ICC is supporting new connector design ideas to promote the LED lighting industry. These LED standards can be broadly classified into 3 categories: LED lights including integrated LED ...
Amphenol Communication Solutions Extends high-speed cable product ...
Enterprise Server Solution Providers Launches EDSFF, OCP, Power Shelf and PCIe ® DirectAttached ® Cable Solutions. Singapore, March 4, 2023 – Amphenol Communications Solutions is pleased to announce today, the release of its high-speed cable solutions with options to meet PCIe ®, EDSFF, OCP specifications, and power shelf requirements. In close collaboration with the PCI-SIG association ...
Tag Archives: RJ45 - Amphenol CS
Multi-Trak (1) Multipitch 1.25mm (1) ND9 Series (1) NEPCON (1) NEPCON Japan (1) National Intern Day (1) Network (1) PCE (1) PCIE Gen 5 connetcors (1) PCIe 6.0 (1) PCIe Card Edge Connectors (1) PCIe DirectAttached (1) PCIe Gen 4 & Gen 5 CEM connectors (1) PCIe Gen 5 CEM Connector (1) PCIe Gen 5 CEM Connectors (1) PCIe M.2 Gen 5 Connectors (1 ...
ComboStak® and PowerStak® Connectors for Data Centers - Amphenol CS
ComboStak ® is a symmetrical board-to board-connector with an even number of power contacts from 2 up to 10 positions at both ends of the connector and signal contacts from 6 up to 140 positions placed in between, and available in stack heights from 5mm to 20mm in 1mm increments . With signal speeds up to 12Gb/s, these connectors form a double ...
nano-pitch | Amphenol Global Search | Amphenol
The 0.60mm pitch connector come with a slim form factor design, capable of transmitting high-speed signal up to 56G PAM4 PCIe® Gen 5 and target to meet 64G PAM4 PCIe® Gen 6 and a. Amphenol introduces the next-generation product - Multi-Trak™.
Amphenol’s Newest High Speed Interconnect Offerings
Amphenol’s high speed loopback modules include 10G SFP+, 28/56G QSFP, 40G QSFP+, 200G / 400G QSFP DD and OSFP. The SFP+ loopbacks are offered as passive electrical modules and come with and without EMI spring fingers. Amphenol's QSFP28/56G loopback modules are part of our comprehensive QSFP28/56G product family which includes copper cables ...
Tag Archives: Mini Cool Edge IO - Amphenol CS
Self-driving cars, automated homes, and intelligent office spaces are a reality today and are taking a new level up each day. With the implementation of the fifth generation of telecom networking, the 5G, it is not only meeting high-speed requirements but also creating a new ecosystem with the Internet of Things where these connected devices communicate with each other making life easier.