Search Results for oreshnik rocket
Market Connector: Directed Energy Weapons - Amphenol Aerospace
With a range of more than six miles, the Iron Beam is designed to precisely target and shoot down incoming rockets and missiles at a cost of no more than a few dollars per “shot.” Another promising application for DEW technology is non-lethal weapons such as the Active Denial System (ADS), a microwave non-lethal weapon.
Israel Signs $540 Million Deal to Fast-Track Iron Beam Laser Defense ...
Israel has finalized a $540 million contract with Rafael Advanced Defense Systems and Elbit Systems to accelerate the deployment of the Iron Beam laser air defense system. With this investment, the Iron Beam is slated to come online sometime in 2025.
Industry Briefs | Products - Amphenol Aerospace
Lockheed Martin received a $4.8 billion contract from the U.S. Army for additional GMLRS rockets, the primary munition for the HIMARS and MLRS launcher systems. U.S. Space Force selects Lockheed, Raytheon to develop satellite ground systems
SV Microwave Advances The RF Trend Towards Smaller Communication ...
SpaceX has more compet itive pricing, charging around $1,300 per pound of payload on its medium-lift Falcon 9 rocket, and even offering a SmallSat rideshare program. SmallSats are dominating Low Earth Orbit (LEO), where the shorter distance for radio signals to travel is an advantage for communications speed.
AEROSPACE FLIGHT TEST - PCB
source for operation. These pressure sensors are useful for measuring transient pressure events, air turbulence, and other such acoustic phenomena on aircraft structures, rockets, . y pressure phenomena. Miniature high sensitivity ICP® probes are used to measure small dynamic pressures such as turbulence, noise, sound, and pulsations, especially in
TECHNICAL NOTE TN-15 - PCB
high-frequency pressure sensors to make shock wave, blast, rocket combustion instability, and ballistic measurements. Piezoelectric sensors at that time had limited frequency response, and were mainly used for acoustic and engine combustion applications. It was during this period that Walter Kistler, working closely with Abe
AERODYNAMIC AND AERO-ACOUSTICS SENSORS - PCB
Aerodynamics and rocket acoustics : Small scale models in wind tunnels, aerodynamic surfaces during flight tests, and helicopter or turbine blade surface. pressure measurements
Space | Markets - Amphenol Aerospace
Rugged High Speed & Fiber Optic Connectors and Cable Assemblies -- Quadrax, Octonet, Differential Twinax, Triax, Coaxial, ARINC 801, M29504 -- up to 10 Gb/s. Integrated connectors that convert to fiber optics or between protocols.
Aerodynamic & Aero-Acoustics Sensors for A&D - PCB
PCB manufactures sensors used by aerodynamics & aero-acoustics measurements, including wind tunnel testing for airplanes and rockets.
Lockheed Martin tasked with developing nuclear-powered spacecraft
As the prime contractor, Lockheed Martin will develop an experimental nuclear thermal rocket vehicle (X-NTRV) and engine. If successful, the demonstration could pave the way for nuclear propulsion systems to be used for deep space exploration.
Aerospace Flight Test | PCB Piezotronics
PCB’s engineering staff is experienced in design of sensors, cables, and signal conditioning for flight test applications.
IECEx - PCB
Rocket launch loading and acceleration. MEMS DC . RESPONSE . ACCELEROMETERS SERIES . 3711E, 3713E, & 3741E. Series 3713E. Series 3711E. Series 3741E. IECEx IECEx IECEx IECEx. Rugged and Durable Series 3711E and 3713E MEMS DC . Response Accelerometers . Series 3711E and series 3713E have
Press Release: Endevco Series 2680B Airborne Charge Amplifier
Series 2680B can be used in flight testing, gas turbine engine testing, and rocket launch payload acoustic measurements.
How small satellites are leading to big leaps in space
While heavier satellites require larger and more expensive rockets, smallsats can be launched using smaller and cheaper rockets which can significantly reduce the overall cost of a space mission. Improved Launch Systems: The emergence of dedicated smallsat launch vehicles and rideshare opportunities has lowered the barriers to access space.
Poland signs contract for 800 Hellfire Missiles
Poland has signed a contract to purchase 800 AGM-114R2 Hellfire II Missiles from the U.S. The missiles are planned to be used with the Polish Air Force’s new fleet of 32 Leonardo AW149 helicopters, which the country signed a deal to acquire in July 2022.
TN-26 Why Is MEMS the Preferred Technology for High Shock ... - PCB
veloping and launching rocket systems from Sandia and NASA facilities. These rocket focused activ. s part of the FAA’s congressionally mandated Aging Aircraft Program. He validated this program with the aircraft and engine OEMs, the Air Transport Association, and other organizations, .
Lockheed Martin receives $4.8 billion contract for more GMLRS rockets ...
The U.S. Army awarded Lockheed Martin a $4.8 billion contract for two full-rate production lots of Guided Multiple Launch Rocket System (GMLRS) all-weather rockets and associated equipment.
TN-23 Pyroshock Explained - PCB
environment of pyroshock. Specifically, it (1) defines pyroshock, (2) identifies those situations where pyroshock can induce equipment failure, (3) explains the response of structural systems to pyroshock, and (4) discusses uniqueness in the shock spectra (see PCB® Tech Note 19) .
Dynamic ICP Pressure Sensors - PCB
Quartz piezoelectric pressure sensors are ideal for rocket motor testing to verify instabilities during motor firings. One such example was a hybrid engine comprised of solid fuel and liquid oxidizer. Testing performed on the rocket motor used a Series 124A water cooled sensor mounted in the combustion chamber. Figure 7 shows
PCB's Model 351A15 Withstands Temps Down to -420°F | PCB Piezotronics
It is the new flagship model in the 351 family of cryogenic accelerometers. Model 351A15 features: Small size, 0.77 in x 0.28 in hex (19.6 mm x 7.2 mm) and low weight, 0.07 oz (2 gm). The cold side operating temperature of the model is -320°F (-196°C).