Search Results for phone connector jack
Handportable Antennas ELF 900/...-TNC - amphenolprocom.com
Amphenol Procom offers BFME-connectors which are applicable for the entire product line of the black portable antennas or other equipment with FME-connectors. Explore all Portable Antenna Connectors . to product finder. PRODUCT_CONTACT. If you need help. Denmark: dksales@amphenolprocom.com UK:
Website Registration - amphenol-ns.com
Cable Management; Racks and Accessories; Enclosures; Optical Passives; Partners. For Our Customers; For Our Distribution Partners. Project Registration; Logo Style Guide and Use; Lineamientos del Logotipo; Our Services. Configure to Order Solutions; Custom Configured Solutions; Fiber Raceway Solutions; Pre-Terminated Solutions
Amphenol Automotive | sehpunkt
The product family is available in the HV power classes 2, 3, 4 and 5, the connector housings with cable outlet in 90° and 180° offer customers a comprehensive choice for a wide variety of applications.... 2. August 2019 Amphenol Tunesia A look at our company and the production in Tunisia. Enabling the electronics revolution. ...
750700JBT0BK02000001 - Amphenol Broadband Solutions
Skip to main content. Products; Solutions; Company. News; Events; Media; Fiber 101 Training; Certifications
ASRN7A22S - Amphenol Air LB
Plug ASR Metallized 2 socket contacts size 20 + 6 socket contacts size 22 (A2) Polarizing 2
DAS Antennas PCPO xH/TETRA/ - amphenolprocom.com
The connector is placed at one side to enable mounting close to a wall. Including wall mounting bracket. PATCH-MAMO and PATCH/WAMO to be ordered separately. Specifications. Electrical; Model: PCPO xH/TETRA/... Frequency: 380 - 470 MHz covered by two models: Antenna Type: Left or right hand circularly polarized patch antenna: Max. Input Power
C:UsersROrmanDesktopFLS Customer DWG Drawing updateUpdated 5-16C ...
of: sh: rev: dwg no: title: rev description date revisions eco by appr 1 1 a3 fls014xxxp03 ecomate aquarius,receptacle, square flange, xx position, male,shell size 14
Website Registration - amphenol-ns.com
Cable Management; Racks and Accessories; Enclosures; Optical Passives; Partners. For Our Customers; For Our Distribution Partners. Project Registration; Logo Style Guide and Use; Lineamientos del Logotipo; Our Services. Configure to Order Solutions; Custom Configured Solutions; Fiber Raceway Solutions; Pre-Terminated Solutions
Chem-Gard 200 Single Conductor Cable replaces THHN Wire at Wastewater ...
cable running through conduit under sedimentation basins. Caps on conduit at these sedimentation basins had been left open, so the old THHN wire was getting damaged and failing as a result of being run over or water infiltrating the conduit. The wastewater treatment plant was also facing cable failure in its junction boxes due to high temperatures.
Plug Reversed rack 2 Modules Metallic Standard Black nickel ...
Plug Reversed rack 2 Modules Metallic Standard Black nickel Polarization D Not mounted
PRO-MCU380-EXT-ELW
19" Front plate black with connectors in front * 210003008: Add to quote: 19" Front plate black with connectors in back * 210003009: Add to quote: Typical Attenuation values. The built-in high-pass filter attenuates large signal interference and harmonic from radiosystems below 174 MHz.
Amphenol AMAO Product Compliance - Environmental Engineering
MS27656T21F11S YES CONNECTOR, ELECTRICAL RECEP. N/A Per review of the materials & processes utilized in the manufacture of the above -listed PN, Amphenol Military - Aerospace Operations hereby acknowledges the referenced product is in conformity with Directive 2011/65/EU
EU RoHS II Certificate of Conformance - amphenol-aerospace.com
10-552011-98P YES CONNECTOR, ELECTRICAL, RECEPTACLE 6(c) Per review of the materials & processes utilized in the manufacture of the above -listed part number , Amphenol Aerospace Operations and Commercial Air Division hereby acknowledges the referenced product is in conformity with the following: Directive 2011/65/EU (as amended)
SS164 50/200kHz, 1kW, 20° Tilt, M&M Transducer, DT
SS164 50/200kHz, 1kW, 20° Tilt, M&M Transducer, DT. Support. Cables & Adapters. Mix and Match Cables 1kW; Mix and Match Cables 600W
Amphenol AAO/ACAD Product Compliance - Environmental Engineering
D38999/24FA35SD YES CONNECTOR, ELECTRICAL, RECEP. 6(c) Per review of the materials & processes utilized in the manufacture of the above -listed part number , Amphenol Aerospace Operations and Commercial Air Division her eby acknowledges the referenced product is in conformity with the following:
Amphenol AAO/ACAD Product Compliance - Environmental Engineering
D38999/20KB98PN YES CONNECTOR, ELECTRICAL, RECEP. 6(c) Per review of the materials & processes utilized in the manufacture of the above -listed part number , Amphenol Aerospace Operations and Commercial Air Division hereby acknowledges the referenced product is in conformity with the following:
Long flanged Receptacle monomodule With conductive panel sealing With ...
Military & Commercial Aerospace specification for rectangular modular connectors; Fully qualified and compliant with ARINC 809 specifications; Tested and qualified per EN4165 Seri
Feeder Cable - Amphenol Antenna Solutions
Feeder Cable AAF-78-ST-JJ 7/8” Low Loss Coaxial Cable Quoted performance parameters are provided to offer typical, peak or range values only and may vary as a result of normal testing, manufacturing and operational conditions. Extreme operational conditions and/or stress on structural supports is beyond our control.
Amphenol AAO/ACAD Product Compliance - Environmental Engineering
D38999/26FJ35PN YES CONNECTOR, ELECTRICAL, PLUG 6(c) Per review of the materials & processes utilized in the manufacture of the above -listed part number , Amphenol Aerospace Operations and Commercial Air Division hereby acknowledges the referenced product is in conformity with the following:
Test2 - US Wire
What is Lorem Ipsum? Lorem Ipsum is simply dummy text of the printing and typesetting industry. Lorem Ipsum has been the industry’s standard dummy text ever since the 1500s, when an unknown printer took a galley of type and scrambled it to make a type specimen book. It has survived not only five centuries, but […]