Search Results for psas
OverPass™- The High Speed Solution - Amphenol CS
Amphenol’s OverPass ™ cable system allows for the transfer of high-speed signals to twinax cables shortly after they are launched from the ASIC. This enables a simple, low-loss, direct link to pluggable modules or anywhere in the system. Multiple interface choices are available, so system designers can optimize key parameters like signaling ...
PCIe® Gen 4 & Gen 5 CEM connectors for High Speed Connections
PCIe ® Gen 4 & Gen 5 CEM Connectors. Amphenol offers PCIe ® Gen 4 & Gen 5 CEM connectors that meet and outperform industry standard PCIe ® 4.0 and 5.0 with enhanced speed performance. Footprint compatible with PCIe Gen 3/2/1, these optimized series supports backwards mating and supports higher speed performance without altering footprint.
Learn More about Connector Mating Cycles - Amphenol CS
The number of times a connector can connect and disconnect with its counterpart while meeting all its specifications is termed as “mating cycles”. The mating cycle of a connector helps to estimate the life span of a connector in a particular application. For instance, while the mating cycle for a USB connector will be in thousands, a FFC ...
All About QSFP Cables, Connectors, and More - Amphenol CS
All About QSFP Cables, Connectors, and More. Nov 6, 2020. Amphenol is your industry leader when it comes to the innovation, design, manufacture, and supply of high-performance cable connectors and assemblies. Our customer base consists of all major data center, networking, HPC, telecom, server and storage system providers across the globe.
The Evolution of PCI Express® - Amphenol CS
PCI Express ® provides a point-to-point interconnect solution for communication between two devices. PCIe ® Gen1 was introduced in 2003 and supported a transfer rate of 2.5GT/s and a data rate of 250MB/s per lane. With technological improvements, people began looking for higher speed and performance which led to the introduction of PCIe ...
Learn about Ingress Protection - Amphenol CS
A rating of IP67 however, provides protection from dust as well as protection from water ingress when submerged under 1 Metre of water for 30 minutes, while IP68 defines protection from being submerged for extended periods of time. IP69K is a more recent designation which specifies protection from powerful, high-temperature water jets.
Track the Modern Train: Outlook on Railway Connectors - Amphenol CS
Track-side signaling cabinets and on-track interlock switches communicate with the train using GSM-R, a wireless protocol having a rail-specific spectrum. GSM-R also allows signals to clearly pass from locomotive to end coach and back, regardless of travel speed. 5G is expected to replace GSM-R in the coming years.
Amphenol Exhibits and Demos at DesignCon 2022
Amphenol Exhibits and Demos at DesignCon 2022. DesignCon, the largest event for Chip, Board, and Systems Design Engineers, brings together the brightest talents across the world. This premier gathering has the legacy of more than two decades in solving the signal and power integrity challenges and creating innovative design solutions for tomorrow.
Smarter Vehicles - CAN Bus to Automotive Ethernet - Amphenol CS
Automotive Ethernet delivers unmatched data transfer speeds up to 100x faster than CAN bus, and will establish the necessary standards for advancing autonomous vehicle technology. Connectors like NETBridge from Amphenol ICC are ideal for automotive Ethernet connections. These USCAR-2 compliant connectors are designed for the harsh automotive ...
Amphenol Receives CISCO 2021 GSM Supplier of The Year and Cisco Supply ...
Wallingford, Connecticut, September 21, 2021. Amphenol Corporation today announced it was the recipient of two Cisco awards: Cisco 2021 GSM Supplier of the Year and Cisco 2021 Supply Chain Operations Supplier of the Year. Cisco unveiled the award winners at its annual Supplier Appreciation Event (S
Mini Cool Edge: Fine Pitch and Versatile Connectors - Amphenol CS
With a discrete pin design, these connectors support single-ended and high-speed differential pairs up to 32G NRZ, 56G PAM4. Mini Cool Edge 0.60mm connectors meet SFF-TA-1002, Gen Z, EDSFF and OCP NIC3.0 specifications. Though these connectors are primarily used in servers and data centers, these can be used in most of board-to-board ...
High-Performance Industrial Computing with CompactPCI Serial - Amphenol CS
High-Performance Industrial Computing with CompactPCI Serial. May 30, 2019. CompactPCI is an architecture for industrial computers that combines PCI signaling protocols with Eurocard-type connectors. Introduced over 20 years ago, it continues to be a successful architecture. CompactPCI continues to evolve to meet increasing speed demands; from ...
Amphenol will be at Smart Production Solutions (SPS) 2023
Nov 10, 2023. Amphenol is participating in the much-anticipated Smart Production Solutions (SPS) 2023 event with a vast display of cutting-edge industrial technology and solutions. Amphenol divisions that will be present at SPS include Amphenol Industrial, Amphenol CONEC, Amphenol LTW, and Amphenol Communication Solutions.
Amphenol Communications Solutions releases Internal High-Speed Link ...
Amphenol Communications Solutions releases Internal High-Speed Link Input Output Connectors Performing to PCI-SIG Gen 6 Specifications - Designed for Next Generation Enterprise Server Equipment
Welcome to the AICC Connect - Amphenol CS
Welcome to the AICC Connect. Nov 13, 2017. Our goal is to connect with you and share our exciting new products and technology which are enabling the electronics revolution and helping our customers to develop faster, smaller and cost effective solutions. We will also share some of the key events and exhibitions we will be attending, so watch ...
The Crucial Role of Battery Management Systems (BMS) in Robotics
Feb 7, 2024. In the ever-evolving landscape of robotics, the heartbeat of these autonomous systems lies within their power source – the battery. Much like in electric vehicles, the Battery Management System (BMS) emerges as a critical player, ensuring the efficient utilization of energy and the safeguarding of batteries against potential hazards.
Human Machine Interface (HMI)- The Intelligent Interface between ...
The interface, which acts between the sophisticated pieces of machinery and the operators, is commonly known as Human Machine Interface . HMI can be any medium that helps you communicate with the connected machineries or devices from a simple mobile device like a tablet, to multi-touch-enabled control panels installed in high-end CNC machines ...
Visit Amphenol at Avnet Future Mobility Asia 2023
May 15, 2023. Amphenol’s latest power connectors will be presented in Avnet’s exhibition and summit Future Mobility Asia, on May 17-19, 2023 from 9:00 to 18:00. The venue is at Queen Sirikit National Convention Centre, Bangkok. Amphenol’s booth is in Hall 3, MD17.
Components of Advanced E-Bikes - Amphenol CS
Basic components of E-Bikes. There are three primary components for an e-bike, which differentiate it from a normal bicycle: Battery Pack, Control Console, and Motor Unit. Like mentioned earlier, the battery pack is the powerhouse of an e-bike. Most modern e-bikes use lithium battery which is generally placed in the downtube or on the rear ...
Amphenol Communication Solutions releases Busbar Connectors – Open ...
Amphenol Communications Solutions is pleased to announce today, the release of its BarKlip® BK500 IO and BarKlip® BK150 IO busbar connectors. These high-current connectors are fully compliant with OCP ORv3 power output and IT gear specifications supporting 48V power rack architecture and are ideal f