Search Results for rangiora medical - good street
PROTIMETER Timbermaster - amphenol-sensors.com
1 Timbermaster® Introduction The Protimeter Timbermaster is a conductivity moisture meter designed for use in wood. Moisture measure-ments can be taken using the integral pin electrodes, or using the meter in
PROTIMETER Timbermaster - amphenol-sensors.com
1 Timbermaster® Introduction The Protimeter Timbermaster is a conductivity moisture meter designed for use in wood. Moisture measure-ments can be taken using the integral pin electrodes, or using the meter in
NTC Type C100 - amphenol-sensors.com
• Resin coated for good mechanical strength and resistance to solvents NTC Type C100 Thermometrics Epoxy-Coated Chip Thermistor Description Epoxy-coated chip thermistors with 0.012 in (0.3 mm) bare tinned-copper lead-wires. Amphenol Advanced Sensors. Data Thermal And Electrical Properties:
PROTIMETER Timbermaster - amphenol-sensors.com
1 Timbermaster® Introduction The Protimeter Timbermaster is a conductivity moisture meter designed for use in wood. Moisture measure-ments can be taken using the integral pin electrodes, or using the meter in
PROTIMETER Timbermaster - amphenol-sensors.com
1 Timbermaster® Introduction The Protimeter Timbermaster is a conductivity moisture meter designed for use in wood. Moisture measure-ments can be taken using the integral pin electrodes, or using the meter in
CERTIFICATE - amphenolalden.com
117 North Main St. Brockton, MA 02301 USA At the Sites Specific Scope Site Amphenol Alden Products Company 117 North Main St. Brockton, MA 02301 USA Central Function, Design and Manufacture the Medical Market Ave. Severiano Talamante No. 6-B, Hermosillo, Sonora 83170 Mexico Manufacture of Connectors and Cable Assemblies for the Medical Market
NovaSensor Medium and High Pressure MEMS Pressure Sensor Die
Each wafer will have the following information: Lot #, Wafer #, Part #, and the number of good (yielded) die. Warranty NovaSensor warrants its products against defects in material and workmanship for 12 months from date of shipment. Products not subjected to misuse will be repaired or replaced. THE FOREGOING IS IN LIEU OF ANY OTHER EX-
P1300 Low Pressure Sensor Die - amphenol-sensors.com
P1300 Low Pressure Sensor Die Silicon Pressure Sensor Die Features • High reliability, solid state silicon pressure sensors • Standard pressure ranges: 2.5 kPa (0.3 psi) and
PROTIMETER - amphenol-sensors.com
they do not measure relative humidity, their indications are a fairly good representation of it. A high reading on such a meter (in the absence of contaminating salts or carbonaceous materials) indicates a damp condition of approximately equal significance in wood, brick, plaster or wallboard, regardless of the very different moisture contents.
P330W Eval Kit - amphenol-sensors.com
applications with restricted dimensional profiles, such as medical catheters and IC packages. When excited with a DC voltage source, the P330W produces a mV output that is proportional to the applied pressure. The P330W employs a half-bridge design, which requires two external resistors to complete a full- bridge configuration.
P1300 Low Pressure Sensor Die - amphenol-sensors.com
P1300 Low Pressure Sensor Die Silicon Pressure Sensor Die Features • High reliability, solid state silicon pressure sensors • Standard pressure ranges: 2.5 kPa (0.3 psi) and